<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックSlow TAD Debugging when using external DDR RAM on TWR-K70 (MQX 4.0.1, CW10.4)</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Slow-TAD-Debugging-when-using-external-DDR-RAM-on-TWR-K70-MQX-4/m-p/271387#M8318</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Although TAD debugging works in general while using external DDR RAM, it is painfully slow. On hitting a breakpoint it takes very long until the TAD data is shown, even if I have only one TAD view enabled. Also the whole CodeWarrior IDE often freezes for minutes until it can be accessed again. This makes debugging with OS awareness impossible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone confirm these issues? Is there a way to improve the debugging experience with DDR RAM?&lt;/P&gt;&lt;P&gt;By the way: I'm using the onboard programmer/debugger of the TWR-K70.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 08 Jul 2013 14:16:53 GMT</pubDate>
    <dc:creator>friederschrempf</dc:creator>
    <dc:date>2013-07-08T14:16:53Z</dc:date>
    <item>
      <title>Slow TAD Debugging when using external DDR RAM on TWR-K70 (MQX 4.0.1, CW10.4)</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Slow-TAD-Debugging-when-using-external-DDR-RAM-on-TWR-K70-MQX-4/m-p/271387#M8318</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Although TAD debugging works in general while using external DDR RAM, it is painfully slow. On hitting a breakpoint it takes very long until the TAD data is shown, even if I have only one TAD view enabled. Also the whole CodeWarrior IDE often freezes for minutes until it can be accessed again. This makes debugging with OS awareness impossible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone confirm these issues? Is there a way to improve the debugging experience with DDR RAM?&lt;/P&gt;&lt;P&gt;By the way: I'm using the onboard programmer/debugger of the TWR-K70.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Jul 2013 14:16:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Slow-TAD-Debugging-when-using-external-DDR-RAM-on-TWR-K70-MQX-4/m-p/271387#M8318</guid>
      <dc:creator>friederschrempf</dc:creator>
      <dc:date>2013-07-08T14:16:53Z</dc:date>
    </item>
  </channel>
</rss>