<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックRe: Start a timer in a interrupt?</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Start-a-timer-in-a-interrupt/m-p/266433#M8042</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MQX timer functions do a call to _lwsem_wait(), under some conditions. _lwsem_wait() can't be called from an isr. Therefore, MQX timer functions should not be called from an isr.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Aug 2013 05:28:08 GMT</pubDate>
    <dc:creator>Martin_</dc:creator>
    <dc:date>2013-08-21T05:28:08Z</dc:date>
    <item>
      <title>Start a timer in a interrupt?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Start-a-timer-in-a-interrupt/m-p/266432#M8041</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I am using MK60F120, MQX4.0.1, cw10.4.&lt;/P&gt;&lt;P&gt;And now I create a timer to generate a interrupt every 50ms.&lt;/P&gt;&lt;P&gt;When I start the timer in the main task, it works fine. But when I start the timer in a button interrupt, it does not work.&lt;/P&gt;&lt;P&gt;I am using following code to start the timer.&lt;/P&gt;&lt;P&gt;*TimerID = _timer_start_periodic_every_ticks(key_generator, 0, TIMER_ELAPSED_TIME_MODE,Ticks);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there something wrong or I can't start a timer in a interrupt?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Aug 2013 23:22:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Start-a-timer-in-a-interrupt/m-p/266432#M8041</guid>
      <dc:creator>danielchai</dc:creator>
      <dc:date>2013-08-20T23:22:50Z</dc:date>
    </item>
    <item>
      <title>Re: Start a timer in a interrupt?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Start-a-timer-in-a-interrupt/m-p/266433#M8042</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MQX timer functions do a call to _lwsem_wait(), under some conditions. _lwsem_wait() can't be called from an isr. Therefore, MQX timer functions should not be called from an isr.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Aug 2013 05:28:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Start-a-timer-in-a-interrupt/m-p/266433#M8042</guid>
      <dc:creator>Martin_</dc:creator>
      <dc:date>2013-08-21T05:28:08Z</dc:date>
    </item>
  </channel>
</rss>