<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Getting the MAC Address for AR4100 SPI flash memory in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Getting-the-MAC-Address-for-AR4100-SPI-flash-memory/m-p/262309#M7819</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I try to program the SPI-flash memory for AR4100 wifi module. To do that I follow an app note called "Programming the AR4100 SIP and SPI-flash on the Freescale Tower". One of the items needed to be programmed is the MAC address. I assume the MAC address should be a 12-digit unique number. So my question is how can I get or generate a new MAC address for my phy chip? Is there any process we can use for our production line?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Sina &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Feb 2014 22:00:57 GMT</pubDate>
    <dc:creator>amleng</dc:creator>
    <dc:date>2014-02-26T22:00:57Z</dc:date>
    <item>
      <title>Getting the MAC Address for AR4100 SPI flash memory</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Getting-the-MAC-Address-for-AR4100-SPI-flash-memory/m-p/262309#M7819</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I try to program the SPI-flash memory for AR4100 wifi module. To do that I follow an app note called "Programming the AR4100 SIP and SPI-flash on the Freescale Tower". One of the items needed to be programmed is the MAC address. I assume the MAC address should be a 12-digit unique number. So my question is how can I get or generate a new MAC address for my phy chip? Is there any process we can use for our production line?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Sina &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Feb 2014 22:00:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Getting-the-MAC-Address-for-AR4100-SPI-flash-memory/m-p/262309#M7819</guid>
      <dc:creator>amleng</dc:creator>
      <dc:date>2014-02-26T22:00:57Z</dc:date>
    </item>
    <item>
      <title>Re: Getting the MAC Address for AR4100 SPI flash memory</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Getting-the-MAC-Address-for-AR4100-SPI-flash-memory/m-p/262310#M7820</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As first I would like to note that generally MAC address has to be unique.&lt;/P&gt;&lt;P&gt;Therefore there is IEEE Standards Association where you can register block of MAC addresses in case when you produce end point devices (like routers, network cards, mobile phones with wifi,...).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, there are two options:&lt;/P&gt;&lt;P&gt;If you buy wifi module as end point device, MAC address should be provided by Atheros together with wifi module.&lt;/P&gt;&lt;P&gt;If you buy wifi module as component and you want produce end point devices, you have to contact IEEE Standards Association and register some block of MAC addreses for your devices.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For testing purposes you can use locally administered MAC adresses (second least significant bit of first byte=1).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Few links about MAC addresses:&lt;/P&gt;&lt;P&gt;&lt;A href="http://en.wikipedia.org/wiki/MAC_address"&gt;http://en.wikipedia.org/wiki/MAC_address&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://standards.ieee.org/develop/regauth/"&gt;http://standards.ieee.org/develop/regauth/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://en.wikipedia.org/wiki/Organizationally_Unique_Identifier"&gt;http://en.wikipedia.org/wiki/Organizationally_Unique_Identifier&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://standards.ieee.org/develop/regauth/tut/macgrp.pdf"&gt;http://standards.ieee.org/develop/regauth/tut/macgrp.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Feb 2014 15:01:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Getting-the-MAC-Address-for-AR4100-SPI-flash-memory/m-p/262310#M7820</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2014-02-27T15:01:48Z</dc:date>
    </item>
  </channel>
</rss>