<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RTCS ipcfg in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/RTCS-ipcfg/m-p/258016#M7599</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is a short description of ipcfg in the MQX RTCS User Guide (MQXRTCSUG), section 5.10.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Essentially ipcfg is a higher-level wrapper over the underlying RTCS functions which makes them a bit easier to use. It also provides an associated link monitoring task which takes care of (un)binding interfaces when a cable is (dis)connected. It will manage multiple interfaces.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Oct 2014 19:38:53 GMT</pubDate>
    <dc:creator>matthewkendall</dc:creator>
    <dc:date>2014-10-15T19:38:53Z</dc:date>
    <item>
      <title>RTCS ipcfg</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/RTCS-ipcfg/m-p/258014#M7597</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I haven't been able to find a good general description of the ipcfg module in RTCS. It seems to duplicate functionality within RTCS and it's not clear why I would use one or the other&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there an intended application for the ipcfg_[xyz] functions? Eg. Why would I use ipcfg_bind_dhcp() instead of RTCS_if_bind_DHCP()?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;General guidance from users would be much appreciated. Also, any Freescale documentation on their intent would be good.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;+Joel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Aug 2013 22:03:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/RTCS-ipcfg/m-p/258014#M7597</guid>
      <dc:creator>theJoel</dc:creator>
      <dc:date>2013-08-15T22:03:30Z</dc:date>
    </item>
    <item>
      <title>Re: RTCS ipcfg</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/RTCS-ipcfg/m-p/258015#M7598</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I also don't know this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sean&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Oct 2014 18:58:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/RTCS-ipcfg/m-p/258015#M7598</guid>
      <dc:creator>ironsean</dc:creator>
      <dc:date>2014-10-14T18:58:09Z</dc:date>
    </item>
    <item>
      <title>Re: RTCS ipcfg</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/RTCS-ipcfg/m-p/258016#M7599</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is a short description of ipcfg in the MQX RTCS User Guide (MQXRTCSUG), section 5.10.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Essentially ipcfg is a higher-level wrapper over the underlying RTCS functions which makes them a bit easier to use. It also provides an associated link monitoring task which takes care of (un)binding interfaces when a cable is (dis)connected. It will manage multiple interfaces.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Oct 2014 19:38:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/RTCS-ipcfg/m-p/258016#M7599</guid>
      <dc:creator>matthewkendall</dc:creator>
      <dc:date>2014-10-15T19:38:53Z</dc:date>
    </item>
  </channel>
</rss>