<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic NAND Flash File System patch for Freescale MQX buffer size adjustment? in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/NAND-Flash-File-System-patch-for-Freescale-MQX-buffer-size/m-p/254783#M7489</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working with a custom K60 120MHz board we designed that uses the same NAND FLASH as the K60F120M tower board.&amp;nbsp; I added the NAND Flash File system patch to MQX 4.0 and I was able to get the NAND working and can read and write to it.&amp;nbsp; I then added the web server that come with MQX.&amp;nbsp; Now both the web server and the NAND drive work correctly, but will not operate together.&amp;nbsp; I also enable the shell to allow manual control of the initialization. The problem I have Is memory, specifically RAM.&amp;nbsp; If I start my firmware with the NAND uninitialized the web server works correctly. Once I initialize/open the NAND Flash drive, the webserver can no longer allocate enough memory for the RX and TX buffers and stops working.&amp;nbsp; If I close the NAND drive the web server recovers and works correctly.&amp;nbsp; Since the documentation for the NAND Flash file system patch does not explain how the buffer management is handled and configured I can not easily resolve this issue.&amp;nbsp; Is there an unreleased document that can be made available that may speed my understanding of the NAND Flash driver and wear leveling code to save me from reading all the source files and figuring this out myself?&amp;nbsp; Also can the wear leveling code be disabled?&amp;nbsp; My application will not be writing tot he NAND very often so I would be willing to sacrifice wear leveling if it will save me RAM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Frank&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 07 Apr 2013 21:36:40 GMT</pubDate>
    <dc:creator>Frank_D</dc:creator>
    <dc:date>2013-04-07T21:36:40Z</dc:date>
    <item>
      <title>NAND Flash File System patch for Freescale MQX buffer size adjustment?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/NAND-Flash-File-System-patch-for-Freescale-MQX-buffer-size/m-p/254783#M7489</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working with a custom K60 120MHz board we designed that uses the same NAND FLASH as the K60F120M tower board.&amp;nbsp; I added the NAND Flash File system patch to MQX 4.0 and I was able to get the NAND working and can read and write to it.&amp;nbsp; I then added the web server that come with MQX.&amp;nbsp; Now both the web server and the NAND drive work correctly, but will not operate together.&amp;nbsp; I also enable the shell to allow manual control of the initialization. The problem I have Is memory, specifically RAM.&amp;nbsp; If I start my firmware with the NAND uninitialized the web server works correctly. Once I initialize/open the NAND Flash drive, the webserver can no longer allocate enough memory for the RX and TX buffers and stops working.&amp;nbsp; If I close the NAND drive the web server recovers and works correctly.&amp;nbsp; Since the documentation for the NAND Flash file system patch does not explain how the buffer management is handled and configured I can not easily resolve this issue.&amp;nbsp; Is there an unreleased document that can be made available that may speed my understanding of the NAND Flash driver and wear leveling code to save me from reading all the source files and figuring this out myself?&amp;nbsp; Also can the wear leveling code be disabled?&amp;nbsp; My application will not be writing tot he NAND very often so I would be willing to sacrifice wear leveling if it will save me RAM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Frank&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 07 Apr 2013 21:36:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/NAND-Flash-File-System-patch-for-Freescale-MQX-buffer-size/m-p/254783#M7489</guid>
      <dc:creator>Frank_D</dc:creator>
      <dc:date>2013-04-07T21:36:40Z</dc:date>
    </item>
    <item>
      <title>Re: NAND Flash File System patch for Freescale MQX buffer size adjustment?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/NAND-Flash-File-System-patch-for-Freescale-MQX-buffer-size/m-p/254784#M7490</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Frank,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There exists a demo:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; \mqx\examples\nandflash\nandflash_demo.c&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It shows how to use nand flash driver to read and write data in block mode (512 bytes) without wear leveling layer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can imagine a custom load mechanism can be implemented to write TFS data into NAND flash and then customize TFS low level read and write functions to call NAND flash read and write functions, with some sort of simple caching mechanism for 512 bytes. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm sorry I don't have experience with FFS much so I can't advice about its memory consumption at the moment.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;K70 has possibility to interface a large SDRAM, this might be also an option.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Apr 2013 07:14:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/NAND-Flash-File-System-patch-for-Freescale-MQX-buffer-size/m-p/254784#M7490</guid>
      <dc:creator>Martin_</dc:creator>
      <dc:date>2013-04-09T07:14:32Z</dc:date>
    </item>
    <item>
      <title>Re: NAND Flash File System patch for Freescale MQX buffer size adjustment?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/NAND-Flash-File-System-patch-for-Freescale-MQX-buffer-size/m-p/254785#M7491</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Martin,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thanks for the reply but I need to have MFS on top of the NAND driver.&amp;nbsp; My goal is to have the HTTP server retrieve it's data from the NAND drive.&amp;nbsp; I also plan on enabling the FTP server to allow the web page files to be updated.&amp;nbsp; Once I get the memory issue resolved I intend to remove the TFS from the server code I am currently using and sever the pages from the NAND drive. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for pointing me to the nandflach_demo under the MQX examples.&amp;nbsp; I did not notice that example as I was looking at the FFS example which looks like it has wear leveling enabled.&amp;nbsp; I am going to try to disable wear leveling to see if that helps with the memory allocation problem I am experiencing.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Apr 2013 00:40:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/NAND-Flash-File-System-patch-for-Freescale-MQX-buffer-size/m-p/254785#M7491</guid>
      <dc:creator>Frank_D</dc:creator>
      <dc:date>2013-04-10T00:40:29Z</dc:date>
    </item>
    <item>
      <title>Re: NAND Flash File System patch for Freescale MQX buffer size adjustment?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/NAND-Flash-File-System-patch-for-Freescale-MQX-buffer-size/m-p/254786#M7492</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please check your &lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif'; color: #1f497d;"&gt;NUM_OF_MAX_SIZE_NS_SECTORS_MAPS &lt;/SPAN&gt;setting, by default, it is 128, and thus this will consume &lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif'; color: #1f497d;"&gt;NUM_OF_MAX_SIZE_NS_SECTORS_MAPS*&lt;/SPAN&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt; &lt;SPAN style="color: #1f497d;"&gt;(NSSM_BASE_PAGE_PER_BLOCK_COUNT /NumSectorsPerBlock)*sizeof(map_entry)*2 = 128 * 4 * 48 * 2 = 48K&lt;/SPAN&gt;&lt;/SPAN&gt; memory. Please change it&amp;nbsp; to 9, then about 40K mem can be saved.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Apr 2013 03:36:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/NAND-Flash-File-System-patch-for-Freescale-MQX-buffer-size/m-p/254786#M7492</guid>
      <dc:creator>JerryFan</dc:creator>
      <dc:date>2013-04-11T03:36:29Z</dc:date>
    </item>
    <item>
      <title>Re: NAND Flash File System patch for Freescale MQX buffer size adjustment?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/NAND-Flash-File-System-patch-for-Freescale-MQX-buffer-size/m-p/254787#M7493</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Chongbin,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thanks for the suggestion.&amp;nbsp; That did the trick and I now have enough memory to run the webserver and the NAND Flash with MFS without memory allocation issues.&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Apr 2013 21:15:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/NAND-Flash-File-System-patch-for-Freescale-MQX-buffer-size/m-p/254787#M7493</guid>
      <dc:creator>Frank_D</dc:creator>
      <dc:date>2013-04-11T21:15:53Z</dc:date>
    </item>
  </channel>
</rss>