<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to change the IP address when Http server is running? in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-change-the-IP-address-when-Http-server-is-running/m-p/249670#M7188</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I have a GS1500M WiFi tower and TWRK60F120.&lt;/P&gt;&lt;P&gt;In httpsrv demo code IN mqx4.0.2, I can change the &lt;/P&gt;&lt;P&gt;#define ENET_IPADDR&amp;nbsp; IPADDR(192,168,0,1) and &lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; #define A 192&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; #define B 168&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; #define C 0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; #define D 1&lt;/P&gt;&lt;P&gt;to change the IP address of my device.&lt;/P&gt;&lt;P&gt;Now after I configure all the setting for httpsrv and use the HTTPSRV_init function start it, how can I reconfigure the IP address,switch the mode from "adhoc" to "managed"&lt;/P&gt;&lt;P&gt;and restart the HTTPSRV_init? Because by default I want the WiFi device act as a "adhoc" mode, after user finish some configurations through a browser, I can set it back to&lt;/P&gt;&lt;P&gt;"managed" mode. Is there a way to do this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Jan 2014 14:47:21 GMT</pubDate>
    <dc:creator>danielchai</dc:creator>
    <dc:date>2014-01-22T14:47:21Z</dc:date>
    <item>
      <title>How to change the IP address when Http server is running?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-change-the-IP-address-when-Http-server-is-running/m-p/249670#M7188</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I have a GS1500M WiFi tower and TWRK60F120.&lt;/P&gt;&lt;P&gt;In httpsrv demo code IN mqx4.0.2, I can change the &lt;/P&gt;&lt;P&gt;#define ENET_IPADDR&amp;nbsp; IPADDR(192,168,0,1) and &lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; #define A 192&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; #define B 168&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; #define C 0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; #define D 1&lt;/P&gt;&lt;P&gt;to change the IP address of my device.&lt;/P&gt;&lt;P&gt;Now after I configure all the setting for httpsrv and use the HTTPSRV_init function start it, how can I reconfigure the IP address,switch the mode from "adhoc" to "managed"&lt;/P&gt;&lt;P&gt;and restart the HTTPSRV_init? Because by default I want the WiFi device act as a "adhoc" mode, after user finish some configurations through a browser, I can set it back to&lt;/P&gt;&lt;P&gt;"managed" mode. Is there a way to do this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jan 2014 14:47:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-change-the-IP-address-when-Http-server-is-running/m-p/249670#M7188</guid>
      <dc:creator>danielchai</dc:creator>
      <dc:date>2014-01-22T14:47:21Z</dc:date>
    </item>
    <item>
      <title>Re: How to change the IP address when Http server is running?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-change-the-IP-address-when-Http-server-is-running/m-p/249671#M7189</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To unbind an IP address from a device interface, call RTCS_if_unbind()&lt;/P&gt;&lt;P&gt;Description of the RTCS functions can be found in the RTCS Reference Manual. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Sol&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jan 2014 22:53:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-change-the-IP-address-when-Http-server-is-running/m-p/249671#M7189</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2014-01-22T22:53:43Z</dc:date>
    </item>
  </channel>
</rss>