<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックMQX USB problem when writing to SPI registers</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-USB-problem-when-writing-to-SPI-registers/m-p/248498#M7145</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all&lt;/P&gt;&lt;P&gt;I'm using the TWR-K60F120M board with uVision 5 and MQX 4.0.1&lt;/P&gt;&lt;P&gt;I'm trying to send some data over USB that I get from another board I'm talking to via SPI.&lt;/P&gt;&lt;P&gt;Both bits work individually but I've found that whenever I'm writing directly to the registers USB wont work.&lt;/P&gt;&lt;P&gt;I had the same problem when using the LEDS on the board so I just switched to using the MQX GPIO functions.&lt;/P&gt;&lt;P&gt;I have tried MQXs SPI driver and that doesn't seem to work properly as I mentioned in here &lt;A href="https://community.nxp.com/thread/315410"&gt;MQX 4 SPI Problem TWR-K60F120M&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So I'm wondering why can't I use the USB driver and write directly to the registers? Is there any way to do this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 06 Dec 2013 15:07:54 GMT</pubDate>
    <dc:creator>terencet</dc:creator>
    <dc:date>2013-12-06T15:07:54Z</dc:date>
    <item>
      <title>MQX USB problem when writing to SPI registers</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-USB-problem-when-writing-to-SPI-registers/m-p/248498#M7145</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all&lt;/P&gt;&lt;P&gt;I'm using the TWR-K60F120M board with uVision 5 and MQX 4.0.1&lt;/P&gt;&lt;P&gt;I'm trying to send some data over USB that I get from another board I'm talking to via SPI.&lt;/P&gt;&lt;P&gt;Both bits work individually but I've found that whenever I'm writing directly to the registers USB wont work.&lt;/P&gt;&lt;P&gt;I had the same problem when using the LEDS on the board so I just switched to using the MQX GPIO functions.&lt;/P&gt;&lt;P&gt;I have tried MQXs SPI driver and that doesn't seem to work properly as I mentioned in here &lt;A href="https://community.nxp.com/thread/315410"&gt;MQX 4 SPI Problem TWR-K60F120M&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So I'm wondering why can't I use the USB driver and write directly to the registers? Is there any way to do this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Dec 2013 15:07:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-USB-problem-when-writing-to-SPI-registers/m-p/248498#M7145</guid>
      <dc:creator>terencet</dc:creator>
      <dc:date>2013-12-06T15:07:54Z</dc:date>
    </item>
    <item>
      <title>Re: MQX USB problem when writing to SPI registers</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-USB-problem-when-writing-to-SPI-registers/m-p/248499#M7146</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hmm apparently it doesn't work when I'm writing to the LEDs using the GPIO functions as well. Not to sure why it doesn't like playing nice must be some thing odd I'm doing.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Dec 2013 15:56:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-USB-problem-when-writing-to-SPI-registers/m-p/248499#M7146</guid>
      <dc:creator>terencet</dc:creator>
      <dc:date>2013-12-06T15:56:18Z</dc:date>
    </item>
    <item>
      <title>Re: MQX USB problem when writing to SPI registers</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-USB-problem-when-writing-to-SPI-registers/m-p/248500#M7147</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So it looks like the LEDs are using the same port as the ULPI interface (A 10,11,28,19) which would explain why I am having problems there.&lt;/P&gt;&lt;P&gt;It also says in the TWR-SER2 User manual that SPI0 is being used which is the same SPI device that I am trying to use.&lt;/P&gt;&lt;P&gt;Does any one know what it is used by? it doesn't seem to connect to anything on the schematic diagram and doesn't mark anything else in the user guide apart from a mark in the used column.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Dec 2013 10:06:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-USB-problem-when-writing-to-SPI-registers/m-p/248500#M7147</guid>
      <dc:creator>terencet</dc:creator>
      <dc:date>2013-12-09T10:06:57Z</dc:date>
    </item>
    <item>
      <title>Re: MQX USB problem when writing to SPI registers</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-USB-problem-when-writing-to-SPI-registers/m-p/248501#M7148</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok cleared the last piece up it was all to do with the GPIOs I was using. I was using SPI to communicate with a specific chip that I needed to use some GPIOs with to set the mode and such. Turns out that these are being used by the USB on the TWR-SER2 as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So it was the PORTA 10, 11, 28, 19 and PORTB 8, 9 that were causing the problems looks like I'll have to use some other ones but at least I know what it was now.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Dec 2013 11:53:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-USB-problem-when-writing-to-SPI-registers/m-p/248501#M7148</guid>
      <dc:creator>terencet</dc:creator>
      <dc:date>2013-12-09T11:53:52Z</dc:date>
    </item>
  </channel>
</rss>