<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Memory Map Error during compilation - Vybrid Tower in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Memory-Map-Error-during-compilation-Vybrid-Tower/m-p/248072#M7118</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I asked this question over in the Processor Expert (PEx) forum and one of the Freescale guys asked me to post it here.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am able to compile my PEx project without errors and run it on the Vybrid tower under the DS-5 Debugger. I'm using MQX v4.0.2-GA&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, I just added the MQX component to my PEx project and now I get this compile error:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"../Generated_Code/IO_Map.h", line 49: Error:&amp;nbsp; #35: #error directive: MVF61NN151MK50 memory map: There is already included another memory map. Only one memory map can be included."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My project compiled fine before and all I did was add the MQX component; then I got that compile error message. I don't know where another memory map could have been included or where I could begin looking for this other memory map.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm finding that IO_Map.h (generated code) and MVF50GS10MK50.h (part of the BSP) collide in their memory maps when the MQX component is added to a PEx project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this a bug? Or am I not configuring this correctly?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone help?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, the online Help for the MQX component says "Vector table is not generated. All interrupt service routines (ISR) are installed through RTOS.", but the vector_table[] array is generated in Generated_Code/Vectors.c and is populated with the interrupt for the serial port I'm using. I found in AS1.c, that PEx is making the call to _int_install_isr() for the AS1 ISR installation into MQX. So that seems to be working ok, but it's still generating the vector table, too. Is that a bug?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is the original discussion: &lt;A href="https://community.nxp.com/message/374320"&gt;Re: Memory Map Error during compilation - Vybrid Tower&lt;/A&gt; .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Jan 2014 01:42:17 GMT</pubDate>
    <dc:creator>jackblather</dc:creator>
    <dc:date>2014-01-22T01:42:17Z</dc:date>
    <item>
      <title>Memory Map Error during compilation - Vybrid Tower</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Memory-Map-Error-during-compilation-Vybrid-Tower/m-p/248072#M7118</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I asked this question over in the Processor Expert (PEx) forum and one of the Freescale guys asked me to post it here.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am able to compile my PEx project without errors and run it on the Vybrid tower under the DS-5 Debugger. I'm using MQX v4.0.2-GA&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, I just added the MQX component to my PEx project and now I get this compile error:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"../Generated_Code/IO_Map.h", line 49: Error:&amp;nbsp; #35: #error directive: MVF61NN151MK50 memory map: There is already included another memory map. Only one memory map can be included."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My project compiled fine before and all I did was add the MQX component; then I got that compile error message. I don't know where another memory map could have been included or where I could begin looking for this other memory map.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm finding that IO_Map.h (generated code) and MVF50GS10MK50.h (part of the BSP) collide in their memory maps when the MQX component is added to a PEx project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this a bug? Or am I not configuring this correctly?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone help?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, the online Help for the MQX component says "Vector table is not generated. All interrupt service routines (ISR) are installed through RTOS.", but the vector_table[] array is generated in Generated_Code/Vectors.c and is populated with the interrupt for the serial port I'm using. I found in AS1.c, that PEx is making the call to _int_install_isr() for the AS1 ISR installation into MQX. So that seems to be working ok, but it's still generating the vector table, too. Is that a bug?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is the original discussion: &lt;A href="https://community.nxp.com/message/374320"&gt;Re: Memory Map Error during compilation - Vybrid Tower&lt;/A&gt; .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jan 2014 01:42:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Memory-Map-Error-during-compilation-Vybrid-Tower/m-p/248072#M7118</guid>
      <dc:creator>jackblather</dc:creator>
      <dc:date>2014-01-22T01:42:17Z</dc:date>
    </item>
    <item>
      <title>Re: Memory Map Error during compilation - Vybrid Tower</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Memory-Map-Error-during-compilation-Vybrid-Tower/m-p/248073#M7119</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;Hi Jack,&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;the MQX and ProcessorExpert is supported just on Kinetis and ColdFire+ platforms and there are no plans to support Vybrid.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;regards Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jan 2014 14:34:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Memory-Map-Error-during-compilation-Vybrid-Tower/m-p/248073#M7119</guid>
      <dc:creator>petr_uhlir</dc:creator>
      <dc:date>2014-01-22T14:34:51Z</dc:date>
    </item>
  </channel>
</rss>