<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software Solutions中的主题 PCB-based SPI driver needed for IPC on Kinetis</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/PCB-based-SPI-driver-needed-for-IPC-on-Kinetis/m-p/247367#M7081</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've developed a solution using the IPC component to connect 2 Kinetis processors using a NULL-modem connection. Now I need to reconfigure this setup to use SPI (one Kinetis in master and the other one in slave mode) and for that I need a PCB-based SPI driver capable of using master and slave mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone tell me if this driver is available and where to find it. If it is nog available (and I have to develop it myself) can anyone direct me to a good starting place for developing PCB-based drivers?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If PCB-based is not really an option I can also develop my own mechanism for the IPC protocol implementation. For that I also need a good starting point.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone help me to get on track?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ralph.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Sep 2013 07:35:56 GMT</pubDate>
    <dc:creator>ralphmaas</dc:creator>
    <dc:date>2013-09-24T07:35:56Z</dc:date>
    <item>
      <title>PCB-based SPI driver needed for IPC on Kinetis</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/PCB-based-SPI-driver-needed-for-IPC-on-Kinetis/m-p/247367#M7081</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've developed a solution using the IPC component to connect 2 Kinetis processors using a NULL-modem connection. Now I need to reconfigure this setup to use SPI (one Kinetis in master and the other one in slave mode) and for that I need a PCB-based SPI driver capable of using master and slave mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone tell me if this driver is available and where to find it. If it is nog available (and I have to develop it myself) can anyone direct me to a good starting place for developing PCB-based drivers?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If PCB-based is not really an option I can also develop my own mechanism for the IPC protocol implementation. For that I also need a good starting point.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone help me to get on track?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ralph.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Sep 2013 07:35:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/PCB-based-SPI-driver-needed-for-IPC-on-Kinetis/m-p/247367#M7081</guid>
      <dc:creator>ralphmaas</dc:creator>
      <dc:date>2013-09-24T07:35:56Z</dc:date>
    </item>
  </channel>
</rss>