<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックRe: Installing an MQX driver - i2c</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Installing-an-MQX-driver-i2c/m-p/154726#M705</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Robert,&lt;BR /&gt;&lt;BR /&gt;I might suggest a couple of options - given I've recently shared your pain with MQX &amp;amp; I2C!&lt;BR /&gt;First: get an O'Scope on your SDA &amp;amp; SCL lines. This gives you that warm fuzzy feeling you are really connected to something&lt;/P&gt;&lt;P&gt;Second: read the manual (I found one online here &lt;A href="http://www.jameco.com/Jameco/Products/ProdDS/2109667.pdf" rel="nofollow" target="_blank"&gt;http://www.jameco.com/Jameco/Products/ProdDS/2109667.pdf&lt;/A&gt;﻿) and it does describe the I2C protocol. Is your HW setting CS high so I2C is enabled?&lt;/P&gt;&lt;P&gt;third: remember it's 7 bit device addressing...&lt;/P&gt;&lt;P&gt;fourth, write the code so that the initialisation ends, you STOP the device (pretty important)!&lt;/P&gt;&lt;P&gt;fifth: when you write a packet to the device do you see the data transferred on the O'scope... oh I mentioned that already :smileywink:&lt;/P&gt;&lt;P&gt;sixth: does it work in polling or interupt mod?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Lemme know if you get it working - and then if you can use the Interrupts!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 29 Aug 2011 18:31:57 GMT</pubDate>
    <dc:creator>easybreather</dc:creator>
    <dc:date>2011-08-29T18:31:57Z</dc:date>
    <item>
      <title>Installing an MQX driver - i2c</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Installing-an-MQX-driver-i2c/m-p/154724#M703</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The doc set says that the i2c driver if enabled in the user_config.h file, may be installed in the BSP or application code. I can't see how to do either. When I do an&amp;nbsp;install for cw10.1, mqx, 51jm128 as per the doc set and source files using&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; _mcf51xx_i2c_polled_install("i2c0:", &amp;amp;_bsp_i2c0_init);&lt;/P&gt;&lt;P&gt;I get compile errors following on the next line of code. The address of the init structure is &amp;amp;_bsp_i2c0_init, and is from the board specific source file init_i2c.c, in that file we can see the structure. I added this to the build but still get errors. I tried moving the structure declaration to the function and get errors in compiling.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;At this point we can't even get the app to compile. I have gone through the eeprom demo but that doesn't do it for us. I don't see how to change the structures and we need lower level api access as well for accelerometers and gyros.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have read through all the doc sets and forums but can't find anything on installing drivers other than general guide lines and references.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any starting point would be appreciated. Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Jul 2011 03:36:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Installing-an-MQX-driver-i2c/m-p/154724#M703</guid>
      <dc:creator>Cdn_aye</dc:creator>
      <dc:date>2011-07-29T03:36:04Z</dc:date>
    </item>
    <item>
      <title>Re: Installing an MQX driver - i2c</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Installing-an-MQX-driver-i2c/m-p/154725#M704</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is the code I have for sending reading a character from the MMA7455 i2c accelerometer. I need to do the usual which is to send the slave address wait for the ACK, then send the register start address in the MMA7455 to read from. This all works under CW6.3 without MQX, I can't get the driver to work under CW10.1 and MQX.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The write hangs and I am not sure if the IO_IOCTL_I2C_SET_DESTINATION_ADDRESS is sent out by the driver or not since I always get a 0 on the read result and a read buffer of zeros. We need to read 20 characters to verify the device. If we implement a fwrite the code just hangs, probably waiting on an ACK.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There is something wrong with the basic concept but I can't figure it out from the example code. Any help would be appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;/*FUNCTION*-----------------------------------------------------------------------------------------&lt;BR /&gt;(((((((((((((((((((((((((((((((((( I2C_Task )))))))))))))))))))))))))))))))))))&lt;BR /&gt;----------------------------------------------------------------------------------------------------&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; vFn_i2c_test&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; test driver fcn&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Input Parameter:&amp;nbsp;&amp;nbsp;&amp;nbsp; void&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Return Type:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; none&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Notes:&lt;BR /&gt;--------------------------------------------------------------------------------------------------*/&lt;BR /&gt;void I2C_task(uint_32)&lt;BR /&gt;{&lt;BR /&gt;MQX_FILE_PTR&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fd;&lt;BR /&gt;uint_32&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; param, result;&lt;BR /&gt;I2C_STATISTICS_STRUCT&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; stats;&lt;BR /&gt;uchar_ptr&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; recv_buffer;&lt;BR /&gt;uint8&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; buffer[30];&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Allocate receive buffer */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; recv_buffer = _mem_alloc_zero (RECV_BUFFER_SIZE);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (recv_buffer == NULL){&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf ("ERROR getting receive buffer!\n");&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; _task_block ();&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Open the I2C driver */&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fd = fopen ("i2c0:", NULL);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (fd == NULL){&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf ("ERROR opening the I2C driver!\n");&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; _time_delay (200L);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; _mqx_exit (1L);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Test ioctl commands */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; param = 100000;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (I2C_OK != ioctl (fd, IO_IOCTL_I2C_SET_BAUD, &amp;amp;param)){&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Set current baud rate to param&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf ("ERROR\n");&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (I2C_OK != ioctl (fd, IO_IOCTL_I2C_SET_MASTER_MODE, NULL)){&amp;nbsp; // printf ("Set master mode ... ");&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf ("OK\n");&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; param = 0x69;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // slave address of accelerometer&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (I2C_OK != ioctl (fd, IO_IOCTL_I2C_SET_STATION_ADDRESS, &amp;amp;param)){ // printf ("Set destination address to 0x%02x ... ", param);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf ("ERROR\n");&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; param = 0x00;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (I2C_OK != ioctl (fd, IO_IOCTL_I2C_SET_DESTINATION_ADDRESS, &amp;amp;param)){&amp;nbsp; // printf ("Set destination address to 0x%02x ... ", param);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf ("ERROR\n");&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Test request 1 byte, read 1 byte */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; param = 20;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (I2C_OK != ioctl (fd, IO_IOCTL_I2C_SET_RX_REQUEST, &amp;amp;param)){&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // printf ("Test request 1 byte, read 1 byte ... ");&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf ("\n&amp;nbsp; ERROR during set rx request\n");&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; result = fread (&amp;amp;buffer, 1, 1, fd);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (I2C_OK != ioctl (fd, IO_IOCTL_FLUSH_OUTPUT, &amp;amp;param)){&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf ("\n&amp;nbsp; ERROR during flush\n");&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (I2C_OK != ioctl (fd, IO_IOCTL_I2C_STOP, NULL)){&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf ("\n&amp;nbsp; ERROR during stop\n");&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; _task_block();&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 27 Aug 2011 00:27:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Installing-an-MQX-driver-i2c/m-p/154725#M704</guid>
      <dc:creator>Cdn_aye</dc:creator>
      <dc:date>2011-08-27T00:27:20Z</dc:date>
    </item>
    <item>
      <title>Re: Installing an MQX driver - i2c</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Installing-an-MQX-driver-i2c/m-p/154726#M705</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Robert,&lt;BR /&gt;&lt;BR /&gt;I might suggest a couple of options - given I've recently shared your pain with MQX &amp;amp; I2C!&lt;BR /&gt;First: get an O'Scope on your SDA &amp;amp; SCL lines. This gives you that warm fuzzy feeling you are really connected to something&lt;/P&gt;&lt;P&gt;Second: read the manual (I found one online here &lt;A href="http://www.jameco.com/Jameco/Products/ProdDS/2109667.pdf" rel="nofollow" target="_blank"&gt;http://www.jameco.com/Jameco/Products/ProdDS/2109667.pdf&lt;/A&gt;﻿) and it does describe the I2C protocol. Is your HW setting CS high so I2C is enabled?&lt;/P&gt;&lt;P&gt;third: remember it's 7 bit device addressing...&lt;/P&gt;&lt;P&gt;fourth, write the code so that the initialisation ends, you STOP the device (pretty important)!&lt;/P&gt;&lt;P&gt;fifth: when you write a packet to the device do you see the data transferred on the O'scope... oh I mentioned that already :smileywink:&lt;/P&gt;&lt;P&gt;sixth: does it work in polling or interupt mod?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Lemme know if you get it working - and then if you can use the Interrupts!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Aug 2011 18:31:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Installing-an-MQX-driver-i2c/m-p/154726#M705</guid>
      <dc:creator>easybreather</dc:creator>
      <dc:date>2011-08-29T18:31:57Z</dc:date>
    </item>
    <item>
      <title>Re: Installing an MQX driver - i2c</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Installing-an-MQX-driver-i2c/m-p/154727#M706</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Robert,&lt;/P&gt;&lt;P&gt;Probably the reason is that the fwrite call is missing.&lt;/P&gt;&lt;P&gt;There is an example in file Freescale MQX 3.7\mqx\examples\i2c﻿\eeprom_int.c in function&amp;nbsp;i2c_read_eeprom_interrupt﻿().&lt;/P&gt;&lt;P&gt;I modified that to read/write IO-expander, it works OK.&lt;/P&gt;&lt;P&gt;~Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Aug 2011 23:53:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Installing-an-MQX-driver-i2c/m-p/154727#M706</guid>
      <dc:creator>MarkP_</dc:creator>
      <dc:date>2011-08-29T23:53:21Z</dc:date>
    </item>
  </channel>
</rss>