<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic lwtimer callback function each 70us in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/lwtimer-callback-function-each-70us/m-p/244109#M6928</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all&lt;/P&gt;&lt;P&gt;it is possible to have a callback function called each 70us interval with the lwtimer or using some others mqx timers ?&lt;/P&gt;&lt;P&gt;if yes, which are the configuration to make in order to arrive at that&amp;nbsp; result, i was thinking to change the Bsp time resolution from 200 to 1000(maximum) which is only one ms for the periodic timer ????&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can some please advise/help me&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thx in advance&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wilson&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Mar 2013 09:22:30 GMT</pubDate>
    <dc:creator>Garil</dc:creator>
    <dc:date>2013-03-28T09:22:30Z</dc:date>
    <item>
      <title>lwtimer callback function each 70us</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/lwtimer-callback-function-each-70us/m-p/244109#M6928</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all&lt;/P&gt;&lt;P&gt;it is possible to have a callback function called each 70us interval with the lwtimer or using some others mqx timers ?&lt;/P&gt;&lt;P&gt;if yes, which are the configuration to make in order to arrive at that&amp;nbsp; result, i was thinking to change the Bsp time resolution from 200 to 1000(maximum) which is only one ms for the periodic timer ????&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can some please advise/help me&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thx in advance&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wilson&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Mar 2013 09:22:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/lwtimer-callback-function-each-70us/m-p/244109#M6928</guid>
      <dc:creator>Garil</dc:creator>
      <dc:date>2013-03-28T09:22:30Z</dc:date>
    </item>
    <item>
      <title>Re: lwtimer callback function each 70us</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/lwtimer-callback-function-each-70us/m-p/244110#M6929</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi wilson,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;New release 4.0.1 of MQX is coming with a new timer driver called hwtimer. This driver supports PIT timer and Systick and it is available only for kinetis platforms.&lt;/P&gt;&lt;P&gt;But for your required time 70us there is big overhead inside OS. You should create your own minimalism driver (PIT for example) with interrupt routine out off MQX.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bielik Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Mar 2013 16:50:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/lwtimer-callback-function-each-70us/m-p/244110#M6929</guid>
      <dc:creator>BielikM</dc:creator>
      <dc:date>2013-03-28T16:50:12Z</dc:date>
    </item>
  </channel>
</rss>