<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Target request failed: Failed to step, An error occurred while trying to Step in target. in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Target-request-failed-Failed-to-step-An-error-occurred-while/m-p/243958#M6926</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I figure it out. Because the ttya in the library is mapped to PTA1 and PTA2 which are also used for JTAG on my board. &lt;/P&gt;&lt;P&gt;I need to reconfigure the pin for it and it works.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Aug 2013 15:51:12 GMT</pubDate>
    <dc:creator>danielchai</dc:creator>
    <dc:date>2013-08-07T15:51:12Z</dc:date>
    <item>
      <title>Target request failed: Failed to step, An error occurred while trying to Step in target.</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Target-request-failed-Failed-to-step-An-error-occurred-while/m-p/243957#M6925</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I ported the BSP from K60F120M to my target board. I want to try the UART communication using MQX RTOS.&lt;/P&gt;&lt;P&gt;But when I try to debug it, it always gives me lost connection&amp;nbsp; error. &lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/40261iD2BDBB67E3C58B35/image-size/large?v=v2&amp;amp;px=999" title="p1.png" alt="p1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;When I try to step in it and find which part cause this problem, at first step(when try to disable interrupt and clear flags), it gives me error:&lt;/P&gt;&lt;P&gt;"Target request failed: Failed to step, An error occurred while trying to Step in target."&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/40262i8AB82BE375C8F104/image-size/large?v=v2&amp;amp;px=999" title="p2.png" alt="p2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I checked my debugger setting, it is already set to disable interrupt when stepping.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/40263i9D1CA857C407C776/image-size/large?v=v2&amp;amp;px=999" title="p3.png" alt="p3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Any advices will be appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;-Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Aug 2013 12:47:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Target-request-failed-Failed-to-step-An-error-occurred-while/m-p/243957#M6925</guid>
      <dc:creator>danielchai</dc:creator>
      <dc:date>2013-08-07T12:47:39Z</dc:date>
    </item>
    <item>
      <title>Re: Target request failed: Failed to step, An error occurred while trying to Step in target.</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Target-request-failed-Failed-to-step-An-error-occurred-while/m-p/243958#M6926</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I figure it out. Because the ttya in the library is mapped to PTA1 and PTA2 which are also used for JTAG on my board. &lt;/P&gt;&lt;P&gt;I need to reconfigure the pin for it and it works.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Aug 2013 15:51:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Target-request-failed-Failed-to-step-An-error-occurred-while/m-p/243958#M6926</guid>
      <dc:creator>danielchai</dc:creator>
      <dc:date>2013-08-07T15:51:12Z</dc:date>
    </item>
  </channel>
</rss>