<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックHID USB Communication Failing after exactly 31 sends.</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/HID-USB-Communication-Failing-after-exactly-31-sends/m-p/243004#M6879</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using MQX 4.0 and I'm having an issue with the USB HID communication trying to send data. My HID layout is a modification of the HID Class driver that's built in, different only that I also need to read data were as the base HID class doesn't perform that. What my issue is, is that when I send data from my hardware (K60F120) after exactly 31 transactions I get an error from the USB_Class_Send_Data() which is transfer in progress. I was told to use the _usb_device_free_XD() but I can't find any documentation on how I'm suppose to use. I'm hoping someone might know of a solution to this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Aug 2013 01:00:45 GMT</pubDate>
    <dc:creator>Dealerz</dc:creator>
    <dc:date>2013-08-07T01:00:45Z</dc:date>
    <item>
      <title>HID USB Communication Failing after exactly 31 sends.</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/HID-USB-Communication-Failing-after-exactly-31-sends/m-p/243004#M6879</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using MQX 4.0 and I'm having an issue with the USB HID communication trying to send data. My HID layout is a modification of the HID Class driver that's built in, different only that I also need to read data were as the base HID class doesn't perform that. What my issue is, is that when I send data from my hardware (K60F120) after exactly 31 transactions I get an error from the USB_Class_Send_Data() which is transfer in progress. I was told to use the _usb_device_free_XD() but I can't find any documentation on how I'm suppose to use. I'm hoping someone might know of a solution to this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Aug 2013 01:00:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/HID-USB-Communication-Failing-after-exactly-31-sends/m-p/243004#M6879</guid>
      <dc:creator>Dealerz</dc:creator>
      <dc:date>2013-08-07T01:00:45Z</dc:date>
    </item>
    <item>
      <title>Re: HID USB Communication Failing after exactly 31 sends.</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/HID-USB-Communication-Failing-after-exactly-31-sends/m-p/243005#M6880</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;With MQX 4.0 on a K21. When I make the call to USB_Class_Send_Data() I get and error code of 0x03 (USB_STATUS_TRANSFER_IN_PROGRESS). I was told I had to call _usb_device_free_XD() but wasn't given a place on where or how to make this function call. This happens on the 31st transmission. How do I resolve this, has anybody else ever seen this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Sep 2013 22:13:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/HID-USB-Communication-Failing-after-exactly-31-sends/m-p/243005#M6880</guid>
      <dc:creator>Dealerz</dc:creator>
      <dc:date>2013-09-09T22:13:33Z</dc:date>
    </item>
  </channel>
</rss>