<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Best Place to add external SRAM in MQX in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Best-Place-to-add-external-SRAM-in-MQX/m-p/232745#M6373</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I modified code to configure the bus and set up the SRAM in '_bsp_flexbus_setup()'.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Where is the best place to add to the memory pool?&amp;nbsp; I'm thinking in _bsp_card_enable() before _bsp_low_level_init().&amp;nbsp; Any suggestions?&amp;nbsp; Is the memory added with _mem_extend_pool()?&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, the pool I'm adding is 16-bit external memory vs the existing 32-bit internal memory.&amp;nbsp; Do I want the external memory at a higher address so the 32-bit memory is prioritized ahead of the 16-bit memory?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;PMT &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 May 2013 15:12:36 GMT</pubDate>
    <dc:creator>pmt</dc:creator>
    <dc:date>2013-05-14T15:12:36Z</dc:date>
    <item>
      <title>Best Place to add external SRAM in MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Best-Place-to-add-external-SRAM-in-MQX/m-p/232743#M6371</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am modifying a base BSP (K60F120 tower) for our custom board.&amp;nbsp; Our board has external SRAM hanging off the flexbus.&amp;nbsp; What is the proper place to initialize and add this SRAM into the PSP/BSP?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can guess two options: &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; - Linker does not target this external SRAM and it is only used as an MQX memory pool&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; - Linker targets external SRAM and it needs to be initialized by the debugger (during debug), or by startup code before C-initialization is called.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For these two situations what are my target files for modification?&amp;nbsp; Boot.s, init_bsp.c, etc?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;PMT&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 May 2013 18:11:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Best-Place-to-add-external-SRAM-in-MQX/m-p/232743#M6371</guid>
      <dc:creator>pmt</dc:creator>
      <dc:date>2013-05-09T18:11:22Z</dc:date>
    </item>
    <item>
      <title>Re: Best Place to add external SRAM in MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Best-Place-to-add-external-SRAM-in-MQX/m-p/232744#M6372</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you use the external SRAM as a MQX memory pool, then the linker has no need to know the infor about the external SRAM.&lt;/P&gt;&lt;P&gt;you can refer _bsp_flexbus_mram_setup in the mqx\source\bsp\twrk60f120m\init_hw.c for detail.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 May 2013 08:02:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Best-Place-to-add-external-SRAM-in-MQX/m-p/232744#M6372</guid>
      <dc:creator>JerryFan</dc:creator>
      <dc:date>2013-05-10T08:02:02Z</dc:date>
    </item>
    <item>
      <title>Re: Best Place to add external SRAM in MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Best-Place-to-add-external-SRAM-in-MQX/m-p/232745#M6373</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I modified code to configure the bus and set up the SRAM in '_bsp_flexbus_setup()'.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Where is the best place to add to the memory pool?&amp;nbsp; I'm thinking in _bsp_card_enable() before _bsp_low_level_init().&amp;nbsp; Any suggestions?&amp;nbsp; Is the memory added with _mem_extend_pool()?&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, the pool I'm adding is 16-bit external memory vs the existing 32-bit internal memory.&amp;nbsp; Do I want the external memory at a higher address so the 32-bit memory is prioritized ahead of the 16-bit memory?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;PMT &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 May 2013 15:12:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Best-Place-to-add-external-SRAM-in-MQX/m-p/232745#M6373</guid>
      <dc:creator>pmt</dc:creator>
      <dc:date>2013-05-14T15:12:36Z</dc:date>
    </item>
    <item>
      <title>Re: Best Place to add external SRAM in MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Best-Place-to-add-external-SRAM-in-MQX/m-p/232746#M6374</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The only reqirement about the externl pool is that it must be added before used(malloc, free), so _bsp_card_enable() is a good option.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;_mem_extend will add the extenal sram to the kernel default pool, as a free block, at the beginning of the free block list. So all the mem allocation on the kernel pool will select the external sram firstly.&lt;/P&gt;&lt;P&gt;Another option is _mem_create_pool() to create a new pool, then you can select which pool to malloc.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 May 2013 02:15:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Best-Place-to-add-external-SRAM-in-MQX/m-p/232746#M6374</guid>
      <dc:creator>JerryFan</dc:creator>
      <dc:date>2013-05-15T02:15:15Z</dc:date>
    </item>
    <item>
      <title>Re: Best Place to add external SRAM in MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Best-Place-to-add-external-SRAM-in-MQX/m-p/232747#M6375</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;And demo for the _mem_extend and &lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 12.727272033691406px; background-color: #ffffff;"&gt;_mem_create_poo&lt;/SPAN&gt;:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_text_macro jive_macro_code _jivemacro_uid_13685958436125067" jivemacro_uid="_13685958436125067"&gt;
&lt;P align="left" class="Code"&gt;int32_t test1(void)&lt;/P&gt;
&lt;P align="left" class="Code"&gt;{&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; pointer test_buf = NULL;&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp; &lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if(MQX_OK != _mem_verify(BSP_EXTERNAL_MRAM_RAM_BASE,&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (pointer)((uint_32)BSP_EXTERNAL_MRAM_RAM_BASE + BSP_EXTERNAL_MRAM_RAM_SIZE))){&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf("The external sram failed to be verified.\n");&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; return -1;&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }else{&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf("The external sram verified.\n");&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp; &lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp; if(MQX_OK != _mem_extend(BSP_EXTERNAL_MRAM_RAM_BASE, (_mem_size)BSP_EXTERNAL_MRAM_RAM_SIZE)){&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf("Failed to extend the external SRAM.\n");&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; r;&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }else{&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf("Added the external sram to default mem pool.\n");&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp; &lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if(NULL == (test_buf = _mem_alloc(EXTERNAL_SRAM_TEST_BUF_SZ))){&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf("Failed to alloc buffer in the default pool after it being extended.\n");&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; return -1;&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }else{&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf("Buffer allocated its address is 0x%08x\n", (uint_32)test_buf);&lt;/P&gt;
&lt;P align="left" class="Code"&gt;}&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp; &lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Access the buf here */&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; _task_block();&amp;nbsp; //block here to easy the checking of the memory pool&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; _mem_free(test_buf);&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; return 0;&lt;/P&gt;
&lt;P align="left" class="Code"&gt;}&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&lt;/P&gt;
&lt;P align="left" class="Code"&gt;int32_t test2(void)&lt;/P&gt;
&lt;P align="left" class="Code"&gt;{&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; pointer test_buf = NULL;&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp; &lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if(MQX_OK != _mem_verify(BSP_EXTERNAL_MRAM_RAM_BASE,&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (pointer)((uint_32)BSP_EXTERNAL_MRAM_RAM_BASE + BSP_EXTERNAL_MRAM_RAM_SIZE))){&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf("The external sram failed to be verified.\n");&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; return -1;&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }else{&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf("The external sram verified.\n");&lt;/P&gt;
&lt;P align="left" class="Code"&gt;}&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&lt;/P&gt;
&lt;P align="left" class="Code"&gt;_mem_pool_id ext_sram_pool = NULL;&lt;/P&gt;
&lt;P align="left" class="Code"&gt;ext_sram_pool = _mem_create_pool(BSP_EXTERNAL_MRAM_RAM_BASE, (_mem_size)BSP_EXTERNAL_MRAM_RAM_SIZE);&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf("Created a mem pool on the external sram, and the pool id is 0x%08x.\n", ext_sram_pool);&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp; &lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if(NULL == (test_buf = _mem_alloc_from(ext_sram_pool, EXTERNAL_SRAM_TEST_BUF_SZ))){&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf("Failed to alloc buffer from the new memory pool.\n");&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; return -1;&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }else{&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf("Buffer allocated and its address is 0x%08x\n", (uint_32)test_buf);&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp; /* Access the buf here */&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; _task_block();&amp;nbsp; //block here to easy the checking of the memory pool&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&lt;/P&gt;
&lt;P align="left" class="Code"&gt;_mem_free(test_buf);&lt;/P&gt;
&lt;P align="left" class="Code"&gt;&lt;/P&gt;
&lt;P align="left" class="Code"&gt;return 0;&lt;/P&gt;
&lt;P align="left" class="Code"&gt;}&lt;/P&gt;
&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 May 2013 02:20:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Best-Place-to-add-external-SRAM-in-MQX/m-p/232747#M6375</guid>
      <dc:creator>JerryFan</dc:creator>
      <dc:date>2013-05-15T02:20:26Z</dc:date>
    </item>
    <item>
      <title>Re: Best Place to add external SRAM in MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Best-Place-to-add-external-SRAM-in-MQX/m-p/232748#M6376</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good stuff.&amp;nbsp; Thanks Chongbin!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PMT&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 May 2013 19:50:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Best-Place-to-add-external-SRAM-in-MQX/m-p/232748#M6376</guid>
      <dc:creator>pmt</dc:creator>
      <dc:date>2013-05-15T19:50:26Z</dc:date>
    </item>
    <item>
      <title>Re: Best Place to add external SRAM in MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Best-Place-to-add-external-SRAM-in-MQX/m-p/232749#M6377</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Chongbin / All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did run into some issues.&amp;nbsp; My default BSP defines MQX_USE_LWMEM_ALLOCATOR by default.&amp;nbsp; Some the of documentation in the Users Manual is still kind of light with the LWMEM components, but it looks like the light weight mem does not support "extend"ing non-contiguous memory blocks.&amp;nbsp; My goals is to have the core services malloc(), free(), etc be able to take from the appended memory block.&amp;nbsp; So this will not be able to be done with the lightweight mem components.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So am I best undefining the LWMEM components, and using the standard memory components?&amp;nbsp; When I do this in the BSP I am running into other issues with unhandled interrupts, perhaps due to the initial tight memory footprint.&amp;nbsp; Any advice?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PMT&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 May 2013 13:51:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Best-Place-to-add-external-SRAM-in-MQX/m-p/232749#M6377</guid>
      <dc:creator>pmt</dc:creator>
      <dc:date>2013-05-16T13:51:24Z</dc:date>
    </item>
  </channel>
</rss>