<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックRe: Example for using the basic printer class?</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Example-for-using-the-basic-printer-class/m-p/229800#M6238</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Just a quick update on this one - a Freescale rep suggested looking at the bare metal Freescale USB Stack for an example of printer support.&amp;nbsp; The USB Stack supports USB printers and does have an example.&amp;nbsp; I loaded the printer example into a tower system and (with a few code additions) it is able to print to a Godex DT2 printer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am now in the process of porting the printer example over to my MQX project.&amp;nbsp;&amp;nbsp; Has anyone attempted this already?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will update this thread again when I get further along.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For what it's worth - my MQX project is already working with USB keyboards and USB flash drives.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Mar 2014 14:29:17 GMT</pubDate>
    <dc:creator>gorakk</dc:creator>
    <dc:date>2014-03-11T14:29:17Z</dc:date>
    <item>
      <title>Example for using the basic printer class?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Example-for-using-the-basic-printer-class/m-p/229799#M6237</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there a sample application for using the USB host printer class?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have CodeWarrior 10.3 and MQX 4.0 installed.&amp;nbsp; There are examples for USB keyboard, mouse, etc but none for printer that I can see.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Nov 2013 20:00:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Example-for-using-the-basic-printer-class/m-p/229799#M6237</guid>
      <dc:creator>gorakk</dc:creator>
      <dc:date>2013-11-26T20:00:19Z</dc:date>
    </item>
    <item>
      <title>Re: Example for using the basic printer class?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Example-for-using-the-basic-printer-class/m-p/229800#M6238</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Just a quick update on this one - a Freescale rep suggested looking at the bare metal Freescale USB Stack for an example of printer support.&amp;nbsp; The USB Stack supports USB printers and does have an example.&amp;nbsp; I loaded the printer example into a tower system and (with a few code additions) it is able to print to a Godex DT2 printer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am now in the process of porting the printer example over to my MQX project.&amp;nbsp;&amp;nbsp; Has anyone attempted this already?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will update this thread again when I get further along.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For what it's worth - my MQX project is already working with USB keyboards and USB flash drives.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Mar 2014 14:29:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Example-for-using-the-basic-printer-class/m-p/229800#M6238</guid>
      <dc:creator>gorakk</dc:creator>
      <dc:date>2014-03-11T14:29:17Z</dc:date>
    </item>
  </channel>
</rss>