<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックLink fails while using TSS Library on TWRK40X256</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Link-fails-while-using-TSS-Library-on-TWRK40X256/m-p/229423#M6228</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I try to include the TSS capabilities of the TWRK40X256 board (Touch Electrodes) into an application.&lt;/P&gt;&lt;P&gt;The TSS example compiles and works as intended.&lt;/P&gt;&lt;P&gt;When I use the same code from the example in my own application I get some weird errors in my BSP project about missing definitions. I can't figure out what I missed while porting the example. The references to /lib/twrk40x256.cw10/debug/bsb/tss exist.&lt;/P&gt;&lt;P&gt;I attached a screenshot with the code that causes the errors and the error list.&lt;/P&gt;&lt;P&gt;I use CodeWarrior 10.2 with MQX 4.0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for any help&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 18 Mar 2013 13:50:37 GMT</pubDate>
    <dc:creator>friederschrempf</dc:creator>
    <dc:date>2013-03-18T13:50:37Z</dc:date>
    <item>
      <title>Link fails while using TSS Library on TWRK40X256</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Link-fails-while-using-TSS-Library-on-TWRK40X256/m-p/229423#M6228</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I try to include the TSS capabilities of the TWRK40X256 board (Touch Electrodes) into an application.&lt;/P&gt;&lt;P&gt;The TSS example compiles and works as intended.&lt;/P&gt;&lt;P&gt;When I use the same code from the example in my own application I get some weird errors in my BSP project about missing definitions. I can't figure out what I missed while porting the example. The references to /lib/twrk40x256.cw10/debug/bsb/tss exist.&lt;/P&gt;&lt;P&gt;I attached a screenshot with the code that causes the errors and the error list.&lt;/P&gt;&lt;P&gt;I use CodeWarrior 10.2 with MQX 4.0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for any help&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Mar 2013 13:50:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Link-fails-while-using-TSS-Library-on-TWRK40X256/m-p/229423#M6228</guid>
      <dc:creator>friederschrempf</dc:creator>
      <dc:date>2013-03-18T13:50:37Z</dc:date>
    </item>
    <item>
      <title>Re: Link fails while using TSS Library on TWRK40X256</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Link-fails-while-using-TSS-Library-on-TWRK40X256/m-p/229424#M6229</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Frieder Schrempf,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can you compare linker path settings with the original HMI application (in your monitor application). Are all paths same set ?&lt;/P&gt;&lt;P&gt;It would help you paste them here, linker settings in your application. BSP does not include TSS library, the application's linker must resolve all symbols.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MartinK&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Mar 2013 14:56:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Link-fails-while-using-TSS-Library-on-TWRK40X256/m-p/229424#M6229</guid>
      <dc:creator>c0170</dc:creator>
      <dc:date>2013-03-18T14:56:57Z</dc:date>
    </item>
    <item>
      <title>Re: Link fails while using TSS Library on TWRK40X256</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Link-fails-while-using-TSS-Library-on-TWRK40X256/m-p/229425#M6230</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the quick help!&lt;/P&gt;&lt;P&gt;I did not know that the library has to be added manually.&lt;/P&gt;&lt;P&gt;After including "tss.a" in the Linker settings everything worked.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Mar 2013 15:21:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Link-fails-while-using-TSS-Library-on-TWRK40X256/m-p/229425#M6230</guid>
      <dc:creator>friederschrempf</dc:creator>
      <dc:date>2013-03-18T15:21:18Z</dc:date>
    </item>
  </channel>
</rss>