<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Kinetis EHCI USB-Host 160ms Interrupt in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Kinetis-EHCI-USB-Host-160ms-Interrupt/m-p/226049#M6095</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using USB-Host Mass Storage Device class of MQX 4.0.1. with K70 EHCI and I face the following problem:&lt;/P&gt;&lt;P&gt;When a memory stick is inserted, the function _usb_ehci_reset_and_enable_port is called by the ISR. Inside that function there are two loops which run for approximately 160ms (debounce for 100ms, wait for reset for 60ms). During that time the whole system is unresponsive because it stays inside an ISR.&lt;/P&gt;&lt;P&gt;I don't think it's a good idea to do 100ms debounce loops in RTOS interrupt routines.&lt;/P&gt;&lt;P&gt;Has someone already written a patch for that problem?&lt;/P&gt;&lt;P&gt;Perhaps we can use the uframe-interrupt...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards, Johannes&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 18 Jun 2013 12:58:27 GMT</pubDate>
    <dc:creator>johannesschock</dc:creator>
    <dc:date>2013-06-18T12:58:27Z</dc:date>
    <item>
      <title>Kinetis EHCI USB-Host 160ms Interrupt</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Kinetis-EHCI-USB-Host-160ms-Interrupt/m-p/226049#M6095</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using USB-Host Mass Storage Device class of MQX 4.0.1. with K70 EHCI and I face the following problem:&lt;/P&gt;&lt;P&gt;When a memory stick is inserted, the function _usb_ehci_reset_and_enable_port is called by the ISR. Inside that function there are two loops which run for approximately 160ms (debounce for 100ms, wait for reset for 60ms). During that time the whole system is unresponsive because it stays inside an ISR.&lt;/P&gt;&lt;P&gt;I don't think it's a good idea to do 100ms debounce loops in RTOS interrupt routines.&lt;/P&gt;&lt;P&gt;Has someone already written a patch for that problem?&lt;/P&gt;&lt;P&gt;Perhaps we can use the uframe-interrupt...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards, Johannes&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Jun 2013 12:58:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Kinetis-EHCI-USB-Host-160ms-Interrupt/m-p/226049#M6095</guid>
      <dc:creator>johannesschock</dc:creator>
      <dc:date>2013-06-18T12:58:27Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis EHCI USB-Host 160ms Interrupt</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Kinetis-EHCI-USB-Host-160ms-Interrupt/m-p/226050#M6096</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have checked and so far there is no patch for this.&lt;/P&gt;&lt;P&gt;I can send this feedback to the developers but if you are able to improve this, it would be nice and very appreciated to get this feedback.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp; a lot for the feedback. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alejandro &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Aug 2013 22:51:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Kinetis-EHCI-USB-Host-160ms-Interrupt/m-p/226050#M6096</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2013-08-19T22:51:45Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis EHCI USB-Host 160ms Interrupt</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Kinetis-EHCI-USB-Host-160ms-Interrupt/m-p/226051#M6097</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Alejandro,&lt;/P&gt;&lt;P&gt;sorry for answering late, but I lost focus on that topic (I didn't expect an answer anymore :smileyhappy:).&lt;/P&gt;&lt;P&gt;I've written a patch which propagates all ehci-Interrupts to a high priority task using a lwmessage. The high priority task handles the interrupt then, allowing doing debounce with _time_delay().&lt;/P&gt;&lt;P&gt;I use the follwing scheme:&lt;/P&gt;&lt;P&gt;in _usb_ehci_init: initialize message queue, start additional isr task&lt;/P&gt;&lt;P&gt;in _usb_ehci_isr: disable ehci interrupt, send usb handle via message queue&lt;/P&gt;&lt;P&gt;in interrupt task: while(1) {wait for message, call _usb_ehci_isrfunc (which loops until all pending interrupts are serviced), enable ehci interrupt}&lt;/P&gt;&lt;P&gt;in _usb_ehci_reset_and_enable_port I changed the debounce loops to loops using _time_delay()&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't want to publish my patch here in the forum, because it is a quick and dirty solution and not tested concerning stability and side effects.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Sep 2013 08:51:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Kinetis-EHCI-USB-Host-160ms-Interrupt/m-p/226051#M6097</guid>
      <dc:creator>johannesschock</dc:creator>
      <dc:date>2013-09-13T08:51:36Z</dc:date>
    </item>
  </channel>
</rss>