<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Creating and compiling library project (FFS) in MQX 4.0.1 and CW10.4 in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Creating-and-compiling-library-project-FFS-in-MQX-4-0-1-and-CW10/m-p/224641#M6048</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It seems you have used GNU C compiler for the ffs.a. However, the ffs lib is written in c++ and therefore you need to use GNU C++ compiler. I was able to do what you are looking for (I attach my ffs folder with build projects for CW 10.4 with the gcc compiler). The demo project seems to work with this (tried: nanderasechip, fsopen, format a:, write test00.txt 512, fsclose, Power On Reset, fsopen, dir and read test00.txt). I did only Debug build configuration of MQX libraries and Int Flash Sram Data build configuration for the demo application.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 19 Jun 2013 10:28:22 GMT</pubDate>
    <dc:creator>Martin_</dc:creator>
    <dc:date>2013-06-19T10:28:22Z</dc:date>
    <item>
      <title>Creating and compiling library project (FFS) in MQX 4.0.1 and CW10.4</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Creating-and-compiling-library-project-FFS-in-MQX-4-0-1-and-CW10/m-p/224638#M6045</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to port the FFS library and the corresponding example (&lt;A href="https://community.nxp.com/docs/DOC-94186"&gt;NAND Flash File System patch for Freescale MQX™ RTOS 4.0.0&lt;/A&gt;) from Freescale compiler to GNU GCC compiler.&lt;/P&gt;&lt;P&gt;To do this I set up a new project for the library like it is explained here: &lt;A href="http://mcuoneclipse.com/2012/10/08/a-library-with-arm-gcc-and-eclipse/" title="http://mcuoneclipse.com/2012/10/08/a-library-with-arm-gcc-and-eclipse/"&gt;A Library with ARM gcc and Eclipse | MCU on Eclipse&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;This produces a valid library file (fss.a).&lt;/P&gt;&lt;P&gt;In the next step I tried to port the included msf_nandflash example by creating a new gcc project, including all the references and adding the previously created library to the linker. At this point I'm getting many "undefined reference" errors in the file "Freescale_MQX_4_0\ffs\source\nandflash_wl.c" for funtion names from the library like 'DriveErase' or 'DriveRepair'.&lt;/P&gt;&lt;P&gt;Can somebody please help me?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Jun 2013 13:51:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Creating-and-compiling-library-project-FFS-in-MQX-4-0-1-and-CW10/m-p/224638#M6045</guid>
      <dc:creator>friederschrempf</dc:creator>
      <dc:date>2013-06-17T13:51:16Z</dc:date>
    </item>
    <item>
      <title>Re: Creating and compiling library project (FFS) in MQX 4.0.1 and CW10.4</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Creating-and-compiling-library-project-FFS-in-MQX-4-0-1-and-CW10/m-p/224639#M6046</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Frieder Schrempf,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we could possibly help you in case you share the library you created and the example project with errors.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;c0170&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Jun 2013 05:22:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Creating-and-compiling-library-project-FFS-in-MQX-4-0-1-and-CW10/m-p/224639#M6046</guid>
      <dc:creator>c0170</dc:creator>
      <dc:date>2013-06-18T05:22:51Z</dc:date>
    </item>
    <item>
      <title>Re: Creating and compiling library project (FFS) in MQX 4.0.1 and CW10.4</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Creating-and-compiling-library-project-FFS-in-MQX-4-0-1-and-CW10/m-p/224640#M6047</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your reply!&lt;/P&gt;&lt;P&gt;In the attachment you find the compiled ffs.a library and the example project.&lt;/P&gt;&lt;P&gt;Thanks for any help in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Jun 2013 06:07:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Creating-and-compiling-library-project-FFS-in-MQX-4-0-1-and-CW10/m-p/224640#M6047</guid>
      <dc:creator>friederschrempf</dc:creator>
      <dc:date>2013-06-18T06:07:32Z</dc:date>
    </item>
    <item>
      <title>Re: Creating and compiling library project (FFS) in MQX 4.0.1 and CW10.4</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Creating-and-compiling-library-project-FFS-in-MQX-4-0-1-and-CW10/m-p/224641#M6048</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It seems you have used GNU C compiler for the ffs.a. However, the ffs lib is written in c++ and therefore you need to use GNU C++ compiler. I was able to do what you are looking for (I attach my ffs folder with build projects for CW 10.4 with the gcc compiler). The demo project seems to work with this (tried: nanderasechip, fsopen, format a:, write test00.txt 512, fsclose, Power On Reset, fsopen, dir and read test00.txt). I did only Debug build configuration of MQX libraries and Int Flash Sram Data build configuration for the demo application.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Jun 2013 10:28:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Creating-and-compiling-library-project-FFS-in-MQX-4-0-1-and-CW10/m-p/224641#M6048</guid>
      <dc:creator>Martin_</dc:creator>
      <dc:date>2013-06-19T10:28:22Z</dc:date>
    </item>
    <item>
      <title>Re: Creating and compiling library project (FFS) in MQX 4.0.1 and CW10.4</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Creating-and-compiling-library-project-FFS-in-MQX-4-0-1-and-CW10/m-p/224642#M6049</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your support. It seems to work now as intended!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Jun 2013 11:58:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Creating-and-compiling-library-project-FFS-in-MQX-4-0-1-and-CW10/m-p/224642#M6049</guid>
      <dc:creator>friederschrempf</dc:creator>
      <dc:date>2013-06-20T11:58:25Z</dc:date>
    </item>
    <item>
      <title>Re: Creating and compiling library project (FFS) in MQX 4.0.1 and CW10.4</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Creating-and-compiling-library-project-FFS-in-MQX-4-0-1-and-CW10/m-p/224643#M6050</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've got one question left. Maybe you can help.&lt;/P&gt;&lt;P&gt;How can I specify the size of the FFS partition? After running the format command from the shell I always get 10 723 328 bytes size.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Jun 2013 14:44:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Creating-and-compiling-library-project-FFS-in-MQX-4-0-1-and-CW10/m-p/224643#M6050</guid>
      <dc:creator>friederschrempf</dc:creator>
      <dc:date>2013-06-20T14:44:02Z</dc:date>
    </item>
    <item>
      <title>Re: Creating and compiling library project (FFS) in MQX 4.0.1 and CW10.4</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Creating-and-compiling-library-project-FFS-in-MQX-4-0-1-and-CW10/m-p/224644#M6051</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The drive is defined in g_nandZipConfigBlockInfo in ddi_nand_media_definition.cpp&lt;/P&gt;&lt;P&gt;The #define NANDFLASH_1ST_DATA_DRIVE_SIZE_IN_BLOCK comes from nandflash_wl_ffs.h&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Jun 2013 04:54:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Creating-and-compiling-library-project-FFS-in-MQX-4-0-1-and-CW10/m-p/224644#M6051</guid>
      <dc:creator>Martin_</dc:creator>
      <dc:date>2013-06-21T04:54:58Z</dc:date>
    </item>
    <item>
      <title>Re: Creating and compiling library project (FFS) in MQX 4.0.1 and CW10.4</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Creating-and-compiling-library-project-FFS-in-MQX-4-0-1-and-CW10/m-p/224645#M6052</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks! I tried modifiying NANDFLASH_1ST_DATA_DRIVE_SIZE_IN_BLOCK but without effect: after "format a:" command I still get 10 723 328 bytes size&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Jun 2013 06:27:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Creating-and-compiling-library-project-FFS-in-MQX-4-0-1-and-CW10/m-p/224645#M6052</guid>
      <dc:creator>friederschrempf</dc:creator>
      <dc:date>2013-06-21T06:27:10Z</dc:date>
    </item>
    <item>
      <title>Re: Creating and compiling library project (FFS) in MQX 4.0.1 and CW10.4</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Creating-and-compiling-library-project-FFS-in-MQX-4-0-1-and-CW10/m-p/224646#M6053</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Martin,&lt;/P&gt;&lt;P&gt;I am facing the same problem as Frieder faced. I used the code given by you in ffs.zip for my TWRK60F120M board and got valid library ffs.a and then I created new project with demo.c(given in ffs.zip) then also I am getting undefined reference to _io_nandflash_wl_install(), though I am giving the path of lib in project (settings are same in preference as there in your project).To check for any setting missing I checked your code and build it for TWRK70 and got .elf file successfully then I created new project for demo.c using TWRK70 only but here also I got the same error.&lt;/P&gt;&lt;P&gt;Please help me to figure out this problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 18 Jan 2014 11:43:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Creating-and-compiling-library-project-FFS-in-MQX-4-0-1-and-CW10/m-p/224646#M6053</guid>
      <dc:creator>adt</dc:creator>
      <dc:date>2014-01-18T11:43:23Z</dc:date>
    </item>
    <item>
      <title>Re: Creating and compiling library project (FFS) in MQX 4.0.1 and CW10.4</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Creating-and-compiling-library-project-FFS-in-MQX-4-0-1-and-CW10/m-p/224647#M6054</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Martin,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I used the FFS code given by you in above post for my TWRK60F120M and it worked fine in MQX4.0 CW10.5 due to some issues I faced in FFS now I am using MQX4.1 CW10.6 I checked the demo code and done all changes what you did in MQX4.0 and my demo.c code worked fine but in my project I am getting lots of undefined reference errors for FFS related functions though I have changed C/C++ build settings as there in your project.&lt;/P&gt;&lt;P&gt;Please help me to resolve this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Jul 2014 05:09:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Creating-and-compiling-library-project-FFS-in-MQX-4-0-1-and-CW10/m-p/224647#M6054</guid>
      <dc:creator>adt</dc:creator>
      <dc:date>2014-07-04T05:09:56Z</dc:date>
    </item>
  </channel>
</rss>