<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックRe: MCF52259 SD Card 4-Bit Mode?</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/MCF52259-SD-Card-4-Bit-Mode/m-p/219559#M5761</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For this purpose, eSDHC HW module was introduced on some chips and there's new&amp;nbsp;esdhc driver in MQX 3.6.1. for that.&lt;/P&gt;&lt;P&gt;Unfortunately MCF52259 doesn't support this functionality.&lt;/P&gt;&lt;P&gt;You can try to set the spi to highest speed possible.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;PetrM&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 27 Aug 2010 21:10:05 GMT</pubDate>
    <dc:creator>PetrM</dc:creator>
    <dc:date>2010-08-27T21:10:05Z</dc:date>
    <item>
      <title>MCF52259 SD Card 4-Bit Mode?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MCF52259-SD-Card-4-Bit-Mode/m-p/219558#M5760</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have an SD card fully working with MFS using SPI, but for my application I want to attain the fastest speeds possible with my microSDHC card. So this brings up the question:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it possible using the MCF52259 to operate the SD card in the 4-bit SD mode?The 4-bit mode is significantly faster than the SPI mode. If it is possible, I am a bit confused as to which pins I would connect the DAT[3:0] and CMD lines of the SD card to.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Aug 2010 06:57:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MCF52259-SD-Card-4-Bit-Mode/m-p/219558#M5760</guid>
      <dc:creator>EDesigns</dc:creator>
      <dc:date>2010-08-24T06:57:43Z</dc:date>
    </item>
    <item>
      <title>Re: MCF52259 SD Card 4-Bit Mode?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MCF52259-SD-Card-4-Bit-Mode/m-p/219559#M5761</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For this purpose, eSDHC HW module was introduced on some chips and there's new&amp;nbsp;esdhc driver in MQX 3.6.1. for that.&lt;/P&gt;&lt;P&gt;Unfortunately MCF52259 doesn't support this functionality.&lt;/P&gt;&lt;P&gt;You can try to set the spi to highest speed possible.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;PetrM&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Aug 2010 21:10:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MCF52259-SD-Card-4-Bit-Mode/m-p/219559#M5761</guid>
      <dc:creator>PetrM</dc:creator>
      <dc:date>2010-08-27T21:10:05Z</dc:date>
    </item>
    <item>
      <title>Re: MCF52259 SD Card 4-Bit Mode?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MCF52259-SD-Card-4-Bit-Mode/m-p/219560#M5762</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The MCF52259 datasheet says the QSPI can go as high as 20Mb/sec, which I set the baud rate to.&lt;/P&gt;&lt;P&gt;When I put the pin under a scope, I see the CLK running at the 20Mb/sec speed.&lt;/P&gt;&lt;P&gt;But when I am trying to read data from the SD card, it is moving at a significantly slower speed, around 95kb/sec.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any ideas? I notice that the data is coming out in "bursts" rather continuously. All I am doing is looping and reading data until I reach the "end of file." My intuition tells me there is some sort of interrupt or low level process in MQX that is preventing the SPI from smoothly reading at its highest speed?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Aug 2010 21:30:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MCF52259-SD-Card-4-Bit-Mode/m-p/219560#M5762</guid>
      <dc:creator>EDesigns</dc:creator>
      <dc:date>2010-08-27T21:30:44Z</dc:date>
    </item>
    <item>
      <title>Re: MCF52259 SD Card 4-Bit Mode?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MCF52259-SD-Card-4-Bit-Mode/m-p/219561#M5763</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well, it's not just about SPI. Let me summarize the overheads I know about along with some hints:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1) RAM target (execution from RAM)&amp;nbsp;=&amp;gt; use flash target&lt;/P&gt;&lt;P&gt;2) higher priority tasks and interrupts =&amp;gt; review your needs/architecture&lt;/P&gt;&lt;P&gt;3) MFS stack (caches, FAT read/write, single sector based processing) =&amp;gt; set MFSCFG_FAT_CACHE_SIZE to 2 (minimum)&lt;/P&gt;&lt;P&gt;4) SD card layer (commands issuing, busy waiting, CRC calculation) =&amp;gt; N/A&lt;/P&gt;&lt;P&gt;5) SPI driver (IOCTLs, CS assertions) =&amp;gt; N/A&lt;/P&gt;&lt;P&gt;6)&amp;nbsp;debug code&amp;nbsp;overhead =&amp;gt; use release targets&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There's no doubt that SD card could be operated more efficiently (even on this processor) and there could be done some improvements, but on the other hand, it's quite an universal&amp;nbsp;stack and multitasking we're talking about.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;PetrM&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Aug 2010 23:15:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MCF52259-SD-Card-4-Bit-Mode/m-p/219561#M5763</guid>
      <dc:creator>PetrM</dc:creator>
      <dc:date>2010-08-30T23:15:40Z</dc:date>
    </item>
  </channel>
</rss>