<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: USB DFU driver in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/USB-DFU-driver/m-p/216958#M5563</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I downloaded AN4370SW today and tried to install the driver on my Windows 7 machine and I was able to install both DFU Runtime and DFU Device drivers. Did you follow AN4370 section 5.4.1 Driver installation, especially the "Have disk..." approach ? This worked for me. Windows 7 complain that drivers are not digitally signed, so I used force option to install them and then they worked.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use twrk70f120m with TWR-SER.&lt;/P&gt;&lt;P&gt;First I load the DFU bootloader application for K70 into the board using CW 10.2.&lt;/P&gt;&lt;P&gt;Then I restart the board with the SW2 button on processor board pressed; then I plug-in usb cable into my PC. Windows 7 then install USB HID device automatically, and I use "Have disk..." to force intallation of DFU Runtime.inf.&lt;/P&gt;&lt;P&gt;Then I unplug the usb cable and plug it back and use "Have disk..." to force installation of DFU Device.inf.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 15 Oct 2012 07:40:04 GMT</pubDate>
    <dc:creator>Martin_</dc:creator>
    <dc:date>2012-10-15T07:40:04Z</dc:date>
    <item>
      <title>USB DFU driver</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/USB-DFU-driver/m-p/216957#M5562</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;when I connect my USB DFU Bootloader device (AN4370) to PC, I can see device named DFU DEMO was plugged in, but I can't install driver for it. During drivers installation I navigate to ../DFU_winusb_driver folder with DFU_Device_Runtime.inf, but then it tells me that Windows can't find the driver. Any ideas? I have Windows 7.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Oct 2012 08:39:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/USB-DFU-driver/m-p/216957#M5562</guid>
      <dc:creator>gaminn</dc:creator>
      <dc:date>2012-10-12T08:39:00Z</dc:date>
    </item>
    <item>
      <title>Re: USB DFU driver</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/USB-DFU-driver/m-p/216958#M5563</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I downloaded AN4370SW today and tried to install the driver on my Windows 7 machine and I was able to install both DFU Runtime and DFU Device drivers. Did you follow AN4370 section 5.4.1 Driver installation, especially the "Have disk..." approach ? This worked for me. Windows 7 complain that drivers are not digitally signed, so I used force option to install them and then they worked.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use twrk70f120m with TWR-SER.&lt;/P&gt;&lt;P&gt;First I load the DFU bootloader application for K70 into the board using CW 10.2.&lt;/P&gt;&lt;P&gt;Then I restart the board with the SW2 button on processor board pressed; then I plug-in usb cable into my PC. Windows 7 then install USB HID device automatically, and I use "Have disk..." to force intallation of DFU Runtime.inf.&lt;/P&gt;&lt;P&gt;Then I unplug the usb cable and plug it back and use "Have disk..." to force installation of DFU Device.inf.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Oct 2012 07:40:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/USB-DFU-driver/m-p/216958#M5563</guid>
      <dc:creator>Martin_</dc:creator>
      <dc:date>2012-10-15T07:40:04Z</dc:date>
    </item>
    <item>
      <title>Re: USB DFU driver</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/USB-DFU-driver/m-p/216959#M5564</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Martin!&lt;/P&gt;&lt;P&gt;Thanks for your answer. I use custom board with MK20DX256 MCU. My problem is probably in inaccurate clock source for USB module. At least I hope in that. I have to buy more accurate crystal. &lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Oct 2012 08:58:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/USB-DFU-driver/m-p/216959#M5564</guid>
      <dc:creator>gaminn</dc:creator>
      <dc:date>2012-10-15T08:58:54Z</dc:date>
    </item>
    <item>
      <title>Re: USB DFU driver</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/USB-DFU-driver/m-p/216960#M5565</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Martin,&lt;/P&gt;&lt;P&gt;Are you able to solve the driver issue. I am also facing the driver compatible issue on twrk40x256 board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Sunil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Oct 2012 10:51:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/USB-DFU-driver/m-p/216960#M5565</guid>
      <dc:creator>sunilkonda</dc:creator>
      <dc:date>2012-10-22T10:51:56Z</dc:date>
    </item>
    <item>
      <title>Re: USB DFU driver</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/USB-DFU-driver/m-p/216961#M5566</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I got TWR-K70 and I have the same issue with it as with my custom board. Tried on Windos 7 32 bit and Windows 7 64 bit.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Somebody from Freescale should assist here...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Oct 2012 20:49:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/USB-DFU-driver/m-p/216961#M5566</guid>
      <dc:creator>gaminn</dc:creator>
      <dc:date>2012-10-26T20:49:10Z</dc:date>
    </item>
    <item>
      <title>Re: USB DFU driver</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/USB-DFU-driver/m-p/216962#M5567</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've had the same driver installation problem, and it was solved by strictly following the procedure detailled in AN4370: when installing the driver manually, you must use the "choose driver from a list" option, as described in page 18 of the AN.&lt;/P&gt;&lt;P&gt;Hope this helps...&lt;/P&gt;&lt;P&gt;AV&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Mar 2013 14:45:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/USB-DFU-driver/m-p/216962#M5567</guid>
      <dc:creator>alexandrevincon</dc:creator>
      <dc:date>2013-03-14T14:45:31Z</dc:date>
    </item>
  </channel>
</rss>