<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックRe: MPC5125 and MQX</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/MPC5125-and-MQX/m-p/215434#M5497</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Now it works, I used MQX int_install_isr function.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 01 Jul 2011 17:52:51 GMT</pubDate>
    <dc:creator>Vishwa</dc:creator>
    <dc:date>2011-07-01T17:52:51Z</dc:date>
    <item>
      <title>MPC5125 and MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MPC5125-and-MQX/m-p/215433#M5496</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;We want to use MPC5125 in a new design for a Smart Information Display.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;But, I have lot of confusions:&lt;/FONT&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;There are only two registers for interrupt in MPC5125 DIU, INT_STATUS and INT_MASK. INT_STATUS is Read only. I plan to use LS_BF_VS interrupt.&lt;/FONT&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;&lt;STRONG&gt;So, How do I clear the event once LS_BF_VS is received, I understand I have to clear the event in ISR?.&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;2. I am going through the Chapter 18 IPIC in MPC5125RM, I understand that I have to program the IPIC registers also for handling the DIU interrupt.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;&lt;STRONG&gt;So, I would like to know what all I have to do in IPIC to handle and service DIU interrupt?&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;3. I plan to use Freescale Codewarrior and Freescale MQX to develop the software, I was going through the MQX code and the Freescale GUI code, it does not use interrupt. So, I have to add code for the following:&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;a. Initialize DIU registers and enable LS_BF_VS interrupt.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;&lt;STRONG&gt;b.&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/STRONG&gt; Modify the IPIC to handle DIU interrupt, I saw there is a file int_cntl_mpc5125.c in BSP which I have to modify, &lt;STRONG&gt;if you can tell me what all I have to do in IPIC, I will modify the code in int_cntl_mpc5125.c to handle the DIU interrupt.&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;c. I have to install DIU_Isr and write Isr to service DIU interrupt, if you can tell me what all I have to do to install DIU_Isr, I will write the code.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;&lt;STRONG&gt;Can someone tell how to enable/handle DIU interrupt, program IPIC in MPC5125, install Isr and write Isr.&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;Best Regards.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;M.S.Visweswaraiah.&lt;/FONT&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2011 19:16:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MPC5125-and-MQX/m-p/215433#M5496</guid>
      <dc:creator>Vishwa</dc:creator>
      <dc:date>2011-06-16T19:16:34Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5125 and MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MPC5125-and-MQX/m-p/215434#M5497</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Now it works, I used MQX int_install_isr function.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Jul 2011 17:52:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MPC5125-and-MQX/m-p/215434#M5497</guid>
      <dc:creator>Vishwa</dc:creator>
      <dc:date>2011-07-01T17:52:51Z</dc:date>
    </item>
  </channel>
</rss>