<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックRe: gpio_cpu_configure - override defaults?</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/gpio-cpu-configure-override-defaults/m-p/214222#M5366</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok after digging deeper I see that the code I was looking at leaves the bits alone that are not assigned as GPIO.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I just set the PAR bits and all is well.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Jul 2010 20:15:07 GMT</pubDate>
    <dc:creator>w2vy</dc:creator>
    <dc:date>2010-07-21T20:15:07Z</dc:date>
    <item>
      <title>gpio_cpu_configure - override defaults?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/gpio-cpu-configure-override-defaults/m-p/214221#M5365</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;gpio_cpu_configure is called often to update the pin configurations.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;One problem.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It assumes GPIO or Alternate Function 2 for most (well I care about PORT TC) functions.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How do you select a different non-GPIO function?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If the pin usage is generally GPIO or non-GPIO maybe the BSP should add a table to define the Alt function.&lt;/P&gt;&lt;P&gt;Or is there a clean up function that can be called after gpio_cpu_configure() to fix the 'errors' induced?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using DTIM0 as a clock output... searching ther code I do not see anything in MQX that uses any of the DTIM registers&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Jul 2010 18:45:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/gpio-cpu-configure-override-defaults/m-p/214221#M5365</guid>
      <dc:creator>w2vy</dc:creator>
      <dc:date>2010-07-21T18:45:29Z</dc:date>
    </item>
    <item>
      <title>Re: gpio_cpu_configure - override defaults?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/gpio-cpu-configure-override-defaults/m-p/214222#M5366</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok after digging deeper I see that the code I was looking at leaves the bits alone that are not assigned as GPIO.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I just set the PAR bits and all is well.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Jul 2010 20:15:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/gpio-cpu-configure-override-defaults/m-p/214222#M5366</guid>
      <dc:creator>w2vy</dc:creator>
      <dc:date>2010-07-21T20:15:07Z</dc:date>
    </item>
  </channel>
</rss>