<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Replacing the libraries with source code in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Replacing-the-libraries-with-source-code/m-p/212647#M5314</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;there shouldn't be any difficulties in using source code instead of libraries (although I also do not see much advantages).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The first problem :&lt;/P&gt;&lt;P&gt;shell_flush_cache﻿ - this function is defined in both files, but only one file is really used in shell project. Use the one which you find in shell library.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Telnetd_shell_template﻿ - this is different, the linker automatically override the function definition from library by the one defined in application. In your case - having both files in one project you should delete/rename one of them.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;PetrL&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 09 Jun 2011 04:42:19 GMT</pubDate>
    <dc:creator>PetrL</dc:creator>
    <dc:date>2011-06-09T04:42:19Z</dc:date>
    <item>
      <title>Replacing the libraries with source code</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Replacing-the-libraries-with-source-code/m-p/212646#M5313</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to compiler the web_hvac_m52259evb example without the libraries. Instead, I would like to have the source code.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I started with shell libraries: I removed the shell.a and replaced it with: Shell Source&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; i.e.,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Shell Source\MQX&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Shell Source\Shell&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Shell Source\MFC&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Shell Source\RTCS&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I get a compiling/linker error:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; shell_flush_cache is defined in sh_cash.c and sh_flush.c.&lt;/P&gt;&lt;P&gt;Similarly,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Telnetd_shell_template defined in RTCS.c and sh_tnetd.c&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The function and structure are defined in 2 files and there seem to be no #ifdef dictating which one to use.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So which one should I use and why?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;S&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;﻿&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jun 2011 02:01:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Replacing-the-libraries-with-source-code/m-p/212646#M5313</guid>
      <dc:creator>SVC2</dc:creator>
      <dc:date>2011-06-08T02:01:24Z</dc:date>
    </item>
    <item>
      <title>Re: Replacing the libraries with source code</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Replacing-the-libraries-with-source-code/m-p/212647#M5314</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;there shouldn't be any difficulties in using source code instead of libraries (although I also do not see much advantages).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The first problem :&lt;/P&gt;&lt;P&gt;shell_flush_cache﻿ - this function is defined in both files, but only one file is really used in shell project. Use the one which you find in shell library.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Telnetd_shell_template﻿ - this is different, the linker automatically override the function definition from library by the one defined in application. In your case - having both files in one project you should delete/rename one of them.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;PetrL&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Jun 2011 04:42:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Replacing-the-libraries-with-source-code/m-p/212647#M5314</guid>
      <dc:creator>PetrL</dc:creator>
      <dc:date>2011-06-09T04:42:19Z</dc:date>
    </item>
  </channel>
</rss>