<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software Solutions中的主题 Re: CW Licensing for MQX</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/CW-Licensing-for-MQX/m-p/211532#M5227</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I recently purchased the MCF51CN in the Tower system and have the same concerns.&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 09 Jul 2010 06:01:55 GMT</pubDate>
    <dc:creator>machinegeek</dc:creator>
    <dc:date>2010-07-09T06:01:55Z</dc:date>
    <item>
      <title>CW Licensing for MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/CW-Licensing-for-MQX/m-p/211531#M5226</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Greetings,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it possible to develop MQX applications using CodeWarior's special Edition? I mean, with the code size constrains and number of files constrains, will I have problems with it once my Evaluation License expires?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;By development, I mean not only compilation but also flashing the board. (I'm using the Tower System with the MCF52259 MPU)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What about recompiling the BSP?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If the standard edition is not enough, which suite do I need?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Jul 2010 05:56:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/CW-Licensing-for-MQX/m-p/211531#M5226</guid>
      <dc:creator>rdazcal</dc:creator>
      <dc:date>2010-07-08T05:56:02Z</dc:date>
    </item>
    <item>
      <title>Re: CW Licensing for MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/CW-Licensing-for-MQX/m-p/211532#M5227</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I recently purchased the MCF51CN in the Tower system and have the same concerns.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Jul 2010 06:01:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/CW-Licensing-for-MQX/m-p/211532#M5227</guid>
      <dc:creator>machinegeek</dc:creator>
      <dc:date>2010-07-09T06:01:55Z</dc:date>
    </item>
    <item>
      <title>Re: CW Licensing for MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/CW-Licensing-for-MQX/m-p/211533#M5228</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is possible to use the Special Edition, but it will limit which applications and demos you can use.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can look at &lt;A href="http://www.freescale.com/webapp/sps/site/overview.jsp?code=MQXSWDW%20" rel="nofollow" target="_self"&gt;this page&lt;/A&gt; in the lower left hand corner (click on "Example Applications and Labs") to see which projects, the ones with the astricks, will not work with Special Edition because of code size limitations. That is assuming the default MQX configuration settings, so you might be able to squeeze it down further with some tweaking of user_config.h.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The libraries, with the exception of the default RTCS library, should have no problems compiling. For RTCS, you might have to take out some features to get the library down to the 128K limit.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You should probably get a license that allows you to compile code for the amount of flash on the chip. So for the MCF52259, that would be 512k, which is the Basic edition. The list of CW versions and details can be found here: &lt;A href="http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_SUITES&amp;amp;tid=CWH" rel="nofollow" target="_blank"&gt;http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_SUITES&amp;amp;tid=CWH&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also note that the code size limitations differ based on which core you're using, so a ColdFire V2/V3/V4 has a different size limitaiton than a ColdFire V1 in the Special Edition.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Finally Task Aware Debugging is only enabled on the Professional version, so keep that in mind as well.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-Anthony&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Jul 2010 23:24:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/CW-Licensing-for-MQX/m-p/211533#M5228</guid>
      <dc:creator>anthony_huereca</dc:creator>
      <dc:date>2010-07-16T23:24:57Z</dc:date>
    </item>
    <item>
      <title>Re: CW Licensing for MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/CW-Licensing-for-MQX/m-p/211534#M5229</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Anthony,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;That was exactly the information I was looking for!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 18 Jul 2010 19:52:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/CW-Licensing-for-MQX/m-p/211534#M5229</guid>
      <dc:creator>rdazcal</dc:creator>
      <dc:date>2010-07-18T19:52:34Z</dc:date>
    </item>
  </channel>
</rss>