<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: connect() timeout in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/connect-timeout/m-p/210672#M5194</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Guys,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I guess I found the reason.&lt;/P&gt;&lt;P&gt;The OPT_CONNECT_TIMEOUT socket option sets R2 timeout (defined in RFC 793).&lt;/P&gt;&lt;P&gt;According to the RFC793: &lt;EM&gt;"The value of R2 SHOULD correspond to at least 100 seconds.&lt;/EM&gt;" that equls your 1min 40 seconds.&lt;/P&gt;&lt;P&gt;Based the TCP source code, its values is checked to be not less than 100 sec (defined&amp;nbsp; by TCP_SENDTIMEOUT_MIN in tcp_prv.h).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it is clear,&lt;/P&gt;&lt;P&gt;Andrey Butok&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 Jul 2013 08:11:17 GMT</pubDate>
    <dc:creator>butok</dc:creator>
    <dc:date>2013-07-25T08:11:17Z</dc:date>
    <item>
      <title>connect() timeout</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/connect-timeout/m-p/210669#M5191</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've got a server that is purposely behind a firewall to test the OPT_CONNECT_TIMEOUT.&amp;nbsp; I want it to give up after 5000ms but it will always try somewhere around seven times to SYN before quitting which takes around 1 minute and 40 seconds.&amp;nbsp; Is there soemthing else I need to modify to get it to stop trying after the connect timeout?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;-Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Jul 2010 22:48:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/connect-timeout/m-p/210669#M5191</guid>
      <dc:creator>Mike_d</dc:creator>
      <dc:date>2010-07-02T22:48:50Z</dc:date>
    </item>
    <item>
      <title>Re: connect() timeout</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/connect-timeout/m-p/210670#M5192</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, 1 min and 40 seconds.&amp;nbsp; Same for me!!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm not sure if it's a 7x to SYN issue, as it doesn't seem matter what value I actually set connect timeout too.&amp;nbsp; I tried 1ms and still got a timeout of 1m 40s.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Anyone know a solution?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Oct 2010 17:06:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/connect-timeout/m-p/210670#M5192</guid>
      <dc:creator>Joe2</dc:creator>
      <dc:date>2010-10-07T17:06:46Z</dc:date>
    </item>
    <item>
      <title>Re: connect() timeout</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/connect-timeout/m-p/210671#M5193</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm having this same problem.&lt;/P&gt;&lt;P&gt;I'm using MQX 4.0.0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see your issue was posted in Oct 2010, is there already a fix (workaround) for this? We are already Juli 2013 ??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want a timeout of 10 sec on the connection function. (result = connect(sock, &amp;amp;addr, sizeof(addr));)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt; uint_32&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;sock;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt; uint_32&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;result;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt; uint_32&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;opt_length = sizeof(uint_32);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt; uint_32&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;opt_value;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;opt_value = 10000;&lt;/P&gt;&lt;P&gt;result = setsockopt(sock, SOL_TCP, OPT_CONNECT_TIMEOUT, &amp;amp;opt_value, opt_length);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This results in a timeout after 1 min and 40 seconds&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any idea's ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jul 2013 08:39:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/connect-timeout/m-p/210671#M5193</guid>
      <dc:creator>michris</dc:creator>
      <dc:date>2013-07-24T08:39:17Z</dc:date>
    </item>
    <item>
      <title>Re: connect() timeout</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/connect-timeout/m-p/210672#M5194</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Guys,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I guess I found the reason.&lt;/P&gt;&lt;P&gt;The OPT_CONNECT_TIMEOUT socket option sets R2 timeout (defined in RFC 793).&lt;/P&gt;&lt;P&gt;According to the RFC793: &lt;EM&gt;"The value of R2 SHOULD correspond to at least 100 seconds.&lt;/EM&gt;" that equls your 1min 40 seconds.&lt;/P&gt;&lt;P&gt;Based the TCP source code, its values is checked to be not less than 100 sec (defined&amp;nbsp; by TCP_SENDTIMEOUT_MIN in tcp_prv.h).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it is clear,&lt;/P&gt;&lt;P&gt;Andrey Butok&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Jul 2013 08:11:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/connect-timeout/m-p/210672#M5194</guid>
      <dc:creator>butok</dc:creator>
      <dc:date>2013-07-25T08:11:17Z</dc:date>
    </item>
    <item>
      <title>Re: connect() timeout</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/connect-timeout/m-p/210673#M5195</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andrey,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I changed TCP_SENDTIMEOUT_MIN to 10000. (Instead of default 100000)&lt;/P&gt;&lt;P&gt;Now I have a timeout of 10 sec.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thx&lt;/P&gt;&lt;P&gt;Christophe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Oct 2013 08:43:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/connect-timeout/m-p/210673#M5195</guid>
      <dc:creator>michris</dc:creator>
      <dc:date>2013-10-24T08:43:19Z</dc:date>
    </item>
  </channel>
</rss>