<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software Solutions中的主题 Simple TCP sockets client example?</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Simple-TCP-sockets-client-example/m-p/208069#M4970</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there a complete example of a simple TCP sockets client around somewhere? &amp;nbsp;Found a server (quote-a-day?), but no client.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have an app that works fine under Linux on an Intel box, but after some modifications for MQX and a lot of head banging, I still don't have something that connects and talks to the server. &amp;nbsp;I was getting it to connect to the server, but adding in the recv call was crashing the code completely (as in, before it even got to the recv call). &amp;nbsp;Then I figured out that the task needed more stack space, &amp;nbsp;increased it to 4000 or 6000 and it no longer crashes, but it also no longer connects. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;FWIW, I'm running on a very old M52233DEMO board, so I'm thinking I may also need to patch the phy_mfc5223x.c code for the speed problem?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;John&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 21 May 2011 00:58:47 GMT</pubDate>
    <dc:creator>jpa</dc:creator>
    <dc:date>2011-05-21T00:58:47Z</dc:date>
    <item>
      <title>Simple TCP sockets client example?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Simple-TCP-sockets-client-example/m-p/208069#M4970</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there a complete example of a simple TCP sockets client around somewhere? &amp;nbsp;Found a server (quote-a-day?), but no client.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have an app that works fine under Linux on an Intel box, but after some modifications for MQX and a lot of head banging, I still don't have something that connects and talks to the server. &amp;nbsp;I was getting it to connect to the server, but adding in the recv call was crashing the code completely (as in, before it even got to the recv call). &amp;nbsp;Then I figured out that the task needed more stack space, &amp;nbsp;increased it to 4000 or 6000 and it no longer crashes, but it also no longer connects. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;FWIW, I'm running on a very old M52233DEMO board, so I'm thinking I may also need to patch the phy_mfc5223x.c code for the speed problem?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;John&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 May 2011 00:58:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Simple-TCP-sockets-client-example/m-p/208069#M4970</guid>
      <dc:creator>jpa</dc:creator>
      <dc:date>2011-05-21T00:58:47Z</dc:date>
    </item>
    <item>
      <title>Re: Simple TCP sockets client example?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Simple-TCP-sockets-client-example/m-p/208070#M4971</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;From Technical&amp;nbsp; Support ﻿ I got a server-client example but it is for the MCF52259﻿.&lt;/P&gt;&lt;P&gt;You can easily port it to your system.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jun 2011 17:12:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Simple-TCP-sockets-client-example/m-p/208070#M4971</guid>
      <dc:creator>Steamy</dc:creator>
      <dc:date>2011-06-07T17:12:55Z</dc:date>
    </item>
  </channel>
</rss>