<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to Install New Hardware Intrerrupts in MQX in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-Install-New-Hardware-Intrerrupts-in-MQX/m-p/205830#M4836</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Simillar problem here i am facing. Only timer interrupt working. We are trying here for ADC Limit interrupt, but we are facing the problem in interrupt ISR. We are enabling the interrupt in ADC-&amp;gt;CR1, ADC-&amp;gt;CR2. and getting the interrupt for the same in Interrupt Mask register. It is not setting in IPR.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Below is sample code for code warrior CW 10 and MQX 4.0 given in $ Freescale_MQX_4_0\mqx\source\io\adc\mcf544xx&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;old_isr_adc1_param = _int_get_isr(BSP_ADC_INTERRUPT_VECTOR);&lt;/P&gt;&lt;P&gt;old_isr_adc1 = _int_install_isr(BSP_ADC_INTERRUPT_VECTOR, adc_complete_isr, NULL);&lt;/P&gt;&lt;P&gt;_mcf5441_int_init(BSP_ADC_INTERRUPT_VECTOR, BSP_ADC_INTERRUPT_LEVEL, TRUE);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kindly Help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Sep 2013 10:35:31 GMT</pubDate>
    <dc:creator>pritam_bansod</dc:creator>
    <dc:date>2013-09-11T10:35:31Z</dc:date>
    <item>
      <title>How to Install New Hardware Intrerrupts in MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-Install-New-Hardware-Intrerrupts-in-MQX/m-p/205821#M4827</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I try to make a DMA UART transfer and it works ok. But the problem is in the program i try to put an Intrerrupt for DMA Complete but it doesn't work the interrupt, when I check with the debugger the status for registers them looks ok. Then i tryed to make a button interrupt without MQX GIPIO driver only hardware interrupt. But this to don't work.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The function int_install_isr it's returning the value for ISR ok, i don't receive a NULL pointer.&lt;/P&gt;&lt;P&gt;THis matter drive me crazy !!&lt;/P&gt;&lt;P&gt;Then I try to build my interrupt configuration based on isr.c example from MQX examples.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is the code for ISR&lt;/P&gt;&lt;PRE&gt;void sw2_isr(pointer user_isr_ptr){   MY_ISR_STRUCT_PTR  isr_ptr;   isr_ptr = (MY_ISR_STRUCT_PTR)user_isr_ptr;   /* Chain to the previous notifier */   (*isr_ptr-&amp;gt;OLD_ISR)(isr_ptr-&amp;gt;OLD_ISR_DATA);   printf("SW2 ISR\n");   PORTE_ISFR=0xFFFFFFFF; //Clear Flags on Port E ISR Flag Register}//ANd DMA ISR CODEvoid dma5_isr(pointer data){  if(DMA_ES_REG(DMA_BASE_PTR)&amp;amp;DMA_ES_VLD_MASK == 1)  printf("Eroarre"); else  printf("Intrerupere"); DMA_CERQ=DMA_CERQ_CERQ(5); DMA_CINT=DMA_CINT_CINT(5);
}&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;And This is the code for the task and initialization of the isr's functions&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;void uart5_dma_task(uint_32 data){  //Local Variables MY_ISR_STRUCT_PTR  isr_ptr; MQX_FILE_PTR port_file_sw1; int *isr; uint8_t uint8_dma_channel=5; char c,i=0; enable_dma_clocks(); gpio_init_isr_porte();      /* port_file_sw1=fopen("gpio:input",(char *)&amp;amp;SW1);   if(port_file_sw1!=NULL)   {printf("IRQ  1 SET\n");    _io_ioctl(port_file_sw1,GPIO_IOCTL_SET_IRQ_FUNCTION,(char *)irq_sw1);}*/    //Enable DMA Channel 5 with UART5-RX (12) intrerrupt surce. enable_dmamux(uint8_dma_channel,UART5_DMA_RX_DMAMUX); uart5_dma_init(UART5_BASE_PTR,BSP_BUS_CLOCK_KHZ,UART5_BAUD_RATE);    isr_ptr = _mem_alloc_zero((_mem_size)sizeof(MY_ISR_STRUCT));    isr_ptr-&amp;gt;OLD_ISR_DATA =_int_get_isr_data(INT_PORTE);    isr_ptr-&amp;gt;OLD_ISR=_int_get_isr(INT_PORTE);    if(!_int_install_isr(INT_PORTE, sw2_isr, isr_ptr))     printf("Esuare Instalare ISR\n");    isr_ptr-&amp;gt;OLD_ISR=_int_get_isr(DMA5_ISR_VECTOR);    if(!_int_install_isr(DMA5_ISR_VECTOR,dma5_isr,isr_ptr))     printf("Esuare Instalare DMA5 ISR\n"); printf("ISR NEINITIALIZAT=0x%x\n",isr); isr=(int *)_int_get_isr(DMA5_ISR_VECTOR); printf("ISR pentru DMA5 =0x%x\n",isr); isr=(int *)_int_get_isr(UART5_RX_TX_ISR_VECTOR); printf("ISR pentru UART5 =0x%x\n",isr); uart_putchar(UART5_BASE_PTR,'c'); dma_config_start(uint8_dma_channel); _int_enable(); while(1) {   }}&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;And the header and defines are here used in the uart5_dma_task :&lt;/P&gt;&lt;PRE&gt;#define UART5_RX_TX_ISR_VECTOR 71#define DMA5_ISR_VECTOR 21#define PORTE_ISR_VECTOR 107#define UART5_DMA_RX_DMAMUX 12#define UART5_DMA_TX_DMAMUX 13#define BUFFER_LENGHT 100#define SW_1 (GPIO_PORT_A | GPIO_PIN19)#define SW_2 (GPIO_PORT_E | GPIO_PIN26)void uart5_dma_init(UART_MemMapPtr uartch, int sysclk, int baud);extern void uart5_dma_task(uint_32 data);extern void isr_dma5( void );extern void uart_isr( UART_MemMapPtr base );extern void sw2_isr(pointer);&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Feb 2012 20:28:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-Install-New-Hardware-Intrerrupts-in-MQX/m-p/205821#M4827</guid>
      <dc:creator>Nana</dc:creator>
      <dc:date>2012-02-13T20:28:19Z</dc:date>
    </item>
    <item>
      <title>Re: How to Install New Hardware Intrerrupts in MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-Install-New-Hardware-Intrerrupts-in-MQX/m-p/205822#M4828</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I solved the problem, it was something about setting priority level in NVIC(nested vector interrupt controller) more than 7.&lt;/P&gt;&lt;P&gt;So I made 2 additional functions to set_irq_priority and to do enable_irq.&lt;/P&gt;&lt;PRE&gt;void enable_irq (int irq){    int div;        /* Make sure that the IRQ is an allowable number. Right now up to 91 is      * used.     */    if (irq &amp;gt; 91)        printf("\nERR! Invalid IRQ value passed to enable irq function!\n");        /* Determine which of the NVICISERs corresponds to the irq */    div = irq/32;        switch (div)    {     case 0x0:              NVICICPR0 = 1 &amp;lt;&amp;lt; (irq%32);              NVICISER0 = 1 &amp;lt;&amp;lt; (irq%32);              break;     case 0x1:              NVICICPR1 = 1 &amp;lt;&amp;lt; (irq%32);              NVICISER1 = 1 &amp;lt;&amp;lt; (irq%32);              break;     case 0x2:              NVICICPR2 = 1 &amp;lt;&amp;lt; (irq%32);              NVICISER2 = 1 &amp;lt;&amp;lt; (irq%32);              break;    }              }&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;And the one to set priority:&lt;/P&gt;&lt;PRE&gt;void set_irq_priority (int irq, int prio){    /*irq priority pointer*/    uint_8 *prio_reg;        /* Make sure that the IRQ is an allowable number. Right now up to 91 is      * used.     */    if (irq &amp;gt; 91)        printf("\nERR! Invalid IRQ value passed to priority irq function!\n");    if (prio &amp;gt; 15)        printf("\nERR! Invalid priority value passed to priority irq function!\n");        /* Determine which of the NVICIPx corresponds to the irq */    prio_reg = (uint_8 *)(((uint_32)&amp;amp;NVICIP0) + irq);    /* Assign priority to IRQ */    *prio_reg = ( (prio&amp;amp;0xF) &amp;lt;&amp;lt; (8 - ARM_INTERRUPT_LEVEL_BITS) );             }&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;So now all my interrupts are working how I want them to work !!&lt;/P&gt;&lt;P&gt;But another problem came to my attention when I use the DMA transfer on circular queue and the Destination modulo 2 address incremented with offset 1 byte. To transfer data from UART5 Data register, if the start address of the buffer variable is not&amp;nbsp; aligned to a modulo 2 address. It's going to cut from your space available for buffer elements.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Exemple&lt;/P&gt;&lt;P&gt;If i have a modulo 2 bits for incrementing the destination address and the start address for buffer is 0xfffff350&lt;/P&gt;&lt;P&gt;I have 0xfffff350 first element&lt;/P&gt;&lt;P&gt;0xfffff351&amp;nbsp; second one&lt;/P&gt;&lt;P&gt;0xfffff352 3th&lt;/P&gt;&lt;P&gt;0xfffff353 4th one&lt;/P&gt;&lt;P&gt;&amp;nbsp;and if the compiler allocates the start address for the buffer the address 0xfffff352&lt;/P&gt;&lt;P&gt;I remain only with 2 available locations for my buffer to store my data's because the modulo 2 feature let me to increment only the last 2 bits from the start address of the buffer.&lt;/P&gt;&lt;P&gt;So my question is how can I determine the compiler to allocate in memory my buffer to start at the right address.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is the code for DMA configuration&lt;/P&gt;&lt;PRE&gt;/********************************************************************//* * Configuration of DMA_channel and start of the movement data from * UART5 Data register address and to a queue(circular stack) with the  * beginning address of the buffer variable as a destination address. * The destination address will be incremented with the width of the transfered  * data in bytes from the source address in this case sizeof the UART5 Data register *  */void dma_config_start(uint_8 channel){   DMA_CITER_ELINKNO_REG(DMA_BASE_PTR,channel)=DMA_BITER_ELINKNO_REG(DMA_BASE_PTR,channel)=sizeof(UART5_D); DMA_NBYTES_MLNO_REG(DMA_BASE_PTR,channel)=sizeof(UART5_D); DMA_SOFF_REG(DMA_BASE_PTR,channel) = 1; DMA_SADDR_REG(DMA_BASE_PTR,channel)=(uint_32)&amp;amp;UART5_D; DMA_ATTR_REG(DMA_BASE_PTR,channel)=DMA_ATTR_SMOD(0)|DMA_ATTR_SSIZE(0)|DMA_ATTR_DMOD(2)|DMA_ATTR_DSIZE(0); DMA_SLAST_REG(DMA_BASE_PTR,channel)=-sizeof(UART5_D); DMA_DADDR_REG(DMA_BASE_PTR,channel)=(uint_32)&amp;amp;buffer; DMA_DOFF_REG(DMA_BASE_PTR,channel) = sizeof(UART5_D); DMA_DLAST_SGA_REG(DMA_BASE_PTR,channel) = 0; DMA_SERQ_REG(DMA_BASE_PTR)=DMA_SERQ_SERQ(5); DMA_ERQ_REG(DMA_BASE_PTR) |=(1&amp;lt;&amp;lt;channel); DMA_CR |=DMA_CR_EDBG_MASK;   //Enable Debug MODE in DMA  //DMA_INT_REG(DMA_BASE_PTR) |=DMA_INT_INT5_MASK;  DMA_CSR_REG(DMA_BASE_PTR,channel)=DMA_CSR_INTMAJOR_MASK; //DMA_CSR_START_MASK;}&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Feb 2012 17:42:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-Install-New-Hardware-Intrerrupts-in-MQX/m-p/205822#M4828</guid>
      <dc:creator>Nana</dc:creator>
      <dc:date>2012-02-14T17:42:07Z</dc:date>
    </item>
    <item>
      <title>Re: How to Install New Hardware Intrerrupts in MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-Install-New-Hardware-Intrerrupts-in-MQX/m-p/205823#M4829</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nana.&lt;/P&gt;&lt;P&gt;Sorry for your hassles but thank you for sharing your code and experience.&amp;nbsp; It will benefit others trying to do the similar work.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Feb 2012 00:47:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-Install-New-Hardware-Intrerrupts-in-MQX/m-p/205823#M4829</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2012-02-15T00:47:54Z</dc:date>
    </item>
    <item>
      <title>Re: How to Install New Hardware Intrerrupts in MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-Install-New-Hardware-Intrerrupts-in-MQX/m-p/205824#M4830</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Now i have another problem after upgrade to CW 10.2 and MQX 3.8 it seems my ISR don't wana work any more, no one.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The problem is after installing the corresponding ISR in vector table , and reading ok the address for the ISR.&lt;/P&gt;&lt;P&gt;And writing to NVIC register to enable interrupts it seems is not working the MQX activates only the interrupt for timer ! And my interrupt for PORTE are disabled NVICSER2 all the time is 04 and must be 0x8000000 corresponding for PORTE int witch is 91.&lt;/P&gt;&lt;P&gt;And if i set in debug mode the corresponding registers for enable interrupts in NVIC, and activate it manually the ISR kernel Handler send me to the location of default_isr (this is running in desasambled code)&lt;/P&gt;&lt;P&gt;My question is the compiler make some optimization for the new version of CW?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Feb 2012 18:49:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-Install-New-Hardware-Intrerrupts-in-MQX/m-p/205824#M4830</guid>
      <dc:creator>Nana</dc:creator>
      <dc:date>2012-02-24T18:49:41Z</dc:date>
    </item>
    <item>
      <title>Re: How to Install New Hardware Intrerrupts in MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-Install-New-Hardware-Intrerrupts-in-MQX/m-p/205825#M4831</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nana,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;could you simply explain what is your intention with interrupts? I'm sorry but It's really hard to understand your post.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MartinK&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Feb 2012 20:35:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-Install-New-Hardware-Intrerrupts-in-MQX/m-p/205825#M4831</guid>
      <dc:creator>c0170</dc:creator>
      <dc:date>2012-02-24T20:35:44Z</dc:date>
    </item>
    <item>
      <title>Re: How to Install New Hardware Intrerrupts in MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-Install-New-Hardware-Intrerrupts-in-MQX/m-p/205826#M4832</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Now I made a simple new project where I want to use interrupts for Sw1 and Sw2 buttons on my twr-k60n512 board what are connected as ..&lt;/P&gt;&lt;P&gt;SW1 ----&amp;gt; PTA19&lt;/P&gt;&lt;P&gt;SW2 ----&amp;gt; PTE26&lt;/P&gt;&lt;P&gt;So&amp;nbsp;I made my configuration as SW1 used with MQX GPIO driver and installed interrupt with ioctl command. This seems to work OK. But the second one I want to install as a normal interrupt. So i activate the PIN interrupt and this is okey it's detecting de interrupt, because watching the registers in PORTE_PCR26 the interrupt flag is set when the button is pressed.&lt;/P&gt;&lt;P&gt;And in NVIC interrupt controller module is detecting de flag by seting the NVICSPR2 0x8000000&amp;nbsp;register with the bit coresponding to PORTE interup IRQ.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So the problem is the MQX don't install the ISR adress to my interrupt function&amp;nbsp;I belive: i'm geting all the time from install_isr function the address for default_isr &lt;IMG alt=":smileysad:" class="emoticon emoticon-smileysad" id="smileysad" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-sad.gif" title="Smiley Sad" /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here it is my code:&lt;/P&gt;&lt;PRE&gt;#include "main.h"#include &amp;lt;mqx.h&amp;gt;#include &amp;lt;bsp.h&amp;gt;typedef struct my_isr_struct{   pointer               OLD_ISR_DATA;   void      (_CODE_PTR_ OLD_ISR)(pointer);} MY_ISR_STRUCT, _PTR_ MY_ISR_STRUCT_PTR;TASK_TEMPLATE_STRUCT MQX_template_list[] ={/*  Task number, Entry point, Stack, Pri, String, Auto? */   {MAIN_TASK,   Main_task,   2000,  9,   "main", MQX_AUTO_START_TASK},   {0,           0,           0,     0,   0,      0,                 }};void sw2_isr(pointer data){printf("ISR Works\n");PORTE_ISFR=0xFFFFFFFF;}void gpio_init_isr_porte(void) {  SIM_SCGC5 |=SIM_SCGC5_PORTE_MASK;  PORTE_PCR26=PORT_PCR_MUX(1)|PORT_PCR_IRQC(0xA)|PORT_PCR_PE_MASK|PORT_PCR_PS_MASK; } void Main_task(uint_32 initial_data){  pointer result;MY_ISR_STRUCT_PTR  isr_ptr;gpio_init_isr_porte();isr_ptr = _mem_alloc_zero((_mem_size)sizeof(MY_ISR_STRUCT));isr_ptr-&amp;gt;OLD_ISR_DATA = _int_get_isr_data(INT_PORTE);   isr_ptr-&amp;gt;OLD_ISR      = _int_get_isr(INT_PORTE); result=_int_install_isr(INT_PORTE,( pointer )sw2_isr, isr_ptr);       if(result==NULL)       printf("Failed to install ISR");      else       if(result==_int_get_default_isr())       printf("Default ISR installed\n");       printf("ISR Installed = 0x%x",result);      NVICICPR2 = 1 &amp;lt;&amp;lt; (91%32);   NVICISER2 = 1 &amp;lt;&amp;lt; (91%32);   /*******************************   *    * START YOUR CODING HERE   *   ********************************/         for (;;)   {   }}/* EOF */&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Feb 2012 16:26:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-Install-New-Hardware-Intrerrupts-in-MQX/m-p/205826#M4832</guid>
      <dc:creator>Nana</dc:creator>
      <dc:date>2012-02-27T16:26:54Z</dc:date>
    </item>
    <item>
      <title>Re: How to Install New Hardware Intrerrupts in MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-Install-New-Hardware-Intrerrupts-in-MQX/m-p/205827#M4833</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nana,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;please check lwgpio example where one button is used in interrupt mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You have to set the interrupt level e, and unmask the interrupt in interrupt controller with a function&amp;nbsp;in your example code :&lt;/P&gt;&lt;P&gt;&amp;nbsp;_bsp_int_init(INT_PORTE, 3, 0, TRUE);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It works!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MartinK&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Feb 2012 22:31:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-Install-New-Hardware-Intrerrupts-in-MQX/m-p/205827#M4833</guid>
      <dc:creator>c0170</dc:creator>
      <dc:date>2012-02-27T22:31:31Z</dc:date>
    </item>
    <item>
      <title>Re: How to Install New Hardware Interrupts in MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-Install-New-Hardware-Intrerrupts-in-MQX/m-p/205828#M4834</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a question about interrupts: If exist a method to check if the all interrupts are enabled or not ?&lt;/P&gt;&lt;P&gt;Something like int_disabled have ben activa or int_enabled ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 May 2012 16:04:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-Install-New-Hardware-Intrerrupts-in-MQX/m-p/205828#M4834</guid>
      <dc:creator>Nana</dc:creator>
      <dc:date>2012-05-09T16:04:41Z</dc:date>
    </item>
    <item>
      <title>Re: How to Install New Hardware Interrupts in MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-Install-New-Hardware-Intrerrupts-in-MQX/m-p/205829#M4835</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;PRE&gt;isr_tempo = _mem_alloc_zero((_mem_size)sizeof(MY_ISR_STRUCT));;//alloca un po di memoria per gestire l'interrupt isr_tempo-&amp;gt;TICK_COUNT   = 0; isr_tempo-&amp;gt;OLD_ISR_DATA = _int_get_isr_data(BSP_TIMER_INTERRUPT_VECTOR); isr_tempo-&amp;gt;OLD_ISR      = _int_get_isr(BSP_TIMER_INTERRUPT_VECTOR);  _int_install_isr(BSP_TIMER_INTERRUPT_VECTOR, timer_isr, isr_tempo);void timer_isr(pointer user_isr_ptr){   MY_ISR_STRUCT_PTR  isr_ptr;   isr_ptr = (MY_ISR_STRUCT_PTR)user_isr_ptr;   isr_ptr-&amp;gt;TICK_COUNT++;       if(isr_ptr-&amp;gt;TICK_COUNT % 3)  colpi_tempo++;   // Chain to the previous notifier //   (*isr_ptr-&amp;gt;OLD_ISR)(isr_ptr-&amp;gt;OLD_ISR_DATA); //why isr_ptr-&amp;gt;OLD_ISR_DATA is NULL????}&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;SPAN&gt;But&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;also I have&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;a question&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;relating&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;to the example&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;of the&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;interrupt&lt;/SPAN&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Because&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;the example&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;calls&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;_int_get_isr_data&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;when&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;the return value is&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;NULL&lt;/SPAN&gt;&lt;SPAN&gt;?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 May 2012 17:21:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-Install-New-Hardware-Intrerrupts-in-MQX/m-p/205829#M4835</guid>
      <dc:creator>Britti1982</dc:creator>
      <dc:date>2012-05-25T17:21:18Z</dc:date>
    </item>
    <item>
      <title>Re: How to Install New Hardware Intrerrupts in MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-Install-New-Hardware-Intrerrupts-in-MQX/m-p/205830#M4836</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Simillar problem here i am facing. Only timer interrupt working. We are trying here for ADC Limit interrupt, but we are facing the problem in interrupt ISR. We are enabling the interrupt in ADC-&amp;gt;CR1, ADC-&amp;gt;CR2. and getting the interrupt for the same in Interrupt Mask register. It is not setting in IPR.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Below is sample code for code warrior CW 10 and MQX 4.0 given in $ Freescale_MQX_4_0\mqx\source\io\adc\mcf544xx&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;old_isr_adc1_param = _int_get_isr(BSP_ADC_INTERRUPT_VECTOR);&lt;/P&gt;&lt;P&gt;old_isr_adc1 = _int_install_isr(BSP_ADC_INTERRUPT_VECTOR, adc_complete_isr, NULL);&lt;/P&gt;&lt;P&gt;_mcf5441_int_init(BSP_ADC_INTERRUPT_VECTOR, BSP_ADC_INTERRUPT_LEVEL, TRUE);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kindly Help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Sep 2013 10:35:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-Install-New-Hardware-Intrerrupts-in-MQX/m-p/205830#M4836</guid>
      <dc:creator>pritam_bansod</dc:creator>
      <dc:date>2013-09-11T10:35:31Z</dc:date>
    </item>
  </channel>
</rss>