<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックRe: Shocket Shell bind</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Shocket-Shell-bind/m-p/202043#M4630</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kafre,&lt;/P&gt;&lt;P&gt;The C:\Program Files\Freescale\Freescale MQX 3.7\rtcs\examples\shell example has shell capability.&lt;/P&gt;&lt;P&gt;Once you load the example and run, then using the shell/UART interface you can configure the M54455EVB network parameters.&lt;/P&gt;&lt;P&gt;I made a "small" network from laptop to M54455EVB.&lt;/P&gt;&lt;P&gt;I set my laptop Ethernet port to a static IP (192.168.1.1) and then on the M54455EVB I setup it up as follows:&lt;/P&gt;&lt;P&gt;shell&amp;gt; help&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;-- the UART is the upper connection on back of M54455EVB&lt;/P&gt;&lt;P&gt;shell&amp;gt; ipconfig 0 init&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;-- initializes the Eth0 which is the port closes to bottom of M54455EVB&lt;/P&gt;&lt;P&gt;shell&amp;gt; ipconfig 0 staticip 192.168.1.2 255.255.255.0&lt;/P&gt;&lt;P&gt;shell&amp;gt; ping 192.168.1.1&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;-- to see that I could ping the laptop from M54455EVB&lt;/P&gt;&lt;P&gt;shell&amp;gt; telnetd start&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;-- to start the telnet server on M54455EVB&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;On the PC:&lt;/P&gt;&lt;P&gt;Start--&amp;gt;Run then type "cmd".&lt;/P&gt;&lt;P&gt;At shell prompt, I type "telnet 192.168.1.2"&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;-- this opens a telnet session&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 May 2011 00:02:43 GMT</pubDate>
    <dc:creator>DavidS</dc:creator>
    <dc:date>2011-05-10T00:02:43Z</dc:date>
    <item>
      <title>Shocket Shell bind</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Shocket-Shell-bind/m-p/202042#M4629</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using MQX 3.7 with CW for MCU 10.1 over a M54455EVB.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any way to bind a shell to a socket? &amp;nbsp;I mean to use a shell, as defined in the shell_test example, &amp;nbsp;with a manually created socket.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any example will be welcomed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Apr 2011 17:33:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Shocket-Shell-bind/m-p/202042#M4629</guid>
      <dc:creator>Kafre</dc:creator>
      <dc:date>2011-04-29T17:33:13Z</dc:date>
    </item>
    <item>
      <title>Re: Shocket Shell bind</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Shocket-Shell-bind/m-p/202043#M4630</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kafre,&lt;/P&gt;&lt;P&gt;The C:\Program Files\Freescale\Freescale MQX 3.7\rtcs\examples\shell example has shell capability.&lt;/P&gt;&lt;P&gt;Once you load the example and run, then using the shell/UART interface you can configure the M54455EVB network parameters.&lt;/P&gt;&lt;P&gt;I made a "small" network from laptop to M54455EVB.&lt;/P&gt;&lt;P&gt;I set my laptop Ethernet port to a static IP (192.168.1.1) and then on the M54455EVB I setup it up as follows:&lt;/P&gt;&lt;P&gt;shell&amp;gt; help&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;-- the UART is the upper connection on back of M54455EVB&lt;/P&gt;&lt;P&gt;shell&amp;gt; ipconfig 0 init&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;-- initializes the Eth0 which is the port closes to bottom of M54455EVB&lt;/P&gt;&lt;P&gt;shell&amp;gt; ipconfig 0 staticip 192.168.1.2 255.255.255.0&lt;/P&gt;&lt;P&gt;shell&amp;gt; ping 192.168.1.1&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;-- to see that I could ping the laptop from M54455EVB&lt;/P&gt;&lt;P&gt;shell&amp;gt; telnetd start&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;-- to start the telnet server on M54455EVB&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;On the PC:&lt;/P&gt;&lt;P&gt;Start--&amp;gt;Run then type "cmd".&lt;/P&gt;&lt;P&gt;At shell prompt, I type "telnet 192.168.1.2"&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;-- this opens a telnet session&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 May 2011 00:02:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Shocket-Shell-bind/m-p/202043#M4630</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2011-05-10T00:02:43Z</dc:date>
    </item>
    <item>
      <title>Re: Shocket Shell bind</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Shocket-Shell-bind/m-p/202044#M4631</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you DavidS,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But my question was oriented to a socket creation case. (Create Socket -&amp;gt; Bind Port -&amp;gt; Listen -&amp;gt; Wait for event...) I will try the Telnet solution. Thanks, again.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 May 2011 14:47:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Shocket-Shell-bind/m-p/202044#M4631</guid>
      <dc:creator>Kafre</dc:creator>
      <dc:date>2011-05-12T14:47:19Z</dc:date>
    </item>
  </channel>
</rss>