<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Booting with external flash? in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Booting-with-external-flash/m-p/201407#M4554</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using the M52259EVB with MQX 3.5 and Codewarrior Eclipse IDE.&amp;nbsp; My application is larger than the internal flash memory, so I was wondering if it is possible to boot from an external flash device like a CF card or a USB memory stick.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I saw that with the M54455EVB there is external flash on board that you can boot from.&amp;nbsp; Is it possible to do something similar with the M52259, but using CF card or USB stick as the source of external flash instead?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 30 Jan 2012 00:43:28 GMT</pubDate>
    <dc:creator>njk909</dc:creator>
    <dc:date>2012-01-30T00:43:28Z</dc:date>
    <item>
      <title>Booting with external flash?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Booting-with-external-flash/m-p/201407#M4554</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using the M52259EVB with MQX 3.5 and Codewarrior Eclipse IDE.&amp;nbsp; My application is larger than the internal flash memory, so I was wondering if it is possible to boot from an external flash device like a CF card or a USB memory stick.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I saw that with the M54455EVB there is external flash on board that you can boot from.&amp;nbsp; Is it possible to do something similar with the M52259, but using CF card or USB stick as the source of external flash instead?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jan 2012 00:43:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Booting-with-external-flash/m-p/201407#M4554</guid>
      <dc:creator>njk909</dc:creator>
      <dc:date>2012-01-30T00:43:28Z</dc:date>
    </item>
    <item>
      <title>Re: Booting with external flash?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Booting-with-external-flash/m-p/201408#M4555</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi njk909,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;On m52259evb, there is MRAM IC on board that can be used. In general, any memory that can be accessed by external bus could be used for memory capacity expansion.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MartinK&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jan 2012 19:34:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Booting-with-external-flash/m-p/201408#M4555</guid>
      <dc:creator>c0170</dc:creator>
      <dc:date>2012-01-30T19:34:13Z</dc:date>
    </item>
    <item>
      <title>Re: Booting with external flash?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Booting-with-external-flash/m-p/201409#M4556</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi njk909,&lt;/P&gt;&lt;P&gt;The MCF52259 is combined MCU (has intergrated flash and sram) and MPU (support extermal memory devices like MRAM, SRAM, and NOR flash).&lt;/P&gt;&lt;P&gt;The MPU mode can boot from external devices like MRAM (as&amp;nbsp;MartinK mentioned) and NOR flash but does not have the ability/capability to boot from USB or compact flash, or serial flash.&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jan 2012 23:17:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Booting-with-external-flash/m-p/201409#M4556</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2012-01-30T23:17:39Z</dc:date>
    </item>
  </channel>
</rss>