<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RTOS independant ISR in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/RTOS-independant-ISR/m-p/150928#M453</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Check your vector table if it is correct. Then, check the interrupt controller settings (interrupt mask bit, interrupt mask all bit).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 01 Oct 2010 15:59:07 GMT</pubDate>
    <dc:creator>JuroV</dc:creator>
    <dc:date>2010-10-01T15:59:07Z</dc:date>
    <item>
      <title>RTOS independant ISR</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/RTOS-independant-ISR/m-p/150925#M450</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need to have a direct interrupt, which means MQX RTOS must not drive this interrupt. These interrupts come from Input Capture on all DMA and GPT pins. I managed to solve the problem using codewarrior 7.1 and MQX 3.3 and the following code. Unfortunately this is not working on Codewarrior 7.2 and MQX 3.61. What could I be missing? or what changes on MQX and compiler might affect the behavior of a working code?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;extern void main_task(uint_32);const TASK_TEMPLATE_STRUCT  MQX_template_list[] = {    /* Task Index,   Function,   Stack,  Priority, Name,     Attributes,          Param, Time Slice */    { MAIN_TASK,   main_task, 1500,   5,        "main",  MQX_AUTO_START_TASK, 0,     0 },    { 0 }};__declspec(interrupt:0) void DMA_T3_ISR(pointer dummy_param){   VMCF5225_STRUCT_PTR reg_ptr = (VMCF5225_STRUCT_PTR)BSP_IPSBAR;      reg_ptr-&amp;gt;DMA_TIMER[ 3 ].DTER =  0b00000011; //Apaga las Banderas de Interrupcion}__declspec(interrupt:0) void DMA_T2_ISR(pointer dummy_param){   VMCF5225_STRUCT_PTR reg_ptr = (VMCF5225_STRUCT_PTR)BSP_IPSBAR;      reg_ptr-&amp;gt;DMA_TIMER[ 2 ].DTER =  0b00000011; //Apaga las Banderas de Interrupcion}/*Prueba para lector y tarjeta juntos*/__declspec(interrupt:0) void DMA_T1_ISR(pointer dummy_param){   VMCF5225_STRUCT_PTR reg_ptr = (VMCF5225_STRUCT_PTR)BSP_IPSBAR;      reg_ptr-&amp;gt;DMA_TIMER[ 1 ].DTER =  0b00000011; //Apaga las Banderas de Interrupcion}__declspec(interrupt:0) void DMA_T0_ISR(pointer dummy_param){   VMCF5225_STRUCT_PTR reg_ptr = (VMCF5225_STRUCT_PTR)BSP_IPSBAR;      reg_ptr-&amp;gt;DMA_TIMER[ 0 ].DTER =  0b00000011; //Apaga las Banderas de Interrupcion}void main_task   (      uint_32 initial_data   ){VMCF5225_STRUCT_PTR reg_ptr = (VMCF5225_STRUCT_PTR)BSP_IPSBAR;     reg_ptr-&amp;gt;GPIO.PORTTC = 0x00;  /*GPIO Configuration for DMA Edge Triggered Interrupt 0 = Output low level*/     reg_ptr-&amp;gt;GPIO.DDRTC = 0x00;   /*GPIO Configuration for DMA Edge Triggered Interrupt 0 = Direction Input*/     reg_ptr-&amp;gt;GPIO.PORTTCP_SETTC = 0x00;  /*GPIO Configuration for DMA Edge Triggered Interrupt Nothing since it is input*/     reg_ptr-&amp;gt;GPIO.CLRTC = 0x00;   /*GPIO Configuration for DMA Edge Triggered Interrupt Nothing since it is input*/     reg_ptr-&amp;gt;GPIO.PTCPAR = 0x55;  /*GPIO Configuration for DMA Edge Triggered Interrupt Primary Function for all DTIM pins*/  reg_ptr-&amp;gt;ICTRL0.ICR[19] = 0b01110011;  //DES DMA_Timer[0] set to IL=7, IP=3     reg_ptr-&amp;gt;ICTRL0.ICR[20] = 0b01110010;  //DES DMA_Timer[1] set to IL=7, IP=2     reg_ptr-&amp;gt;ICTRL0.ICR[21] = 0b01110001;  //DES DMA_Timer[2] set to IL=7, IP=1  reg_ptr-&amp;gt;ICTRL0.ICR[22] = 0b01110000;  //DES DMA_Timer[3] set to IL=7, IP=0    reg_ptr-&amp;gt;DMA_TIMER[ 0 ].DTMR =  0b0000000010000011;   reg_ptr-&amp;gt;DMA_TIMER[ 1 ].DTMR =  0b0000000010000011;   reg_ptr-&amp;gt;DMA_TIMER[ 2 ].DTMR =  0b0000000010000011;      reg_ptr-&amp;gt;DMA_TIMER[ 3 ].DTMR =  0b0000000010000011;           reg_ptr-&amp;gt;DMA_TIMER[ 0 ].DTXTMR = 0b01000000;//Everything Zero in order to:     reg_ptr-&amp;gt;DMA_TIMER[ 1 ].DTXTMR = 0b01000000;//1.- Have the timer increment by one     reg_ptr-&amp;gt;DMA_TIMER[ 2 ].DTXTMR = 0b01000000;//2.- Interrupt Enabled and DMA request disabled     reg_ptr-&amp;gt;DMA_TIMER[ 3 ].DTXTMR = 0b01000000;//3.- Timer Continues if core halts ( Dont need this feature , just trying to see if it works like this)     reg_ptr-&amp;gt;DMA_TIMER[ 0 ].DTER =  0b00000011;  //Clear event condition     reg_ptr-&amp;gt;DMA_TIMER[ 1 ].DTER =  0b00000011;  //Clear event condition     reg_ptr-&amp;gt;DMA_TIMER[ 2 ].DTER =  0b00000011;  //Clear event condition     reg_ptr-&amp;gt;DMA_TIMER[ 3 ].DTER =  0b00000011;  //Clear event condition     reg_ptr-&amp;gt;DMA_TIMER[ 0 ].DTCN =  0x0000;       reg_ptr-&amp;gt;DMA_TIMER[ 1 ].DTCN =  0x0000;      reg_ptr-&amp;gt;DMA_TIMER[ 2 ].DTCN =  0x0000;      reg_ptr-&amp;gt;DMA_TIMER[ 3 ].DTCN =  0x0000;      *(unsigned int *) 0x2000014C = (unsigned int)&amp;amp;DMA_T0_ISR; //Install direct ISR vector for DTIM3     *(unsigned int *) 0x20000150 = (unsigned int)&amp;amp;DMA_T1_ISR; //Install direct ISR vector for DTIM3     *(unsigned int *) 0x20000154 = (unsigned int)&amp;amp;DMA_T2_ISR; //Install direct ISR vector for DTIM3  *(unsigned int *) 0x20000158 = (unsigned int)&amp;amp;DMA_T3_ISR; //Install direct ISR vector for DTIM3     _interrupt_controller_unmask(MCF5225_INT_DTIM0); //DES unmask DTIM3     _interrupt_controller_unmask(MCF5225_INT_DTIM1); //DES unmask DTIM3     _interrupt_controller_unmask(MCF5225_INT_DTIM2); //DES unmask DTIM3     _interrupt_controller_unmask(MCF5225_INT_DTIM3); //DES unmask DTIM3         while(1)   {       _time_delay(200);      }}&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Oct 2020 08:53:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/RTOS-independant-ISR/m-p/150925#M450</guid>
      <dc:creator>MQXuser</dc:creator>
      <dc:date>2020-10-29T08:53:55Z</dc:date>
    </item>
    <item>
      <title>Re: RTOS independant ISR</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/RTOS-independant-ISR/m-p/150926#M451</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Do yo get error in making the project or doesn't it work at all?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can take a look at &lt;A __default_attr="69487" class="jive_macro jive_macro_thread default_title" href="https://community.freescale.com/thread/69487" jivemacro="thread" title="this"&gt;this&lt;/A&gt;....&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do you have MQX_ROM_VECTORS set to 1 in user_config.h?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Marco&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 25 Sep 2010 23:27:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/RTOS-independant-ISR/m-p/150926#M451</guid>
      <dc:creator>LordMark</dc:creator>
      <dc:date>2010-09-25T23:27:02Z</dc:date>
    </item>
    <item>
      <title>Re: RTOS independant ISR</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/RTOS-independant-ISR/m-p/150927#M452</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The project builds and programs correctly but interrupts are never called.&lt;/P&gt;&lt;P&gt;I checked the thread you mention but I know the registers are correctly configured so that is not part of the problem.&lt;/P&gt;&lt;P&gt;I had&amp;nbsp; MQX_ROM_VECTORS = 0 but then I changed it to 1 and the problem continues.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Sep 2010 21:22:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/RTOS-independant-ISR/m-p/150927#M452</guid>
      <dc:creator>MQXuser</dc:creator>
      <dc:date>2010-09-27T21:22:42Z</dc:date>
    </item>
    <item>
      <title>Re: RTOS independant ISR</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/RTOS-independant-ISR/m-p/150928#M453</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Check your vector table if it is correct. Then, check the interrupt controller settings (interrupt mask bit, interrupt mask all bit).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Oct 2010 15:59:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/RTOS-independant-ISR/m-p/150928#M453</guid>
      <dc:creator>JuroV</dc:creator>
      <dc:date>2010-10-01T15:59:07Z</dc:date>
    </item>
  </channel>
</rss>