<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software Solutionsのトピックegui image loading</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/egui-image-loading/m-p/194558#M3997</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there a simple way to load images from another type of flash device without having to copy them to local flash? &amp;nbsp;If I had some images on an sd card, usb, or some other serial flash, how can I load these as I need them without declaring them as part of the screen before hand?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 Jan 2012 07:01:02 GMT</pubDate>
    <dc:creator>Toe</dc:creator>
    <dc:date>2012-01-05T07:01:02Z</dc:date>
    <item>
      <title>egui image loading</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/egui-image-loading/m-p/194558#M3997</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there a simple way to load images from another type of flash device without having to copy them to local flash? &amp;nbsp;If I had some images on an sd card, usb, or some other serial flash, how can I load these as I need them without declaring them as part of the screen before hand?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Jan 2012 07:01:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/egui-image-loading/m-p/194558#M3997</guid>
      <dc:creator>Toe</dc:creator>
      <dc:date>2012-01-05T07:01:02Z</dc:date>
    </item>
    <item>
      <title>Re: egui image loading</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/egui-image-loading/m-p/194559#M3998</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;the new version (not released yet) support external bitmap *.BMP file.&lt;BR /&gt;&lt;BR /&gt;You can look at it in this thread:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.freescale.com/message/100414#100414" title="https://community.freescale.com/message/100414#100414"&gt;https://community.freescale.com/message/100414#100414&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Jan 2012 17:14:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/egui-image-loading/m-p/194559#M3998</guid>
      <dc:creator>Gargy</dc:creator>
      <dc:date>2012-01-05T17:14:11Z</dc:date>
    </item>
  </channel>
</rss>