<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Moving an MQX project using IAR 6.21 ?? in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Moving-an-MQX-project-using-IAR-6-21/m-p/192970#M3905</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Newbie question:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using the K60N512 board under IAR 6.21.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've gotten several MQX supplied examples to run out of the box (for example, mqx/examples/tfs). When I load up the app and start the debugger, the app starts at the mqx_main function.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, simply moving the tfs directory elsewhere and changing the include and linker paths in IAR results in the app starting with the main: label. It doesn't appear to start MQX at all.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm sure there's an easy fix, but it's evaded me for some time. Help?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Mark Miller&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Dec 2011 01:08:34 GMT</pubDate>
    <dc:creator>Chalkboard</dc:creator>
    <dc:date>2011-12-28T01:08:34Z</dc:date>
    <item>
      <title>Moving an MQX project using IAR 6.21 ??</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Moving-an-MQX-project-using-IAR-6-21/m-p/192970#M3905</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Newbie question:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using the K60N512 board under IAR 6.21.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've gotten several MQX supplied examples to run out of the box (for example, mqx/examples/tfs). When I load up the app and start the debugger, the app starts at the mqx_main function.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, simply moving the tfs directory elsewhere and changing the include and linker paths in IAR results in the app starting with the main: label. It doesn't appear to start MQX at all.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm sure there's an easy fix, but it's evaded me for some time. Help?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Mark Miller&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Dec 2011 01:08:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Moving-an-MQX-project-using-IAR-6-21/m-p/192970#M3905</guid>
      <dc:creator>Chalkboard</dc:creator>
      <dc:date>2011-12-28T01:08:34Z</dc:date>
    </item>
    <item>
      <title>Re: Moving an MQX project using IAR 6.21 ??</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Moving-an-MQX-project-using-IAR-6-21/m-p/192971#M3906</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Chalkboard,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;this could be helpfull for you how to create your own project, there's document attached in second post.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A __default_attr="94698" class="jive_macro jive_macro_thread default_title" href="https://community.freescale.com/thread/94698" jivemacro="thread" title="https://community.freescale.com/thread/94698"&gt;https://community.freescale.com/thread/94698&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Back to your issue, I don't see any problem you possibly could have if it compiled and linked properly. I can't run IAR at the moment, got some issues with a computer :smileyhappy:&lt;/P&gt;&lt;P&gt;There is MQX plugin, you can check many information about MQX as task, memory , etc.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MartinK&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Dec 2011 03:15:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Moving-an-MQX-project-using-IAR-6-21/m-p/192971#M3906</guid>
      <dc:creator>c0170</dc:creator>
      <dc:date>2011-12-29T03:15:29Z</dc:date>
    </item>
  </channel>
</rss>