<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックBreakpoint warning</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Breakpoint-warning/m-p/192948#M3895</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I am using cw 10.0 and MQX 3.6.2. I have 4 breakpoints and when I start the debugger I receive the following " breakpoint warning unable set all the breakpoints requested...." No information on which breakpoint is causing the issue. How do I determine which breakpoint is causing the problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 Mar 2011 19:54:57 GMT</pubDate>
    <dc:creator>barbercolman</dc:creator>
    <dc:date>2011-03-23T19:54:57Z</dc:date>
    <item>
      <title>Breakpoint warning</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Breakpoint-warning/m-p/192948#M3895</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I am using cw 10.0 and MQX 3.6.2. I have 4 breakpoints and when I start the debugger I receive the following " breakpoint warning unable set all the breakpoints requested...." No information on which breakpoint is causing the issue. How do I determine which breakpoint is causing the problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Mar 2011 19:54:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Breakpoint-warning/m-p/192948#M3895</guid>
      <dc:creator>barbercolman</dc:creator>
      <dc:date>2011-03-23T19:54:57Z</dc:date>
    </item>
    <item>
      <title>Re: Breakpoint warning</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Breakpoint-warning/m-p/192949#M3896</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can only set 4 active breakpoints at same time. This is a hardware limitation in same MCU&lt;/P&gt;&lt;P&gt;see&amp;nbsp;&lt;A href="http://cache.freescale.com/files/32bit/doc/data_sheet/MCF52259.pdf?fpsp=1" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/32bit/doc/data_sheet/MCF52259.pdf?fpsp=1&lt;/A&gt;&amp;nbsp;page 5, section&amp;nbsp;&amp;nbsp;System debug support.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Mar 2011 21:12:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Breakpoint-warning/m-p/192949#M3896</guid>
      <dc:creator>madifazio</dc:creator>
      <dc:date>2011-03-23T21:12:23Z</dc:date>
    </item>
    <item>
      <title>Re: Breakpoint warning</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Breakpoint-warning/m-p/192950#M3897</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've discovered and worked around the max four breakpoints, but I have discovered that many of my breakpoints don't seem to get triggered.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As well as I can tell, any breakpoint that is deeper than one function call into the mqx libraries from my application won't trigger.&amp;nbsp; Tracing takes me through the same code, so I believe the breakpoint should be triggered when I hit F8, but no joy.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So with a call stack like: AppFunction()-&amp;gt;mqxFunction0()-&amp;gt;mqxFunction2()-&amp;gt;mqxFunction3() I find that the processor breaks on breakpoints in AppFunction() and the entry to mqxFunction0().&amp;nbsp; Breakpoints in any of mqxFunction2() or mqxFunction3() never break.&amp;nbsp; But if I trace, i can follow the entire flow, step in, step return, run-to-line all work in mqxFunction2() and mqxFunction3() but no breakpoints.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Apr 2011 06:10:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Breakpoint-warning/m-p/192950#M3897</guid>
      <dc:creator>dhlocker</dc:creator>
      <dc:date>2011-04-11T06:10:41Z</dc:date>
    </item>
  </channel>
</rss>