<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software Solutions中的主题 LWTimer reset?</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/LWTimer-reset/m-p/191485#M3743</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want a timer that after 3 seconds with out user input the UI is reset. I can start a 3 second timer, but I do not see any way of resetting the timer to 3 seconds. Is there another option to canceling and restarting a timer?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;MQX 3.6.2&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 16 Mar 2011 20:35:18 GMT</pubDate>
    <dc:creator>barbercolman</dc:creator>
    <dc:date>2011-03-16T20:35:18Z</dc:date>
    <item>
      <title>LWTimer reset?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/LWTimer-reset/m-p/191485#M3743</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want a timer that after 3 seconds with out user input the UI is reset. I can start a 3 second timer, but I do not see any way of resetting the timer to 3 seconds. Is there another option to canceling and restarting a timer?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;MQX 3.6.2&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Mar 2011 20:35:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/LWTimer-reset/m-p/191485#M3743</guid>
      <dc:creator>barbercolman</dc:creator>
      <dc:date>2011-03-16T20:35:18Z</dc:date>
    </item>
    <item>
      <title>Re: LWTimer reset?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/LWTimer-reset/m-p/191486#M3744</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Barber,&lt;/P&gt;&lt;P&gt;The lightweight timer is a very simple and limited capability timer module as compared to the full timer operations.&amp;nbsp; The full timer can be setup as a one shot occurence or periodic with a bunch of other capabilities.&lt;/P&gt;&lt;P&gt;Once you start a lightweight timer at whatever periodic rate you want you can cancel it using the _lwtimer_cancel_timer() function call.&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Mar 2011 02:00:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/LWTimer-reset/m-p/191486#M3744</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2011-03-18T02:00:01Z</dc:date>
    </item>
  </channel>
</rss>