<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックRe: SD card demo</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/SD-card-demo/m-p/188497#M3517</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;TWRK60N512 MQX 3.7&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 08 Dec 2011 02:12:06 GMT</pubDate>
    <dc:creator>ronysha</dc:creator>
    <dc:date>2011-12-08T02:12:06Z</dc:date>
    <item>
      <title>SD card demo</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/SD-card-demo/m-p/188495#M3515</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When running the SD card demo (mfs_sdcard) I can get up to the following place:&lt;/P&gt;&lt;P&gt;sdcard_handle = fopen("sdcard:", 0);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if ( sdcard_handle == NULL )&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf("Unable to open SD card device.\n");&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; _task_block();&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;Here it fails and I get the error message :Unable to open SD card device.&lt;/P&gt;&lt;P&gt;I configured user_config.h as required.&lt;/P&gt;&lt;P&gt;Are there any hw switches I have to change to access the card?&lt;/P&gt;&lt;P&gt;I can access the card from the PC w/o any problems.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Dec 2011 17:14:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/SD-card-demo/m-p/188495#M3515</guid>
      <dc:creator>ronysha</dc:creator>
      <dc:date>2011-12-07T17:14:24Z</dc:date>
    </item>
    <item>
      <title>Re: SD card demo</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/SD-card-demo/m-p/188496#M3516</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ronysha,&lt;/P&gt;&lt;P&gt;Which processor and which version of MQX are you using?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Dec 2011 22:56:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/SD-card-demo/m-p/188496#M3516</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2011-12-07T22:56:19Z</dc:date>
    </item>
    <item>
      <title>Re: SD card demo</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/SD-card-demo/m-p/188497#M3517</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;TWRK60N512 MQX 3.7&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Dec 2011 02:12:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/SD-card-demo/m-p/188497#M3517</guid>
      <dc:creator>ronysha</dc:creator>
      <dc:date>2011-12-08T02:12:06Z</dc:date>
    </item>
    <item>
      <title>Re: SD card demo</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/SD-card-demo/m-p/188498#M3518</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ronysha,&lt;/P&gt;&lt;P&gt;I made mod to user_config.h (made the #define BSPCFG_ENABLE_ESDHC 1), then recompiled the BSP,PSP,MFS, and then example/application).&lt;/P&gt;&lt;P&gt;It works for me.&lt;/P&gt;&lt;P&gt;I'm using the TWRK60 and TWRSER cards.&lt;/P&gt;&lt;P&gt;TWRK60 jumpers: J1 in, J6=2-3, J8 in, J9=1-2&lt;/P&gt;&lt;P&gt;TWRSER jumpers: J2=3-4, J3=2-3, J10=1-2, J11=5-6, J12=9-10, J16=1-2 and 5-6, J15=1-2, J17=1-2, J19=1-2&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Dec 2011 00:49:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/SD-card-demo/m-p/188498#M3518</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2011-12-09T00:49:14Z</dc:date>
    </item>
    <item>
      <title>Re: SD card demo</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/SD-card-demo/m-p/188499#M3519</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I did as you said and was able to get over that point.&lt;/P&gt;&lt;P&gt;Now I get the message: File system not mounted.&lt;/P&gt;&lt;P&gt;What am I doing wrong now?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Dec 2011 19:50:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/SD-card-demo/m-p/188499#M3519</guid>
      <dc:creator>ronysha</dc:creator>
      <dc:date>2011-12-09T19:50:17Z</dc:date>
    </item>
    <item>
      <title>Re: SD card demo</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/SD-card-demo/m-p/188500#M3520</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ronysha,&lt;/P&gt;&lt;P&gt;Sounds like it is close!&amp;nbsp; I recommend doing a total clean of the software....so do a clean on each project (BSP,PSP,MSF,Shell and application) then rebuild them all.&amp;nbsp; Make sure if you build for the Debug target that the application is built for Debug target too.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If that doesn't work I've attach my elf file, s-record, and map file in the attached ZIP.&amp;nbsp; You can compare the map file to yours.&amp;nbsp; You can also program my elf or s-record on your hardware to see if the hardware is good.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sorry for the hassles.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Dec 2011 22:56:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/SD-card-demo/m-p/188500#M3520</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2011-12-09T22:56:33Z</dc:date>
    </item>
  </channel>
</rss>