<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックUsing shell examples with terminal I/o</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Using-shell-examples-with-terminal-I-o/m-p/188426#M3496</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using IAR. In order to use the terminal I/o of the tool instead of external terminal e.g.. pemicro I have to do some settings.&lt;/P&gt;&lt;P&gt;I am able to&amp;nbsp; force the printf and gets functions to use the terminal I/O (by commenting the #define printf of fio.h).&lt;/P&gt;&lt;P&gt;But shell.c printf and similar commands still try to access the uart. How can I force them to approach the terminal I/o too?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Dec 2011 16:39:29 GMT</pubDate>
    <dc:creator>ronysha</dc:creator>
    <dc:date>2011-12-07T16:39:29Z</dc:date>
    <item>
      <title>Using shell examples with terminal I/o</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Using-shell-examples-with-terminal-I-o/m-p/188426#M3496</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using IAR. In order to use the terminal I/o of the tool instead of external terminal e.g.. pemicro I have to do some settings.&lt;/P&gt;&lt;P&gt;I am able to&amp;nbsp; force the printf and gets functions to use the terminal I/O (by commenting the #define printf of fio.h).&lt;/P&gt;&lt;P&gt;But shell.c printf and similar commands still try to access the uart. How can I force them to approach the terminal I/o too?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Dec 2011 16:39:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Using-shell-examples-with-terminal-I-o/m-p/188426#M3496</guid>
      <dc:creator>ronysha</dc:creator>
      <dc:date>2011-12-07T16:39:29Z</dc:date>
    </item>
    <item>
      <title>Re: Using shell examples with terminal I/o</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Using-shell-examples-with-terminal-I-o/m-p/188427#M3497</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi ronysha,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;there is IODEBUG feature in MQX 3.8 which uses ide terminal. If it is enabled in user_config.h and board.h selected as default, everything is printed to the i/o terminal.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MartinK&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Dec 2011 22:34:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Using-shell-examples-with-terminal-I-o/m-p/188427#M3497</guid>
      <dc:creator>c0170</dc:creator>
      <dc:date>2011-12-22T22:34:32Z</dc:date>
    </item>
  </channel>
</rss>