<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックNeed SPI drivers for MPC5125</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Need-SPI-drivers-for-MPC5125/m-p/187800#M3421</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am running the TWR-MPC5125 with the Linear Tech TWR-ADCDAC-LTC board. In order to run the ADC board, the MPC5125 needs to generate SPI signals. However, examination of the MQX code for the TWR-MPC5125 shows that all PSCs are set to be UARTs. I can see how to set the PSC to SPI mode, but actually using it is a bit more puzzling. What I need is a driver so that I can issue ioctl calls to the SPI chip, similar to what is available in the code for the TWR-MCF52259:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;_mcf5xxx_qspi_int_install("ispi0:", &amp;amp;_bsp_qspi0_init);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;in mqx/source/bsp/twrmcf52259/init_bsp.c.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How can I get such a driver?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Mar 2011 06:55:27 GMT</pubDate>
    <dc:creator>FrankB</dc:creator>
    <dc:date>2011-03-03T06:55:27Z</dc:date>
    <item>
      <title>Need SPI drivers for MPC5125</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Need-SPI-drivers-for-MPC5125/m-p/187800#M3421</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am running the TWR-MPC5125 with the Linear Tech TWR-ADCDAC-LTC board. In order to run the ADC board, the MPC5125 needs to generate SPI signals. However, examination of the MQX code for the TWR-MPC5125 shows that all PSCs are set to be UARTs. I can see how to set the PSC to SPI mode, but actually using it is a bit more puzzling. What I need is a driver so that I can issue ioctl calls to the SPI chip, similar to what is available in the code for the TWR-MCF52259:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;_mcf5xxx_qspi_int_install("ispi0:", &amp;amp;_bsp_qspi0_init);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;in mqx/source/bsp/twrmcf52259/init_bsp.c.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How can I get such a driver?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Mar 2011 06:55:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Need-SPI-drivers-for-MPC5125/m-p/187800#M3421</guid>
      <dc:creator>FrankB</dc:creator>
      <dc:date>2011-03-03T06:55:27Z</dc:date>
    </item>
    <item>
      <title>Re: Need SPI drivers for MPC5125</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Need-SPI-drivers-for-MPC5125/m-p/187801#M3422</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi FrankB,&lt;/P&gt;&lt;P&gt;Later this month there will be a FSLMQX3.7Beta release that will have the SPI driver support if you can wait.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Mar 2011 06:53:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Need-SPI-drivers-for-MPC5125/m-p/187801#M3422</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2011-03-04T06:53:33Z</dc:date>
    </item>
  </channel>
</rss>