<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックUSB Debug with TWR-K60N512</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/USB-Debug-with-TWR-K60N512/m-p/185831#M3206</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am testing the Kinetis60 tower with the USB connector and the IAR Embedded Workbench IDE.&amp;nbsp; I have not been able to connect/debug/download code via the USB (OSBDM).&amp;nbsp; The drivers are installed on my computer but I get the following error message when I try to connect:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;"Fatal Error: Can not connect to J-Link via USB"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I attempted to try to configure the Project-&amp;gt;Options-&amp;gt;Debugger to other drivers, but was unsuccessful.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does anyone know the settings to allow the IAR to connect via USB?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 24 Feb 2011 03:37:58 GMT</pubDate>
    <dc:creator>davidcav</dc:creator>
    <dc:date>2011-02-24T03:37:58Z</dc:date>
    <item>
      <title>USB Debug with TWR-K60N512</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/USB-Debug-with-TWR-K60N512/m-p/185831#M3206</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am testing the Kinetis60 tower with the USB connector and the IAR Embedded Workbench IDE.&amp;nbsp; I have not been able to connect/debug/download code via the USB (OSBDM).&amp;nbsp; The drivers are installed on my computer but I get the following error message when I try to connect:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;"Fatal Error: Can not connect to J-Link via USB"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I attempted to try to configure the Project-&amp;gt;Options-&amp;gt;Debugger to other drivers, but was unsuccessful.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does anyone know the settings to allow the IAR to connect via USB?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Feb 2011 03:37:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/USB-Debug-with-TWR-K60N512/m-p/185831#M3206</guid>
      <dc:creator>davidcav</dc:creator>
      <dc:date>2011-02-24T03:37:58Z</dc:date>
    </item>
    <item>
      <title>Re: USB Debug with TWR-K60N512</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/USB-Debug-with-TWR-K60N512/m-p/185832#M3207</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Davidcav,&lt;/P&gt;&lt;P&gt;Some of the IAR projects default to using the JLINK JTAG debugger interface.&amp;nbsp; When Kinetis was first out and being tested that was the only debugger interface available.&lt;/P&gt;&lt;P&gt;Now the OSJTAG from P&amp;amp;E is used on the Tower.&lt;/P&gt;&lt;P&gt;Highlight your application project and select Options.&lt;/P&gt;&lt;P&gt;Then click onthe Debugger Category.&lt;/P&gt;&lt;P&gt;Set the Driver to PE micro.&lt;/P&gt;&lt;P&gt;Click OK.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Feb 2011 22:40:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/USB-Debug-with-TWR-K60N512/m-p/185832#M3207</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2011-02-24T22:40:03Z</dc:date>
    </item>
  </channel>
</rss>