<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Problem Configuring New Set Up with CW 10.1 and MQX 3.7.0 EAR - Build Fixed, now trying to Progr in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-Configuring-New-Set-Up-with-CW-10-1-and-MQX-3-7-0-EAR/m-p/185510#M3146</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mykepredko,&lt;/P&gt;&lt;P&gt;Sorry for delay...my computer had virus.&lt;/P&gt;&lt;P&gt;Often when I have connection issue with a project I will try to step back and either use another version of CodeWarrior (easy for me but if you have older one handy) or try to find an exiting project (FSLMQX/mqx/examples/hello) or create a new baremetal project for the processor.&amp;nbsp; A trouble project sometimes is very difficult to debug since they have soooo many settings that could go wrong.&lt;/P&gt;&lt;P&gt;Please try to run existing project or create a new baremetal project for the processor and see if that allows you to connect.&lt;/P&gt;&lt;P&gt;Assuming it does then either you can compare the configuration windows (fun...not) or create a new project as similar to the one you are debugging and pull your code base into the working project.&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 Mar 2011 06:20:42 GMT</pubDate>
    <dc:creator>DavidS</dc:creator>
    <dc:date>2011-03-02T06:20:42Z</dc:date>
    <item>
      <title>Problem Configuring New Set Up with CW 10.1 and MQX 3.7.0 EAR</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-Configuring-New-Set-Up-with-CW-10-1-and-MQX-3-7-0-EAR/m-p/185506#M3142</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Folks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm porting my ColdFire MQX application over to Kinetis and I', hitting a bit of a brick wall&amp;nbsp;when I try to build an existing CF application and then when I can see it working, I’ll port it to the Kinetis.&amp;nbsp; &amp;nbsp; First off, the path information for compiling isn’t correct&amp;nbsp;– it looks like the installation for CW and MQX isn’t 100%.&amp;nbsp; To get the code to build, in the Project Properties&amp;nbsp;I had to:&lt;/P&gt;&lt;TABLE border="0" cellpadding="0" cellspacing="0"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;Add "Include Directory" for C Source Files: "${MQX_PATH}/m522223evb.cw10/psp&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;Add "Include Directory" for C Source Files: "${MQX_PATH}/m522223evb.cw10/bsp after psp&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;Now, the compilation works okay, but I am getting the error: &amp;nbsp;&lt;/P&gt;&lt;P&gt;C:\Program Files\Freescale\CW MCU v10.1\gnu\bin\make: *** No rule to make target `C:/Freescale MQX 3.7 EAR/lib/m52223evb.cw10/mqx/intflash.lcf', needed by `Blink5.elf'.&amp;nbsp; Stop. &amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried inserting:&lt;/P&gt;&lt;TABLE border="0" cellpadding="0" cellspacing="0"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;Add "Include Directory" for Object File: "${MQX_PATH}/m522223evb.cw10/bsp&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;because I thought this is where the linker picks up the object location and there isn’t any “mqx” folder under the “m52223evb.cw10” folder.&amp;nbsp; I don’t see anywhere else where this can be done.&amp;nbsp; Any ideas?&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanx, &amp;nbsp;&lt;/P&gt;&lt;P&gt;myke&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Feb 2011 04:02:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-Configuring-New-Set-Up-with-CW-10-1-and-MQX-3-7-0-EAR/m-p/185506#M3142</guid>
      <dc:creator>mykepredko</dc:creator>
      <dc:date>2011-02-23T04:02:31Z</dc:date>
    </item>
    <item>
      <title>Problem Configuring New Set Up with CW 10.1 and MQX 3.7.0 EAR - Build Fixed, now trying to Program</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-Configuring-New-Set-Up-with-CW-10-1-and-MQX-3-7-0-EAR/m-p/185507#M3143</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey Folks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Moving along, I discovered that you need to do the following to get the linking to complete:&lt;/P&gt;&lt;TABLE border="0" cellpadding="0" cellspacing="0"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;FONT&gt;In "C/C++" Buid - Settings - Tool Settings - ColdFire Linker - Input - Link Command File - Change the path to "${MQX_Path}\lib\m52223evb.cw10\bsp\intflash.lcf"&lt;/FONT&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;FONT&gt;In "C/C++" Buid - Settings - Tool Settings - ColdFire Linker - Input - Library Search Paths - Added the path to "${MQX_Path}/lib/m52223evb.cw10/psp"&lt;/FONT&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Now I can’t seem to get a the P&amp;amp;E USB ColdFire Multi-Link to be recognized – I go to the “Device/Connection Change Wizard” and select a “m52223evb” and then a “P&amp;amp;E Universal/USB MultiLink” (which should be correct).&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Next, I select “Flash File to Target”, with everything set up as I did with my previous version of MQX &amp;amp; CW and and get a window saying that there was an error connecting to the Launch Configuration Dialog.&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;When I go to the Debug Launch Config Dialog, I don't get an option to specify the programmer's connection (like I did with CW10.0 and MQX 3.6.0).&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Calibri" size="3"&gt;In trying to figure out what the issue is, I discovered that when I go to “File” and then “New”, I don’t have the capability to create a new MQX Project – it seems like the installation (which was done after installing MQX 10.1) didn’t take.&amp;nbsp;&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;Comments or ideas on what to try next?&lt;/DIV&gt;&lt;DIV&gt;Thanx,&lt;/DIV&gt;&lt;DIV&gt;myke&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Feb 2011 06:51:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-Configuring-New-Set-Up-with-CW-10-1-and-MQX-3-7-0-EAR/m-p/185507#M3143</guid>
      <dc:creator>mykepredko</dc:creator>
      <dc:date>2011-02-24T06:51:49Z</dc:date>
    </item>
    <item>
      <title>Re: Problem Configuring New Set Up with CW 10.1 and MQX 3.7.0 EAR - Build Fixed, now trying to Progr</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-Configuring-New-Set-Up-with-CW-10-1-and-MQX-3-7-0-EAR/m-p/185508#M3144</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mykepredko,&lt;/P&gt;&lt;P&gt;The MCF52223EVB projects aren't fully supported yet in FSLMQX3.7.0EAR...ergo your issues.&lt;/P&gt;&lt;P&gt;I've been playing with the FSLMQX/mqx/examples/hello example for the MCF52223EVB and generically had to do the following:&lt;/P&gt;&lt;P&gt;- change the paths for compile and link from:&lt;/P&gt;&lt;P&gt;FSLMQX/lib/mqx&lt;/P&gt;&lt;P&gt;to:&lt;/P&gt;&lt;P&gt;FSLMQX/lib/bsp and FSLMQX/lib/psp&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Once it compiled and linked I too got the error during flash that you got.&amp;nbsp; Turns out the paths for the P&amp;amp;E *.cfg and *.mem were pointing to the FSLMQX/lib/mqx/dbg path and should be FSLMQX/lib/bsp/dbg.&lt;/P&gt;&lt;P&gt;Note I had to update this for both Relase and Debug targets to get the erase and programming to work correctly.&lt;/P&gt;&lt;P&gt;My guess is it is the Release target paths that get used.....&lt;/P&gt;&lt;P&gt;To update those paths do following:&lt;/P&gt;&lt;P&gt;Right click on your application project and selecte Properties.&lt;/P&gt;&lt;P&gt;Click on Run/Debug Setting and select one of the Launch configurations, then click Edit.&lt;/P&gt;&lt;P&gt;Click Edit under the Remote system heading.&lt;/P&gt;&lt;P&gt;Click the System tab next to the Connect (default) tab.&lt;/P&gt;&lt;P&gt;Update the path from:&lt;/P&gt;&lt;P&gt;${MQX_PATH}/lib/m52223evb.cw10/mqx/dbg/m52223evb.cfg&lt;/P&gt;&lt;P&gt;To:&lt;/P&gt;&lt;P&gt;${MQX_PATH}/lib/m52223evb.cw10/bsp/dbg/m52223evb.cfg&lt;/P&gt;&lt;P&gt;Repeat for the Memory configuration.&lt;/P&gt;&lt;P&gt;Repeat steps for the other Launch configuration.&lt;/P&gt;&lt;P&gt;Then try your Flash File To Target process.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Feb 2011 06:19:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-Configuring-New-Set-Up-with-CW-10-1-and-MQX-3-7-0-EAR/m-p/185508#M3144</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2011-02-25T06:19:47Z</dc:date>
    </item>
    <item>
      <title>Re: Problem Configuring New Set Up with CW 10.1 and MQX 3.7.0 EAR - Build Fixed, now trying to Progr</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-Configuring-New-Set-Up-with-CW-10-1-and-MQX-3-7-0-EAR/m-p/185509#M3145</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanx for the suggestions but no joy.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I still get the same message saying:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#ff0000" size="2"&gt;&lt;FONT color="#ff0000" size="2"&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P align="left"&gt;Error: Connect Failed.&lt;/P&gt;&lt;P align="left"&gt;Can't connect. The Debugger can not connect to the P&amp;amp;E BDC interface or targetted hardware board.(ColdFire GDI Protocol Adapter&lt;/P&gt;&lt;P&gt;Error: command failed&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#888888"&gt;I tried changing the "Connection type:" to "Generic GDI" as well some others with no luck.&amp;nbsp; The correct one seems to be a "P&amp;amp;E ColdFire V234 Multilink\Cyclone Max" and when I click on "Compatible Hardware" in the "Connection" box, I get a web page with three devices, one of which is my ColdFire Multilink Adapter.&amp;nbsp; The "Interface" (also under "Connection") options available to me are "USB Multilink, Embedded OSBDM - USB Port", "Cyclone Max - Serial Port", "Cyclone Max - Ethernet Port" and "Cyclone Max - USB Port".&amp;nbsp; When I try to program and get the P&amp;amp;E COnnection Assistant and it seems to be looking for a BDM port.&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#888888"&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#888888"&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#888888"&gt;Any ideas?&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#888888"&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#888888"&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#888888"&gt;Thanx,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#888888"&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#888888"&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#888888"&gt;myke&lt;/FONT&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Feb 2011 14:00:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-Configuring-New-Set-Up-with-CW-10-1-and-MQX-3-7-0-EAR/m-p/185509#M3145</guid>
      <dc:creator>mykepredko</dc:creator>
      <dc:date>2011-02-28T14:00:05Z</dc:date>
    </item>
    <item>
      <title>Re: Problem Configuring New Set Up with CW 10.1 and MQX 3.7.0 EAR - Build Fixed, now trying to Progr</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-Configuring-New-Set-Up-with-CW-10-1-and-MQX-3-7-0-EAR/m-p/185510#M3146</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mykepredko,&lt;/P&gt;&lt;P&gt;Sorry for delay...my computer had virus.&lt;/P&gt;&lt;P&gt;Often when I have connection issue with a project I will try to step back and either use another version of CodeWarrior (easy for me but if you have older one handy) or try to find an exiting project (FSLMQX/mqx/examples/hello) or create a new baremetal project for the processor.&amp;nbsp; A trouble project sometimes is very difficult to debug since they have soooo many settings that could go wrong.&lt;/P&gt;&lt;P&gt;Please try to run existing project or create a new baremetal project for the processor and see if that allows you to connect.&lt;/P&gt;&lt;P&gt;Assuming it does then either you can compare the configuration windows (fun...not) or create a new project as similar to the one you are debugging and pull your code base into the working project.&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Mar 2011 06:20:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-Configuring-New-Set-Up-with-CW-10-1-and-MQX-3-7-0-EAR/m-p/185510#M3146</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2011-03-02T06:20:42Z</dc:date>
    </item>
    <item>
      <title>Re: Problem Configuring New Set Up with CW 10.1 and MQX 3.7.0 EAR - Build Fixed, now trying to Progr</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-Configuring-New-Set-Up-with-CW-10-1-and-MQX-3-7-0-EAR/m-p/185511#M3147</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;That's not a bad suggestion; I think I'm going to try installing CW 10.0 on another PC and see if I can to the point where I can at least program the CF and HCS08 devices again.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;One of the issues is, I use a Win 7 PC for development, which means I have to use CW 10.x but using another PC, along with this I also want to use Kinetis in my app.&amp;nbsp; I suspect my problems are deeper than an incorrect configuration.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Well, this is why they call it the &lt;STRIKE&gt;blues&lt;/STRIKE&gt; bleeding edge.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanx, I'll let you know how I make out.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Good luck with your PC - I hope you can eradicate the virus fairly easily.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;myke&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Mar 2011 13:26:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-Configuring-New-Set-Up-with-CW-10-1-and-MQX-3-7-0-EAR/m-p/185511#M3147</guid>
      <dc:creator>mykepredko</dc:creator>
      <dc:date>2011-03-02T13:26:33Z</dc:date>
    </item>
    <item>
      <title>Re: Problem Configuring New Set Up with CW 10.1 and MQX 3.7.0 EAR - Build Fixed, now trying to Progr</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-Configuring-New-Set-Up-with-CW-10-1-and-MQX-3-7-0-EAR/m-p/185512#M3148</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Myke,&lt;/P&gt;&lt;P&gt;I have a desktop that uses Win7.&amp;nbsp; When I install CW10.x I do not use the "Program Files" path as it has extra permission stuff that gets affects operations unless you always run as Admin.&lt;/P&gt;&lt;P&gt;When I install I use the default path BUT delete the "Program Files" portion of the path so that the default becomes:&lt;/P&gt;&lt;P&gt;c:\Freescale\CW MCU v10.x.&amp;nbsp; Also when installing CW10.x other installs for the debugger drivers get installed.&amp;nbsp; Another reason not to install to Program Files as it might affect their proper install.&lt;/P&gt;&lt;P&gt;I do the same when installing FSLMQX.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Note always install CW first, then FSLMQX as FSLMQX copies some files to CW path.&lt;/P&gt;&lt;P&gt;Good luck.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Mar 2011 23:05:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-Configuring-New-Set-Up-with-CW-10-1-and-MQX-3-7-0-EAR/m-p/185512#M3148</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2011-03-02T23:05:31Z</dc:date>
    </item>
    <item>
      <title>Re: Problem Configuring New Set Up with CW 10.1 and MQX 3.7.0 EAR - Build Fixed, now trying to Progr</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-Configuring-New-Set-Up-with-CW-10-1-and-MQX-3-7-0-EAR/m-p/185513#M3149</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanx for the suggestion - I have been installing MQX at the C root, but not CW.&amp;nbsp; I do always run as administrator and while that was a bit of an issue with CW 10.0, I haven't seen the same issues with 10.1.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'll try deinstalling both and then reinstall CW at the root followed by MQX.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Once this is done, I'll let you know how it goes.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanx again,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;myke&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Mar 2011 00:46:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-Configuring-New-Set-Up-with-CW-10-1-and-MQX-3-7-0-EAR/m-p/185513#M3149</guid>
      <dc:creator>mykepredko</dc:creator>
      <dc:date>2011-03-03T00:46:40Z</dc:date>
    </item>
    <item>
      <title>Re: Problem Configuring New Set Up with CW 10.1 and MQX 3.7.0 EAR</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-Configuring-New-Set-Up-with-CW-10-1-and-MQX-3-7-0-EAR/m-p/185514#M3150</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Mike, Browse to the folder where the MQX libraries are placed, (MQX install folder)\lib\(target).cw10\mqx and verify that the .lcf file is there.&amp;nbsp; On the 3.6.2 version, the lcf file was there.&amp;nbsp; I can't tell you about the 3.7 version because I don't have it yet.&amp;nbsp; If the lcf file is not where you expected, check that the&amp;nbsp;(MQX install folder)\mqx\build\bat\bsp_(target).bat is being run after rebuilding the MQX libraries.&amp;nbsp; Make sure you have rebuilt both debug and release versions.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Mar 2011 07:30:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-Configuring-New-Set-Up-with-CW-10-1-and-MQX-3-7-0-EAR/m-p/185514#M3150</guid>
      <dc:creator>kecart</dc:creator>
      <dc:date>2011-03-03T07:30:37Z</dc:date>
    </item>
    <item>
      <title>Re: Problem Configuring New Set Up with CW 10.1 and MQX 3.7.0 EAR</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-Configuring-New-Set-Up-with-CW-10-1-and-MQX-3-7-0-EAR/m-p/185515#M3151</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Cart,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sorry, I've already done that - I modify my .lcf quite a bit for my application so I'm very familiar with it.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I appreciate you taking the time to make the suggestion - Thanx!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;myke&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Mar 2011 15:58:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-Configuring-New-Set-Up-with-CW-10-1-and-MQX-3-7-0-EAR/m-p/185515#M3151</guid>
      <dc:creator>mykepredko</dc:creator>
      <dc:date>2011-03-03T15:58:07Z</dc:date>
    </item>
    <item>
      <title>Re: Problem Configuring New Set Up with CW 10.1 and MQX 3.7.0 EAR</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-Configuring-New-Set-Up-with-CW-10-1-and-MQX-3-7-0-EAR/m-p/185516#M3152</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Myke,&lt;/P&gt;&lt;P&gt;A link that might help you.&amp;nbsp; It is to check the OSBDM version and also help to update it.&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.pemicro.com/osbdm/" rel="nofollow" target="_blank"&gt;http://www.pemicro.com/osbdm/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Mar 2011 22:20:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Problem-Configuring-New-Set-Up-with-CW-10-1-and-MQX-3-7-0-EAR/m-p/185516#M3152</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2011-03-04T22:20:31Z</dc:date>
    </item>
  </channel>
</rss>