<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックRealizing IEEE 1588 using TWR-WIFI-G1011MI: 802.11b Wi-Fi Module (GainSpan)</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Realizing-IEEE-1588-using-TWR-WIFI-G1011MI-802-11b-Wi-Fi-Module/m-p/185088#M3088</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi you all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;do you know, whether it's possible to synchronize two or more Kinetis K60 tower systems with the TWR-WIFI-G1011MI board based on IEEE 1588 protocol. If yes, is there an AN for it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm looking for a wireless synchronisation of the systems without any access point or wired IP system, only WLAN synchronisation with all the WiFi moduls running in adhoc mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance for any idea or helpful information.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My very best&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Aug 2012 00:46:50 GMT</pubDate>
    <dc:creator>ThomNet</dc:creator>
    <dc:date>2012-08-02T00:46:50Z</dc:date>
    <item>
      <title>Realizing IEEE 1588 using TWR-WIFI-G1011MI: 802.11b Wi-Fi Module (GainSpan)</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Realizing-IEEE-1588-using-TWR-WIFI-G1011MI-802-11b-Wi-Fi-Module/m-p/185088#M3088</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi you all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;do you know, whether it's possible to synchronize two or more Kinetis K60 tower systems with the TWR-WIFI-G1011MI board based on IEEE 1588 protocol. If yes, is there an AN for it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm looking for a wireless synchronisation of the systems without any access point or wired IP system, only WLAN synchronisation with all the WiFi moduls running in adhoc mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance for any idea or helpful information.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My very best&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Aug 2012 00:46:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Realizing-IEEE-1588-using-TWR-WIFI-G1011MI-802-11b-Wi-Fi-Module/m-p/185088#M3088</guid>
      <dc:creator>ThomNet</dc:creator>
      <dc:date>2012-08-02T00:46:50Z</dc:date>
    </item>
    <item>
      <title>Re: Realizing IEEE 1588 using TWR-WIFI-G1011MI: 802.11b Wi-Fi Module (GainSpan)</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Realizing-IEEE-1588-using-TWR-WIFI-G1011MI-802-11b-Wi-Fi-Module/m-p/185089#M3089</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; I am also trying to connect using adhoc mode, but I am using a RedPine Signal module RS-2101 and MQX 3.7. &amp;nbsp;I tried the "light webserver" demo project that installs with the RedPine patch. &amp;nbsp;There is settings (#define) that can be change to compile the software to run in adhoc. &amp;nbsp;I was able to create a network. &amp;nbsp;I am able to join the network from a Ipad, but it looks like I can't reach the web server (a static IP was set on the ipad since no DCHP server is running).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; I am also wondering if adhoc connection is possible (with MQX 3.7 or later) and if there is a working demo that exist.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Aug 2012 05:46:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Realizing-IEEE-1588-using-TWR-WIFI-G1011MI-802-11b-Wi-Fi-Module/m-p/185089#M3089</guid>
      <dc:creator>slaroche</dc:creator>
      <dc:date>2012-08-09T05:46:55Z</dc:date>
    </item>
    <item>
      <title>Re: Realizing IEEE 1588 using TWR-WIFI-G1011MI: 802.11b Wi-Fi Module (GainSpan)</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Realizing-IEEE-1588-using-TWR-WIFI-G1011MI-802-11b-Wi-Fi-Module/m-p/185090#M3090</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Adhoc connection is possible (with MQX 3.7). Were you able to ping from ipad?&lt;/P&gt;&lt;P&gt;Can you try to make ipad as a creator of adhoc and compile the code with setting as Joiner in project.&lt;/P&gt;&lt;P&gt;webserver from ipad should be reachable and it should work.&lt;/P&gt;&lt;P&gt;Please let me know your observation.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Oct 2012 07:46:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Realizing-IEEE-1588-using-TWR-WIFI-G1011MI-802-11b-Wi-Fi-Module/m-p/185090#M3090</guid>
      <dc:creator>Tarun_redpine</dc:creator>
      <dc:date>2012-10-02T07:46:03Z</dc:date>
    </item>
  </channel>
</rss>