<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MQX BSP for MCF52255 in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-BSP-for-MCF52255/m-p/184633#M3075</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;MQX supports the M52259DEMO board, but I'm using the MCF52255 in a new project. Does anyone out there perhaps use this device? If so, I would appreciate it if you could give me and idea of how much effort is involved in modifying the existing BSP to support the MCF52255.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 21 Nov 2011 18:34:58 GMT</pubDate>
    <dc:creator>trusc</dc:creator>
    <dc:date>2011-11-21T18:34:58Z</dc:date>
    <item>
      <title>MQX BSP for MCF52255</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-BSP-for-MCF52255/m-p/184633#M3075</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;MQX supports the M52259DEMO board, but I'm using the MCF52255 in a new project. Does anyone out there perhaps use this device? If so, I would appreciate it if you could give me and idea of how much effort is involved in modifying the existing BSP to support the MCF52255.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Nov 2011 18:34:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-BSP-for-MCF52255/m-p/184633#M3075</guid>
      <dc:creator>trusc</dc:creator>
      <dc:date>2011-11-21T18:34:58Z</dc:date>
    </item>
    <item>
      <title>Re: MQX BSP for MCF52255</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-BSP-for-MCF52255/m-p/184634#M3076</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The BSP for M52259EVB should work as is on your MCF52255 board, however as MCF52255 has no flexbus, you must comment-out the following code in mqx/source/bsp/m52259evb/bsp_init.c :&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;#if 0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Enable Mini FlexBUS signals (used by external MRAM and CPLD) */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; reg_ptr-&amp;gt;GPIO.PASPAR = 0x20;&amp;nbsp;&amp;nbsp; /* enable CS1 operation for CPLD */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; reg_ptr-&amp;gt;GPIO.PTEPAR = 0xff;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; reg_ptr-&amp;gt;GPIO.PTFPAR = 0xff;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; reg_ptr-&amp;gt;GPIO.PTGPAR = 0xff;&amp;nbsp;&amp;nbsp; /* enable CS0 operation for MRAM */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; reg_ptr-&amp;gt;GPIO.PTHPAR = 0x5555;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; _bsp_flexbus_mram_setup((uint_32)BSP_EXTERNAL_MRAM_BASE);&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;#endif&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you don't do that the BSP will fail to start hanging here.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also check that the 80Mhz frequency used on MCF52259EVB is allowed on your CPU.&lt;/P&gt;&lt;P&gt;I worked on an MCF52254 and had to reduce the frequency below 66Mhz by doing changes for PLL settings in the same file.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Nov 2011 21:52:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-BSP-for-MCF52255/m-p/184634#M3076</guid>
      <dc:creator>trailman</dc:creator>
      <dc:date>2011-11-24T21:52:16Z</dc:date>
    </item>
    <item>
      <title>Re: MQX BSP for MCF52255</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-BSP-for-MCF52255/m-p/184635#M3077</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the help. I'll try this now that I'm getting back into the project after the holidays. Sorry for the belated reply.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Jan 2012 16:51:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-BSP-for-MCF52255/m-p/184635#M3077</guid>
      <dc:creator>trusc</dc:creator>
      <dc:date>2012-01-16T16:51:54Z</dc:date>
    </item>
  </channel>
</rss>