<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックRe: MAC address</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/MAC-address/m-p/183016#M2944</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For testing you can use the MAC address you want.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For production you need to acquire a MAC range. Follow this link &lt;A href="http://standards.ieee.org/develop/regauth/oui/index.html" title="http://standards.ieee.org/develop/regauth/oui/index.html"&gt;IEEE-SA - Registration Authority OUI&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Some MCUs already have a registered MAC address of the manufacturer you can use.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Nov 2012 15:26:08 GMT</pubDate>
    <dc:creator>ivanpajuelo</dc:creator>
    <dc:date>2012-11-21T15:26:08Z</dc:date>
    <item>
      <title>MAC address</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MAC-address/m-p/183015#M2943</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems that the MAC address for the MQX is generated depending on the parameters you pass it into.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ENET_get_mac_address(ENET_DEVICE, ipDataGlobal.ip, tempMAC);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Isn't suppose to be a running number based from the manufacturer? If no, can I just use any generated running number here and not worry about licenses or something?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank You.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Nov 2012 11:19:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MAC-address/m-p/183015#M2943</guid>
      <dc:creator>vines</dc:creator>
      <dc:date>2012-11-21T11:19:03Z</dc:date>
    </item>
    <item>
      <title>Re: MAC address</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MAC-address/m-p/183016#M2944</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For testing you can use the MAC address you want.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For production you need to acquire a MAC range. Follow this link &lt;A href="http://standards.ieee.org/develop/regauth/oui/index.html" title="http://standards.ieee.org/develop/regauth/oui/index.html"&gt;IEEE-SA - Registration Authority OUI&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Some MCUs already have a registered MAC address of the manufacturer you can use.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Nov 2012 15:26:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MAC-address/m-p/183016#M2944</guid>
      <dc:creator>ivanpajuelo</dc:creator>
      <dc:date>2012-11-21T15:26:08Z</dc:date>
    </item>
    <item>
      <title>Re: MAC address</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MAC-address/m-p/183017#M2945</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ivan is right, just would like to add the function which should be modified for production: _bsp_get_mac_address() function in your BSP (init_enet.c source file).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Nov 2012 15:32:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MAC-address/m-p/183017#M2945</guid>
      <dc:creator>Martin_</dc:creator>
      <dc:date>2012-11-21T15:32:21Z</dc:date>
    </item>
  </channel>
</rss>