<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Increasing the Heap memory for TWR-K60N512 in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Increasing-the-Heap-memory-for-TWR-K60N512/m-p/181082#M2739</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could disabling the the lwmem option (what i mean here is disabling the MQX_USE_LWMEM_ALLOCATOR macro)&amp;nbsp;help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As of now my _mem_alloc and _mem_free are typdef'ed to the respective lwmem functions.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 20 Jul 2012 14:31:16 GMT</pubDate>
    <dc:creator>Akshaya_Mukund</dc:creator>
    <dc:date>2012-07-20T14:31:16Z</dc:date>
    <item>
      <title>Increasing the Heap memory for TWR-K60N512</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Increasing-the-Heap-memory-for-TWR-K60N512/m-p/181080#M2737</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I wanted to know if there is a way to increase the HEAP memory for an application running on MQX. My heap requirements are on the higher side and I require another 30kb or so of heap memory for my application.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am guessing these changes would have to be made in the MQX libraries (bsp, psp etc..). Could anyone point out where these changes would have to be made. Also what is the default size and maximum size of heap.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As of now in the twrk60n512.h the BSP_EXTERNAL_MRAM_RAM_SIZE is commented out. Could the MRAM be used to increase heap size ? I understand that removing the IrDA receiver i.e. R14 allows MRAM usage and the board I am using has this modification (R14 removed) will this be of any help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jul 2012 20:34:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Increasing-the-Heap-memory-for-TWR-K60N512/m-p/181080#M2737</guid>
      <dc:creator>Akshaya_Mukund</dc:creator>
      <dc:date>2012-07-19T20:34:19Z</dc:date>
    </item>
    <item>
      <title>Re: Increasing the Heap memory for TWR-K60N512</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Increasing-the-Heap-memory-for-TWR-K60N512/m-p/181081#M2738</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Your possible choices are:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;optimize code( disable unused components, change linkercomand file, change static data to dynamic ...)&lt;/LI&gt;&lt;LI&gt;change target to mram target (a litle slower memory but bigger)&lt;/LI&gt;&lt;LI&gt;create memory pool at mram (_lwmem_create_pool(...))&amp;nbsp;and alloc your staff there (&amp;nbsp; _mem_alloc_from(...),...),&lt;/LI&gt;&lt;/OL&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jul 2012 22:23:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Increasing-the-Heap-memory-for-TWR-K60N512/m-p/181081#M2738</guid>
      <dc:creator>BielikM</dc:creator>
      <dc:date>2012-07-19T22:23:59Z</dc:date>
    </item>
    <item>
      <title>Re: Increasing the Heap memory for TWR-K60N512</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Increasing-the-Heap-memory-for-TWR-K60N512/m-p/181082#M2739</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could disabling the the lwmem option (what i mean here is disabling the MQX_USE_LWMEM_ALLOCATOR macro)&amp;nbsp;help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As of now my _mem_alloc and _mem_free are typdef'ed to the respective lwmem functions.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jul 2012 14:31:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Increasing-the-Heap-memory-for-TWR-K60N512/m-p/181082#M2739</guid>
      <dc:creator>Akshaya_Mukund</dc:creator>
      <dc:date>2012-07-20T14:31:16Z</dc:date>
    </item>
    <item>
      <title>Re: Increasing the Heap memory for TWR-K60N512</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Increasing-the-Heap-memory-for-TWR-K60N512/m-p/181083#M2740</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I noticed that the available heap memory for mallocs was fixed at ~84.5 KB. Is this the maximum available RAM on the TWR-K60. Can this be increased by changing some macros or is the only way to increase this available memory implemented by&amp;nbsp;physically adding memory via a TWR-MEM (or some MRAM). Also I wasn't able to find any documentation to successfully integrate the TWR-MEM into the MQX/TWR-k60 setup.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please do let me know if you could give me some pointers on this.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Jul 2012 12:23:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Increasing-the-Heap-memory-for-TWR-K60N512/m-p/181083#M2740</guid>
      <dc:creator>Akshaya_Mukund</dc:creator>
      <dc:date>2012-07-27T12:23:49Z</dc:date>
    </item>
    <item>
      <title>Re: Increasing the Heap memory for TWR-K60N512</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Increasing-the-Heap-memory-for-TWR-K60N512/m-p/181084#M2741</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did you get any conclusion about the heap memory? I'm having right now problems with the pool memory and I need to know how could I fix these problems.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks you in advance. Regards, &lt;/P&gt;&lt;P&gt;Eduardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Sep 2012 10:17:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Increasing-the-Heap-memory-for-TWR-K60N512/m-p/181084#M2741</guid>
      <dc:creator>Ardoster</dc:creator>
      <dc:date>2012-09-19T10:17:46Z</dc:date>
    </item>
    <item>
      <title>Re: Increasing the Heap memory for TWR-K60N512</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Increasing-the-Heap-memory-for-TWR-K60N512/m-p/181085#M2742</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I recently played with adding a memory pool using the TWR-K60N512 kit with TWR-MEM Rev B card.&lt;/P&gt;&lt;P&gt;Please look at the following post for more details:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/301229"&gt;https://community.freescale.com/message/301229&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Sep 2012 20:49:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Increasing-the-Heap-memory-for-TWR-K60N512/m-p/181085#M2742</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2012-09-20T20:49:35Z</dc:date>
    </item>
  </channel>
</rss>