<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software Solutions中的主题 Re: CW10, MQX3.6, sem_open, semaphore pointer shared between tasks</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/CW10-MQX3-6-sem-open-semaphore-pointer-shared-between-tasks/m-p/174384#M2166</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Follow up - actually the sample code for sem_open in the MQX Reference Manual would imply this could be done since sem_handle is being used without a corresponding sem_open, although the sem_handle is never initialized.&amp;nbsp; This is different from the same code in the users guide.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Will&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 08 Jan 2011 05:09:05 GMT</pubDate>
    <dc:creator>WHookway</dc:creator>
    <dc:date>2011-01-08T05:09:05Z</dc:date>
    <item>
      <title>CW10, MQX3.6, sem_open, semaphore pointer shared between tasks</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/CW10-MQX3-6-sem-open-semaphore-pointer-shared-between-tasks/m-p/174383#M2165</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Assuming the semaphores and threads are going to be used for the life of the program is it necessary to use sem_open for each thread that wishes to use the semaphore?&amp;nbsp; Can the initialization routine use sem_create followed by a sem_open and then pass the pointer to the semaphore to all those that need it?&amp;nbsp; Same question for the events.&amp;nbsp; I do plan on using the SEM_PRIORITY_INHERITANCE.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Will&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 08 Jan 2011 04:50:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/CW10-MQX3-6-sem-open-semaphore-pointer-shared-between-tasks/m-p/174383#M2165</guid>
      <dc:creator>WHookway</dc:creator>
      <dc:date>2011-01-08T04:50:33Z</dc:date>
    </item>
    <item>
      <title>Re: CW10, MQX3.6, sem_open, semaphore pointer shared between tasks</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/CW10-MQX3-6-sem-open-semaphore-pointer-shared-between-tasks/m-p/174384#M2166</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Follow up - actually the sample code for sem_open in the MQX Reference Manual would imply this could be done since sem_handle is being used without a corresponding sem_open, although the sem_handle is never initialized.&amp;nbsp; This is different from the same code in the users guide.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Will&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 08 Jan 2011 05:09:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/CW10-MQX3-6-sem-open-semaphore-pointer-shared-between-tasks/m-p/174384#M2166</guid>
      <dc:creator>WHookway</dc:creator>
      <dc:date>2011-01-08T05:09:05Z</dc:date>
    </item>
    <item>
      <title>Re: CW10, MQX3.6, sem_open, semaphore pointer shared between tasks</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/CW10-MQX3-6-sem-open-semaphore-pointer-shared-between-tasks/m-p/174385#M2167</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for pointing to this. Your change request was accepted and the RM will be changed with next release of MQX.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Jan 2011 22:15:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/CW10-MQX3-6-sem-open-semaphore-pointer-shared-between-tasks/m-p/174385#M2167</guid>
      <dc:creator>JuroV</dc:creator>
      <dc:date>2011-01-27T22:15:01Z</dc:date>
    </item>
  </channel>
</rss>