<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic RS-485 in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/RS-485/m-p/172852#M2074</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;Hello,&amp;nbsp;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I use CW10.2, MQX 3.8 and TWR-K60F120M tower demo&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;system. I would like to implement RS485. I have seen that&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;there is demo example come with MQX which is at&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;C:\Program Files\Freescale\Freescale MQX&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;3.8\mqx\examples\rs485. I have built this project, but I can’t&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;see any data from Clear Terminal which is connected to my&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;PC RS-232 port.&amp;nbsp;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I set jumpers on TWR-SER board to make J15 as RS-485&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;(instead of RS-232) according to TWR-SER User Manual. I have defined&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;BSPCFG_ENABLE_TTYF and BSPCFG_ENABLE_TTYB to&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;be “1” at both user_config.h and twrk60f120m.h. (I check&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;schematics of TWR-K60F120M, TWR-SER and tower&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;boards, it looks like UART1 is connected to J15 of TWR-&lt;/SPAN&gt;&lt;SPAN&gt;SER. If I am wrong, please point out to me. Thanks!). I also&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;set BSP_DEFAULT_IO_CHANNEL to be “ttyf:”. I use SENA&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;LTC100 RS-232 to RS485 converter connecting to J15 of&amp;nbsp;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;TWR-SER. I can see print out with printf() from both P&amp;amp;E&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;Terminal Window (which I believe is connected to UART6)&amp;nbsp;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;and Clear Terminal which is monitoring RS-232 port of my PC&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;and the other end is UART1 of demo board.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have also tried ITTYB, there is no luck.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What I have missed? Why it doesn't work? I use CW10.2&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;debugger to debug this rs485 demo program, it looks like&amp;nbsp;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;that write() function is not successful. Please help me to&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;identity this problem. I guess the problem is on software, not&amp;nbsp;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;hardware.&amp;nbsp;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks!&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Jun 2012 03:18:51 GMT</pubDate>
    <dc:creator>lisa_tx</dc:creator>
    <dc:date>2012-06-19T03:18:51Z</dc:date>
    <item>
      <title>RS-485</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/RS-485/m-p/172852#M2074</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;Hello,&amp;nbsp;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I use CW10.2, MQX 3.8 and TWR-K60F120M tower demo&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;system. I would like to implement RS485. I have seen that&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;there is demo example come with MQX which is at&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;C:\Program Files\Freescale\Freescale MQX&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;3.8\mqx\examples\rs485. I have built this project, but I can’t&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;see any data from Clear Terminal which is connected to my&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;PC RS-232 port.&amp;nbsp;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I set jumpers on TWR-SER board to make J15 as RS-485&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;(instead of RS-232) according to TWR-SER User Manual. I have defined&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;BSPCFG_ENABLE_TTYF and BSPCFG_ENABLE_TTYB to&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;be “1” at both user_config.h and twrk60f120m.h. (I check&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;schematics of TWR-K60F120M, TWR-SER and tower&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;boards, it looks like UART1 is connected to J15 of TWR-&lt;/SPAN&gt;&lt;SPAN&gt;SER. If I am wrong, please point out to me. Thanks!). I also&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;set BSP_DEFAULT_IO_CHANNEL to be “ttyf:”. I use SENA&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;LTC100 RS-232 to RS485 converter connecting to J15 of&amp;nbsp;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;TWR-SER. I can see print out with printf() from both P&amp;amp;E&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;Terminal Window (which I believe is connected to UART6)&amp;nbsp;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;and Clear Terminal which is monitoring RS-232 port of my PC&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;and the other end is UART1 of demo board.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have also tried ITTYB, there is no luck.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What I have missed? Why it doesn't work? I use CW10.2&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;debugger to debug this rs485 demo program, it looks like&amp;nbsp;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;that write() function is not successful. Please help me to&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;identity this problem. I guess the problem is on software, not&amp;nbsp;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;hardware.&amp;nbsp;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks!&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jun 2012 03:18:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/RS-485/m-p/172852#M2074</guid>
      <dc:creator>lisa_tx</dc:creator>
      <dc:date>2012-06-19T03:18:51Z</dc:date>
    </item>
    <item>
      <title>Re: RS-485 (on twr-k60f120m)</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/RS-485/m-p/172853#M2075</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Never mind. I have figured it out. UART5 (TTYF or ITTYF) is connected to TWR-SER serial connector.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jun 2012 07:28:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/RS-485/m-p/172853#M2075</guid>
      <dc:creator>lisa_tx</dc:creator>
      <dc:date>2012-06-19T07:28:42Z</dc:date>
    </item>
  </channel>
</rss>