<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックRecommended MQX interrupt levels</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Recommended-MQX-interrupt-levels/m-p/172049#M2011</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm working on custom K53 board using MQX 3.8, MFS, RTCS, USB Device, LPM active, I2C and SPI.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Since I'm working on battery powered device I need to save power and hence do clock switching (internal vs external) and turning things on and off all the time. My setup seems to be working relatively well. But...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Looks like after while Timer task is stuck and LW Semaphore TIMER_ISR_LWSEM keeps counting but timer task is stuck.&lt;/P&gt;&lt;P&gt;Have been browsing this forum and found posts "possible scheduler bug in MQX 3.7" and "Ready task not entered" helpful. &lt;A __default_attr="99232" class="jive_macro jive_macro_thread default_title" href="https://community.freescale.com/thread/99232" jivemacro="thread" title="https://community.freescale.com/thread/99232"&gt;https://community.freescale.com/thread/99232&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using pretty much "inherited" interrupt levels from twrk53n512.h. For example I2C interrupt levels are 1 which is same that one set for the timer ISR. So, assuming that interrupt priority levels are the source of the problem.&lt;/P&gt;&lt;P&gt;Just wondering what would be recommended Interrupt priorities for the MQX?&lt;/P&gt;&lt;P&gt;Timer 1, I2C and ports 3 other ones 4-5? Something else?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 Jun 2012 20:43:10 GMT</pubDate>
    <dc:creator>kaskasi</dc:creator>
    <dc:date>2012-06-14T20:43:10Z</dc:date>
    <item>
      <title>Recommended MQX interrupt levels</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Recommended-MQX-interrupt-levels/m-p/172049#M2011</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm working on custom K53 board using MQX 3.8, MFS, RTCS, USB Device, LPM active, I2C and SPI.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Since I'm working on battery powered device I need to save power and hence do clock switching (internal vs external) and turning things on and off all the time. My setup seems to be working relatively well. But...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Looks like after while Timer task is stuck and LW Semaphore TIMER_ISR_LWSEM keeps counting but timer task is stuck.&lt;/P&gt;&lt;P&gt;Have been browsing this forum and found posts "possible scheduler bug in MQX 3.7" and "Ready task not entered" helpful. &lt;A __default_attr="99232" class="jive_macro jive_macro_thread default_title" href="https://community.freescale.com/thread/99232" jivemacro="thread" title="https://community.freescale.com/thread/99232"&gt;https://community.freescale.com/thread/99232&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using pretty much "inherited" interrupt levels from twrk53n512.h. For example I2C interrupt levels are 1 which is same that one set for the timer ISR. So, assuming that interrupt priority levels are the source of the problem.&lt;/P&gt;&lt;P&gt;Just wondering what would be recommended Interrupt priorities for the MQX?&lt;/P&gt;&lt;P&gt;Timer 1, I2C and ports 3 other ones 4-5? Something else?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jun 2012 20:43:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Recommended-MQX-interrupt-levels/m-p/172049#M2011</guid>
      <dc:creator>kaskasi</dc:creator>
      <dc:date>2012-06-14T20:43:10Z</dc:date>
    </item>
  </channel>
</rss>