<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックSDCARD SPI Driver</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/SDCARD-SPI-Driver/m-p/171675#M1988</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I noticied that the clock for the SPI bus is set to 400KHz in the MQX driver.&amp;nbsp; I'd like to run it as fast as possible. Can someone tell me what I need to do to run it at 20MHz?&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 01 Feb 2010 23:31:50 GMT</pubDate>
    <dc:creator>Mike_d</dc:creator>
    <dc:date>2010-02-01T23:31:50Z</dc:date>
    <item>
      <title>SDCARD SPI Driver</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/SDCARD-SPI-Driver/m-p/171675#M1988</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I noticied that the clock for the SPI bus is set to 400KHz in the MQX driver.&amp;nbsp; I'd like to run it as fast as possible. Can someone tell me what I need to do to run it at 20MHz?&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Feb 2010 23:31:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/SDCARD-SPI-Driver/m-p/171675#M1988</guid>
      <dc:creator>Mike_d</dc:creator>
      <dc:date>2010-02-01T23:31:50Z</dc:date>
    </item>
    <item>
      <title>Re: SDCARD SPI Driver</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/SDCARD-SPI-Driver/m-p/171676#M1989</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mike_d,&lt;/P&gt;&lt;P&gt;Assuming M52259EVB bsp inside the m52259evb.h you can change the baud rate:&lt;/P&gt;&lt;P&gt;/*&lt;BR /&gt;** The SPI settings.&lt;BR /&gt;*/&lt;BR /&gt;#define BSP_QSPI_RX_BUFFER_SIZE&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (32)&lt;BR /&gt;#define BSP_QSPI_TX_BUFFER_SIZE&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (32)&lt;BR /&gt;#define BSP_QSPI_BAUDRATE&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1000000&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Feb 2010 23:16:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/SDCARD-SPI-Driver/m-p/171676#M1989</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2010-02-03T23:16:36Z</dc:date>
    </item>
  </channel>
</rss>