<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックSPI driveer question</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/SPI-driveer-question/m-p/171608#M1976</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I have used the MQS spi to control an eeprom which the spi demo did with out any trouble. However, I now want to send and receive data packet&amp;nbsp; using the PSI port on a TWR-K60. I am not sure the SPI demo is still the correct demo to follow.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to send a 32 byte packet in master mode and at the same time receive the responce packet at the same time. Also I the K60 should be able to handle the SS line for me. Any examples or sample code?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Jun 2012 20:46:42 GMT</pubDate>
    <dc:creator>barbercolman</dc:creator>
    <dc:date>2012-06-12T20:46:42Z</dc:date>
    <item>
      <title>SPI driveer question</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/SPI-driveer-question/m-p/171608#M1976</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I have used the MQS spi to control an eeprom which the spi demo did with out any trouble. However, I now want to send and receive data packet&amp;nbsp; using the PSI port on a TWR-K60. I am not sure the SPI demo is still the correct demo to follow.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to send a 32 byte packet in master mode and at the same time receive the responce packet at the same time. Also I the K60 should be able to handle the SS line for me. Any examples or sample code?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jun 2012 20:46:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/SPI-driveer-question/m-p/171608#M1976</guid>
      <dc:creator>barbercolman</dc:creator>
      <dc:date>2012-06-12T20:46:42Z</dc:date>
    </item>
    <item>
      <title>Re: SPI driveer question</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/SPI-driveer-question/m-p/171609#M1977</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the SPI example also shows how to perform duplex read/write operation using IO_IOCTL_SPI_READ_WRITE ioctl command. Please follow this part of the example.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pavel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Nov 2012 10:14:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/SPI-driveer-question/m-p/171609#M1977</guid>
      <dc:creator>pavel_chromy</dc:creator>
      <dc:date>2012-11-13T10:14:50Z</dc:date>
    </item>
  </channel>
</rss>