<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Application freezes after a second or two when using FNET bootloader in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Application-freezes-after-a-second-or-two-when-using-FNET/m-p/170835#M1934</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can try to check if the MQX application sets its vector table properly (copies it to RAM and updates VBR). &lt;/P&gt;&lt;P&gt;It is only guessing (as I personally do not run the bootloader with MQX).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BTW:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I suggest to add a Service Request - "official support of MQX+FNET Bootloader” to:&lt;/P&gt;&lt;P style="text-indent: .5in;"&gt;&lt;A href="https://www.freescale.com/webapp/servicerequest.create_SR.framework"&gt;https://www.freescale.com/webapp/servicerequest.create_SR.framework&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; At least, it should be part of MQX test process.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Andrey Butok&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 12 Nov 2012 09:16:28 GMT</pubDate>
    <dc:creator>butok</dc:creator>
    <dc:date>2012-11-12T09:16:28Z</dc:date>
    <item>
      <title>Application freezes after a second or two when using FNET bootloader</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Application-freezes-after-a-second-or-two-when-using-FNET/m-p/170834#M1933</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am running the HTTP server demo on my 52259EVB.&amp;nbsp; It runs fine by itself.&amp;nbsp; I am trying to add an ethernet bootloader (FNET).&amp;nbsp; I am able to start the TFTP server on FNET and then push my .S19 image of the web server onto the bootloader.&amp;nbsp; The transfer is successfull, and when I restart the board I see the web server application start (I see all my printf statements on the webserver app).&amp;nbsp; I added a loop that puts a print statement out every second and it just stops after 2 or 3 times through the loop.&amp;nbsp; I have plenty or room left in ROM, so it shouldn't have any issue with space...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I made the .lcf mods that are described to change memory start to 0xC000, etc...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems that the application starts and then just freezes after a few seconds.&amp;nbsp; It runs fine when loaded onto the board by itself without the bootloader.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any ideas why?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 11 Nov 2012 16:05:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Application-freezes-after-a-second-or-two-when-using-FNET/m-p/170834#M1933</guid>
      <dc:creator>njk909</dc:creator>
      <dc:date>2012-11-11T16:05:32Z</dc:date>
    </item>
    <item>
      <title>Re: Application freezes after a second or two when using FNET bootloader</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Application-freezes-after-a-second-or-two-when-using-FNET/m-p/170835#M1934</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can try to check if the MQX application sets its vector table properly (copies it to RAM and updates VBR). &lt;/P&gt;&lt;P&gt;It is only guessing (as I personally do not run the bootloader with MQX).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BTW:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I suggest to add a Service Request - "official support of MQX+FNET Bootloader” to:&lt;/P&gt;&lt;P style="text-indent: .5in;"&gt;&lt;A href="https://www.freescale.com/webapp/servicerequest.create_SR.framework"&gt;https://www.freescale.com/webapp/servicerequest.create_SR.framework&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; At least, it should be part of MQX test process.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Andrey Butok&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Nov 2012 09:16:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Application-freezes-after-a-second-or-two-when-using-FNET/m-p/170835#M1934</guid>
      <dc:creator>butok</dc:creator>
      <dc:date>2012-11-12T09:16:28Z</dc:date>
    </item>
  </channel>
</rss>