<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックRe: Configure IPV6 route</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Configure-IPV6-route/m-p/2036647#M18885</link>
    <description>&lt;P&gt;Hello! I forgot to mention that we are using MQX V4.2 + RTCS IPV6 addon that we've previously purchased with NXP.&lt;BR /&gt;Using v5 is not an option for us now, could you help us in this case?&lt;/P&gt;</description>
    <pubDate>Fri, 31 Jan 2025 15:45:59 GMT</pubDate>
    <dc:creator>Coacci</dc:creator>
    <dc:date>2025-01-31T15:45:59Z</dc:date>
    <item>
      <title>Configure IPV6 route</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Configure-IPV6-route/m-p/2035612#M18883</link>
      <description>&lt;P&gt;Hello!&lt;BR /&gt;We are currently using a Wi-SUN Network, where the end-devices have IPV6 address in 2017::/64 range and they are accessible through a gateway on the network 2001 (2001::2). The Ethernet Interface of our communication board is connected directly to this gateway by a ethernet cable and was configured with the address 2001::1.&lt;/P&gt;&lt;P&gt;The initial idea was to send UDP datagrams from the board to one of the end-devices through the gateway, but it did not work (unfortunately we can't get the traffic in this scenario).&lt;/P&gt;&lt;P&gt;We did some tests using a directly communication between the board and a computer with Linux Ubuntu. We've sent the udp datagrams using IPV6 Link-Local Addresses (FE80::/64) and it worked pretty fine, we were able to get the traffic between theses two devices. But the problem is when we try to use another IPV6 address than fe80::/64, it just doesn't work.&lt;/P&gt;&lt;P&gt;With this, we have a scenario where link-local addresses work well in point-to-point communication, but any attempt to use global addresses fails, whether via Wi-SUN gateway or direct connection.&lt;BR /&gt;&lt;BR /&gt;Is there any way to configure a route on RTCS IPV6? If it's not, how can we proceed?&lt;/P&gt;</description>
      <pubDate>Wed, 29 Jan 2025 12:22:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Configure-IPV6-route/m-p/2035612#M18883</guid>
      <dc:creator>Coacci</dc:creator>
      <dc:date>2025-01-29T12:22:20Z</dc:date>
    </item>
    <item>
      <title>Re: Configure IPV6 route</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Configure-IPV6-route/m-p/2036644#M18884</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/244527"&gt;@Coacci&lt;/a&gt;&amp;nbsp;:&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Now RTCS IPv6 is wrapped in MQX v5, under commercial license.&amp;nbsp; Please refer to below link for more details.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/software/embedded-software/mqx-software-solutions/mqx-v5-software-solutions:MQX-V5?tid=vanmqxv5" target="_blank"&gt;MQX™ v5 Software Solutions | NXP Semiconductors&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;If you need further information please contact MQX team at mqxsales@nxp.com&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Fri, 31 Jan 2025 15:43:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Configure-IPV6-route/m-p/2036644#M18884</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2025-01-31T15:43:06Z</dc:date>
    </item>
    <item>
      <title>Re: Configure IPV6 route</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Configure-IPV6-route/m-p/2036647#M18885</link>
      <description>&lt;P&gt;Hello! I forgot to mention that we are using MQX V4.2 + RTCS IPV6 addon that we've previously purchased with NXP.&lt;BR /&gt;Using v5 is not an option for us now, could you help us in this case?&lt;/P&gt;</description>
      <pubDate>Fri, 31 Jan 2025 15:45:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Configure-IPV6-route/m-p/2036647#M18885</guid>
      <dc:creator>Coacci</dc:creator>
      <dc:date>2025-01-31T15:45:59Z</dc:date>
    </item>
    <item>
      <title>Re: Configure IPV6 route</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Configure-IPV6-route/m-p/2036659#M18886</link>
      <description>&lt;P&gt;Please contact &lt;A href="mailto:nxpsales@nxp.com" target="_blank"&gt;nxpsales@nxp.com&lt;/A&gt;&amp;nbsp; for IPv6 relevant questions&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Fri, 31 Jan 2025 16:15:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Configure-IPV6-route/m-p/2036659#M18886</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2025-01-31T16:15:29Z</dc:date>
    </item>
  </channel>
</rss>